全 1173 件が検索されました。(901 - 920件を表示)

  • マニュアル

    ... at startup. Using FinsGateway Select FinsGateway as the communications driver. Using CX-Server Select CX-Server as the communications driver. 1-6-3 Using FinsGateway Regardless of the connection method, use FinsGateway as the communications driver. Communications network Serial co ...

  • マニュアル

    ....0 or later). To change the size of the I/O comment 168 Section 8-2 Programming Console Operations area, refer to the CX-Programmer (version 2.0 or later) Operation Manual (W414). RUN MONITOR OK OK CLR ...

  • マニュアル

    ... Functions Remote I/O Communications Errors Error MS/NS indicators 7-segment display Master status area 1 C0 ↔ Master node address C2 ↔ Master node address C3 ↔ Master node address C4 ↔ Master node address ...

  • マニュアル

    ...A.C1 --- --- 40C1 --- --- A.C2 --- --- 40C2 --- --- A.C5 --- --- 40C5 A.C8 A.C8@ --- --- --- 40C8 A.C9 A.C9@ A.C9 --- --- 40C9 A.CA A.CA@ --- --- --- 40CA A.Cb A.Cb@ --- --- --- 40CB A.CC A.CC@ --- --- --- 40CC A.d0 --- --- --- --- 40D0 --- A.d0@ --- --- --- --- --- A.d0 --- --- 106 Error detection function Encoder overheating (Absolute encoders only) Speed command input reading error Detected error or cause of error Overheating in the encoder was detected. The A/D completion signal from the A/D converter is not being output within the fixed interval. Torque comThe A/D completion signal mand input read- from the A/D ...

  • マニュアル

    ...) 1-3 1-2 Hardware Features 1-2 1 1 Overview 1-3 ID Information Label The ID information label contains relevant information of your Industrial Monitor. A B C D NYM R SAFETY US CA OMRON Corporation Kyoto, 600-8530 JAPAN F Item A E345642 CUSTOM ID INDUSTRIAL MONITOR MADE IN THE NETHERLANDS E Name Product name Description Industrial Monitor B Model C Power rating Power rating details D Custom ID (Optional) A custom ID [NYC£££-££££££££] E Standards and QR code The standards for the OMRON monitor. Check the label of your monitor for the standards that are ...

  • マニュアル

    ... regulations. • The following information must be displayed for all products that contain primary lithium batteries with a perchlorate content of 6 ppb or higher when shipped to or transported through the State of California, USA. Perchlorate Material - special handling may apply. See http://www.dtsc....

  • マニュアル

    ...Active SlaveScaling Command Aborted MasterOffset Error SlaveOffset ErrorID ReferenceType Direction CamTransition BufferMode MC_Axis000 MC_Axis001 CamProfile0 MCCI1_InCam MCCI1_InSync MCCI1_EOP MCCI1_Index MCCI1_B MCCI1_A MCCI1_...

  • マニュアル

    ...TIME_OF_DAY_NSEC Union 0A 0B 0C Vendor Specific Vendor Specific Vendor Specific 8 8-7-1 Data Type Codes C1 C2 C3 C4 C5 C6 C7 C8 C9 CA CB D0 D1 D2 D3 DB D4 A0 A2 A3 04 05 06 07 08 09 8-7 Variable Data Types Boolean (bit) SINT (1-byte signed binary) INT (1-word signed binary) DINT (2-word signed binary) LINT (4-word signed binary) USINT (1-byte unsigned binary) UINT (1-word unsigned binary) UDINT (2-word unsigned binary) ULINT (4-word unsigned binary) REAL (2-word floating point) LREAL (...

  • マニュアル

    ... apply. • The following information must be displayed for all products that contain primary lithium batteries with a perchlorate content of 6 ppb or higher when shipped to or transported through the State of California, USA. Perchlorate Material - special handling may apply. See http://www.dtsc....

  • マニュアル

    ...-E RS-485 E5ZD-8FH03KJ-E E5ZD-8FH03P-E RS-422 E5ZD-8FH02KJM-E E5ZD-8FH02PM-E RS-485 E5ZD-8FH03KJM-E E5ZD-8FH03PM-E 1-3-1 Sensors and Temperature Ranges Thermocouple models are compatible with either K (...

  • マニュアル

    ... not present or other reasons). 4-1-4 Preparations for Operations in Monitor Mode The following information provides the relationships between various settings before the execution of read, write, or test operations in the MONITOR Mode. Operation Setting JOB specification spec ...

  • マニュアル

    ... key while measurement condition Table 3 appears displays the next table of measurement conditions. The following provides examples of measurement conditions specified for 16 scenes. 62 Section 8-4 MEASURE MODE Measurement Condition Table 1 No. Indicates the scene number ...

  • マニュアル

    ... the specified scene is set to ON, DT indicates the dislocation after the system performs coordinate-conversion. When the calibration function is set to OFF, DT indicates the dislocation in the camera coordinate system. 0 is assigned to DT when OVL–2 is initialized. ...

  • マニュアル

    ... are the same, then select O. OK. The Basic Screen will then be displayed. S.Son S.Scn D.Disp C.Camera B.Bin W.Wind O.Condi M.Meas Y.Sys T.Tool Scn00 Cam0 Raw Unfrz W0123 4567 CAL CA OFF CARD – – If the Camera I/F Unit and camera shown in the Initial Screen are not the same as those that are actually connected, then the correct images cannot be taken and the measurements will be wrong. The Camera I/F Unit and camera settings must be corrected before proceeding further. After the settings have been ...

  • マニュアル

    ... Carrier was soaked in concentrated hydrochloric acid (which can easily penetrate through PFA) at 80_C for 300 hours, then extracted substances were analyzed. • Extracted Substances (Concentration) Si . . . . . 700 ng/ml S . . . . . 1000 ng/ml ...

  • マニュアル

    ... Camera Cable is not properly connected. The lens diaphragm is opened or closed too far. The shutter speed is not suitable (for Expert Menu operation only). The lighting method is not suitable. The indicators do not turn ON (for Cameras Source). ...

  • マニュアル

    ... of ICP Emission Spectral Analysis The V600-D23P66SP Data Carrier was soaked in concentrated hydrochloric acid (which can easily penetrate through PFA) at 80°C for 300 hours, then extracted substances were analyzed. Extracted Substances (Concentration) Si: 700 ng/ml, S: 1,000 ng/ml, ...

  • マニュアル

    ... Carrier was soaked in concentrated hydrochloric acid (which can easily penetrate through PFA) at 80_C for 300 hours, then extracted substances were analyzed. • Extracted Substances (Concentration) Si . . . . . 700 ng/ml S . . . . . 1000 ng/ml ...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . 23 Section RS-232C Communications Errors 5-1 5-4 Connection Errors Problem The indicator e POWER O d ca o iss not o lit. Probable cause The Power Supply is not connected properly. The supply voltage is not 24 VDC +10%/–15%. The measurement results do not appear on the Video Monitor. The F400 is not in Monitor or Run mode. The e Video deo Monitor o o iss blank. ba The power to the Video Monitor is not ON. The Monitor Cable is not connected properly. The Video Monitor is malfunctioning. Cannot make key inputs from the...

  • マニュアル

    ... to the Camera. The Camera Cable is not properly connected. The lens diaphragm is opened or closed too far. The shutter speed is not suitable. The lighting method is not suitable. The indicators do not turn ON (for Cameras Source). ...