全 2436 件が検索されました。(921 - 940件を表示)
- マニュアル
... the Unit or the Unit may malfunction. • With the CJ1W-SPU01-V2, do not connect anything other than a UPS to the COMM port. Doing so may inadvertently shut down the SYSMAC SPU Unit. • Before using FTP communications, use the CONFIRM FTP CONNECTION command (command ...
- マニュアル
.... • With the CJ1W-SPU01-V2 SYSMAC SPU Unit, do not connect anything other than a UPS connection to the COMM port. Doing so may inadvertently shut down the SYSMAC SPU Unit. • Before sending or receiving data using FTP, use the CONFIRM FTP CONNECTION command (command ...
- マニュアル
...してから制御してください。 READ/WRITE 21−動作表示灯コネクタ 320 ■入出力回路図 ■上位機器の制御について RUN 61.75 4-スイッチ 調整ドライバ 1個 付属品 ▲ ●警告表示 74.8 71.8 65.75 ビニール絶縁丸形コード Φ9 (7/Φ0.2)23芯 次のような場所では使用お...
- マニュアル
...36 and 37 38 and 39 40 and 41 42 and 43 44 and 45 46 and 47 48 and 49 50 and 51 52 and 53 54 and 55 56 and 57 58 and 59 60 and 61 62 and 63 18 Unit #15 Unit #16 Unit #17 Unit #18 Unit #19 Unit #20 Unit #21 Unit #22 Unit #23 Unit #24 Unit #25 Unit #26 Unit #27 Unit #28 Unit #29 Unit #30 Unit #31 Unit #8 Unit #4 Unit #2 Unit #9 Unit #10 Unit #5 Unit #11 Unit #12 Unit #6 Unit #13 Unit #14 Unit #...
- マニュアル
... is decreased just before the designated position. 4. The motor is stopped, taking the distance the motor moves by inertia into consideration. 5. The brake is turned ON immediately before the designated position. 6. The cutter is activated at the designated position. ...
- マニュアル
...Bit 3 Bit 2 Bit 1 Bit 0 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0 CM* CM* restart error bit flag RM* restart bit SR Wd 61 RM* error flag * RM: Rack-mounting Host Link Unit CM: CPU-mounting Host Link Unit C1000H and C2000H SR Wd 253 SR Wd 252 Bit 15 Bit 14 Bit 13 Bit 12 Bit 11 Bit 10 Bit 9 Bit 8 CM* CM* restart error bit flag RM* restart bit RM* #1 error flag RM* #0 error flag * RM: Rack-mounting Host Link Unit CM: CPU-mounting Host Link ...
- マニュアル
... wrong data, or you want to change the data, press the DATA key and repeat the procedure. If the Read command is subsequently used to read data to the same data area, the set data will be changed to the value read by the Read command. ...
- マニュアル
... is the default port. INPUT$ Function Purpose: To Read a string of characters from the keyboard or from a peripheral device Format: INPUT$ (
[,# ]) is the number of characters to be input. must be from 1 to 255. ... - マニュアル
... activated. Test stopped. 111 2 Data link activated. Data link stopped. 58 3 Operating level 0 Operating level 1 38 41 For maintenance use only. Leave this switch set to OFF. --- 5 38 61 PC enters MONITOR mode at PC enters usual mode at start-up. start-up. Not used. Leave this switch set to OFF. 72 Network Parameters initialized. 40 82 Polled unit Network Parameters not initialized. Polling unit --- 39 1. Pins 4 and 6 should always be OFF. 2. Pins 7 and 8 are normally OFF. 2-5-3 C200HW-SLK13/14/23/24 DIP Switches 1 ...
- マニュアル
.... . . . . . . . . . . 59 Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 vii About this Manual: This manual describes the installation and operation of the C200H-CP114 Cam Positioner Unit and includes the sections described below. Also briefly described is the basic operation and installation of the C200H–DSC01 Data Setting Console. Please read this manual carefully and be sure you understand the information provided before attempting to install and operate the Temperature Control Unit and Data Setting Console. Section 1 provides Cam Positioner Unit features and describes its basic system configuration. Section 2 provides information on the connections and settings of the Cam Positioner Unit. Section ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 62 Appendices A Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 65 B Sensor Temperature Measurement Ranges . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 67 C Heater Burnout Detection . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 69 D Dimensions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 73 Index. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 75 Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 77 vii About this Manual: This manual describes the installation and operation of the C200H-TC@@@ Temperature Control Units and includes the sections described below. Also briefly described is the basic operation and installation of the C200H-DSC01 Data Setting Console. Please read this manual carefully and be sure you understand the information provided before attempting to install and operate a Temperature Control Unit or Data Setting Console. Section 1 provides Temperature Control Unit features ...
- マニュアル
....。 .。 .。 。 .。 。 ..。 ◆。 .。 ..◆◆。 .。 ◆。 .。 。 。 .。 。 .。 。 .。 。 。 ..。 RevisionHistory.......….・・.◆・・・…...........◆ 4且23 56710 920212頒 1 35 36 43 43 53 57 59 61 65 67 69 71 Vii ---------------------[End of Page 1340]--------------------- ---------------------[End of Page 1341]--------------------- AboutthisManua∫: ThismanuaidescribestheinstaliationandoperationoftheC200H-TV口口口Heat/CoolTemperature ControlUnitandincludesthesectionsdescribedbelow.Alsobrieflydescribedisthebasicoperationand installationoftheC200H・DSCOIDataSettingConsole. Pleasereadthismanualcarefullyandbesureyouunderstandtheinformationprovidedbeforeattempting toinstallandoperatetheHeat/CoolTemperatureControlUnitandDataSettingConsole. SectionlprovidesHeaVCoolTemperatureContro│Unitfeaturesanddescribesitsbasicsystemconfiguration. Sθctlon2providesinformationontheconnectionsandsettjngsoftheHeat/CoolTemperatureControl Unit. Sectlon3providesthebasicoperatingprocedureseftheDataSettingConsoieincludingparametersettingsanddisplays. Section4providestheC200HPC'smemoryallocationiortheHeat/CoolTemperatureControlUnit.Basic programmingproceduresandexamplesarealsoprovided. SecttonsprovidespOssibleerrorsanderrorremedies. ThefiveAppendlcesprovidereferencesdealingwithspecificatiens,sensortemperaturemeasurement ranges,heaterbumoutdetection,anddimensions,andatableofDataSettingConsolekeyoperations. WARMNGFailuretoreadandunderstandthejnformationprovided▲nthismanualmay.resultin personalinjuryordeath,damagetotheproduct,orproductfailure.Pleasereadeach sectioninitsentiretyandbesureyouunderstandtheinformationprovidedintheseCtion andrelatedsectionsbeforeattemptinganyoftheproceduresoroperationsgiven. ix ---------------------[End of Page 1342]--------------------- ---------------------[End of Page 1343]--------------------- SECTKONl SystemConfigurationandFeatures Thiss㏄tionprov量desHeaぴCoolTemperatureControlUnitfeatUresanddescribesitSbasicsystemconfiguratien. 1-1Features 1-2BasicSyszemConfiguration (∠3 1 ---------------------[End of Page 1344]---------------------...
- マニュアル
.... . . . . 59 Index. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 63 vii TABLE OF CONTENTS viii About this Manual: This manual describes the installation and operation of the C200H-PID0@ PID Control Unit and includes the sections described below. Also briefly described is the basic operation and installation of the C200H-DSC01 Data Setting Console. Please read this manual carefully and be sure you understand the information provided before attempting to install and operate the C200H-PID0@ PID Control Unit and Data Setting Console. Section 1 provides PID Control Unit features and describes its basic system configuration. Section 2 provides information on the connections ...
- マニュアル
...22 25 26 28 30 32 32 33 37 39 40 40 40 42 42 42 43 44 44 48 52 52 57 59 60 61 62 62 68 69 70 71 77 78 80 82 83 83 85 86 21 Section 2-1 Network Configuration Overview 2-1 2-1-1 Network Configuration Overview Network Configuration The DeviceNet Network can be configured as shown in the following diagrams. Network with General-purpose Slaves Only Connect terminators at both ends of the trunk line. Ground to 100 Ω or less. Trunk line T T T-branch Tap 24 VDC T T-...
- マニュアル
...17 18 19 24 25 27 30 31 31 32 33 33 33 39 47 48 48 49 51 52 53 56 58 59 60 61 vii TABLE OF CONTENTS 3-2-1 3-2-2 3-2-3 Power Supply Wiring . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Standard I/O Unit Wiring . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Electrical Noise . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 4 Programming Console Operation . . . . . . . . . . . . . . . . . . . 4-1 4-2 Using the Programming Console . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-1-1 Nomenclature . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-1-2 Connecting the Programming Console . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Checking Initial Operation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 5 Troubleshooting, Inspections, and Maintenance . . . . . . . 5-1 5-2 5-3 5-4 Troubleshooting . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Inspection and Maintenance . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-2-1 Replacing Output Unit ...
- マニュアル
...39 40 41 42 43 44 45 46 47 48 AR 11 AR 15 49 50 51 52 53 54 55 56 57 58 59 60 61 62 * ** *Communication Controller Error Flag **EEPROM Error Flag 52 06 07 08 11 12 13 14 15 Section 3-5 AR (Auxiliary Relay) Area 3-5-8 SYSMAC LINK/SYSMAC NET Link System Service Time AR 16 provides the time allocated to servicing operating level 0 of the SYSMAC LINK System and/or SYSMAC NET Link System during each cycle when a SYSMAC LINK Unit and/or SYSMAC NET Link Unit is mounted ...
- マニュアル
...+1 Number of send data words (Undefined) Offset Unit No. Contents (data format) Data +0 Number of send data words (4 digits BCD) 0002 (fixed) +1 Unit No. (2 digits BCD) 00 to 31 61 Appendix A E5jK Digital Controller Read Protocol Receive Data Word Allocation (3rd Operand of PMCR) Receive data storage words +0 Number of receive data words +1 Set point during SP ramp Offset Contents (data format) Data +0 Number of receive data words (4 digits BCD) 0002 +1 Set point during SP ramp (4 digits BCD) Set point lower limit to upper limit Read MV (...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 44 44 47 51 53 59 61 62 62 62 63 64 67 69 70 vii TABLE OF CONTENTS 6-2 6-3 6-4 6-5 6-6 Selecting the Data Exchange Method . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Details of the Data Exchange Methods . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Data Exchange Time Charts . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . IOWR/IORD Instruction Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Restrictions for CS1-series PCs. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 74 75 87 95 108 SECTION 7 Editing BASIC Programs . . . . . . . . . . . . . . . . . . . . . . . . . 111 7-1 7-2 7-3 7-4 7-5 7-6 7-7 7-8 Programming Procedure . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Character Variable Space Allocations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Starting/Stopping the BASIC Program . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Program Configuration . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . List of BASIC Commands. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . BASIC Commands . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ....
- マニュアル
...Model External appearance Installation devices PLC Max No. of Units per PLC Section 1-2 Specifications CQM1H-CLK21 CVM1-CLK21 None required. None required. CVM1 and CV-series PLCs 4 maximum CQM1H-CPU51/...
- マニュアル
...m+54, m+55 00 to 15 Counter preset value 2 m+56, m+57 00 to 15 Counter preset value 3 m+58, m+59 00 to 15 Counter preset value 4 m+60, m+61 00 to 15 Counter preset value 5 m+62, m+63 00 to 15 Counter preset value 6 m+64, m+65 00 to 15 Counter preset value 7 m+66, m+67 00 to 15 Counter preset value 8 m+68, m+69 00 to 15 Counter preset value 9 m+70, m+71 00 to 15 Counter preset value 10 m+...