全 2436 件が検索されました。(941 - 960件を表示)
- マニュアル
.... This area is referred to only once when power is supplied to the MC Unit or when the MC Unit restarts. Words PC to MC n n+1 Outline Specification of Expansion DM Area First word of Expansion DM Area ...
- マニュアル
...0002 7890 3456 0002 5678 1234 0002 5432 B876 0003 3456 0012 0002 2100 0543 Means 345678.90 Means 123456.78 Means –387654.32 Means 123.456 Means 54321.00 61 IOWR Instruction Section 4-9 The acceleration time of the X axis is changed to 500 ms. Example 2 Execution condition DIFU(13) R1 R1 Work bit R3 Set in the Set in the DM expansion expansion area the DM area the data positioning positioningindata described the described below. following. R2 Set the address of the acceleration time of the X axis. IOWR #4406 Set the first source word ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 60 60 60 61 62 62 62 64 68 71 71 72 72 72 73 73 74 75 75 77 59 Section Startup Procedure 5-1 5-1 Startup Procedure 5-1-1 Flowchart for Configuring and Checking the System Check the following items when configuring the system. Slave Unit SRM1 CompoBus/S transmission line wiring Power supply connection Node number setting SRM1 startup CompoBus/S communications mode setting I/O device connections End No. 1 Items to check CompoBus/S transmission line wiring Contents Is the CompoBus/S transmission cable securely connected, and with no loose terminal screws?...
- マニュアル
...14 21 22 22 24 25 26 30 34 36 37 39 42 44 46 48 50 51 53 54 56 57 59 60 60 61 61 62 vii TABLE OF CONTENTS SECTION 7 Managing and Printing Files . . . . . . . . . . . . . . . . . . . . . . . 7-1 7-2 Deleting Files . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Printing Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 63 64 65 Appendix Error Messages and Troubleshooting . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . viii 67 69 71 About this Manual: This manual describes the installation and operation of the SYSMAC-NCT Support Tool and includes the sections described below. Please read this manual carefully and be sure you understand the information provided before attempting to install ...
- マニュアル
... EEPROM). Otherwise, illegal data may be written in the Unit’s EEPROM and “Special I/O Unit Errors” may occur when the power supply is turned ON or when the Unit is restarted, causing a malfunction. Note The EEPROM can be overwritten 50,000 times. ...
- マニュアル
... (NC213), Z axis m+60 and U axis m+84 (NC413) 15 00 x103 x102 x101 x100 Setting Range: 0 to 9,999 (pulses) Backlash Compensation Speed X axis m+13 (NC113), Y axis m+37 (NC213), Z axis m+61 and U axis m+85 (NC413) 15 14 13 x103 Factor 12 00 x102 x101 x100 Factor: 00: x1, 01: x10, 10: x100, 11: x1,000 (pps) Acceleration/Deceleration Curves X axis m+14 (NC113), Y axis m+38 (NC213), Z axis m+62 and U axis m+86 (NC413) 15 00 0 0 0 Designation Designation: 0: ...
- マニュアル
...*E00010 *EM_ EM_/EXT Number @E0_00010 000202 TIM SV @E0_00010 Binary Current bank SHIFT *EM WR/LR SHIFT *EM WR/LR Number E00010 000202 TIM SV @E00010 61 Section 4-1 Inputting Instructions • In BCD mode, indirect DM/EM addresses can be specified from D00000 to D09999 and E00000 to E09999. Use binary mode to specify D10000 to D32767 and E10000 to E32767. • If 8000 to FFFF Hex are specified as indirect DM addresses in binary mode, E00000 to E32767 in bank 0 of the EM Area will be designated. • If 8000 to FFFF Hex are specified ...
- マニュアル
... set the local IP address as follows: Set the local IP address in the CPU Bus Unit System Setup when making other settings in the CPU Bus Unit System Setup (i.e., the default settings are not used). The settings are made with CX-Programmer. ...
- マニュアル
...0 0 0 0 0 0 1 1 0 1 2 : : : : 1 1 1 1 1 1 1 1 0 1 1 0 61 62 1 1 1 1 1 1 63 0: OFF, 1: ON Note 1. Refer to Appendix A Node Address Settings Table for a complete table of DIP switch settings. 2. The Slave won’t be able to participate in communications if the same node address is used for the Master or another Slave node (node address duplication error). Baud Rate Setting Pins 7 and 8 are used to set the baud rate as shown in ...
- マニュアル
...#2 #1 32 outputs 4-point 16 inputs Analog Output Unit Output area Input area CIO 355 32 output bits for Unit #0 CIO 356 CIO 57 CIO 58 CIO 59 CIO 60 CIO 61 CIO 360 Unused CIO 63 CIO 64 CIO 65 CIO 66 (See note 1.) CIO 361 CIO 362 4 analog outputs for Unit #1 16 output bits for Unit #2 I/O Unit interface status for node number 05 CIO 357 16 input bits for Unit #2 CIO 358 16 input bits for Unit #3 CIO 359 Unused 4 analog outputs for Unit #1...
- マニュアル
... Units can also be connected. If an Expansion I/O Block is used, a maximum of 16 Units can be connected. (See 1-2-1 Basic Configuration.) Note 1. The CQM1H is mounted to DIN Track. 2. Only the CQM1H-CPU51/...
- マニュアル
...14 13 12 11 10 +3 32 31 30 29 28 27 26 25 24 23 22 21 20 19 18 17 +4 48 47 46 45 44 43 42 41 40 39 38 37 36 35 34 33 +5 Note - - 62 61 60 59 58 57 56 55 54 53 52 51 50 49 Even if the local node is disconnected from the network, only the bit corresponding to the local node is turned OFF (i.e., the entire status area participating in the network is not turned OFF). While the local node is disconnected, the bits corresponding to ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 SECTION 2 Individual Unit Descriptions for CS Series . . . . . . . . . . . . . . . 67 2-1 CS1W-PTS01-V1 Isolated-type Thermocouple Input Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . 68 2-2 CS1W-PTS11 Isolated-type Thermocouple Input Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 80 2-3 CS1W-PTS51 Isolated-type Thermocouple Input Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 97 2-4 CS1W-PTS55 Isolated-type Thermocouple Input Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 109 2-5 CS1W-PTS02 Isolated-type Resistance Thermometer Input Unit (Pt100 or JPt100). . . . . . . . . 121 2-6 CS1W-PTS03 Isolated-type Resistance Thermometer Input Unit (Ni508.4) . . . . . . . . . . . . . . . 132 2-7 CS1W-PTS12 Isolated-type Resistance Thermometer Input Unit (Pt100, JPt100, Pt50, Ni508.4) 142 2-8 CS1W-PTS52 Isolated-...
- マニュアル
.... . . . 60 3-2-2 CS1 and CS1-H PLCs . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 3-2-3 CS1D PLCs . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 62 Optical Wiring . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 63 3-3-1 Optical Fiber Cable Connections for H-PCF Cable. . . . . . . . . . . . . 63 3-3-2 Optical Fiber Cable Connections for GI Cable . . . . . . . . . . . . . . . . 65 3-3-3 Backup Power Supply Wiring . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 67 3-3-4 Connecting Optical Fiber Cable to Connectors for H-PCF Cable . . 68 3-3-5 Connecting Optical Fiber Cable to Connectors for GI Cable . . . . . 70 3-3-6 Connecting Backup Power Supply Cables. . . . . . . . . . . . . . . . . . . . 73 47 Section 3-1 Component Names and Functions 3-1 Component Names and ...
- マニュアル
... Box for the Project Workspace level. When an LCU or LCB element is selected, function block group, or function block is selected Function Block Reference Displays the reference help for the selected function block. When a function block is selected ...
- マニュアル
... function block database error) is stored on the Loop Control Unit. Note If pin 2 of the DIP switch is ON, flash memory contents will be automatically transferred to RAM at startup, bit 5 of word n will be ON, and ITEM 095 of the ...
- マニュアル
...output Parameter 095 Host display of 0, 1 0 Yes R/W(O) R/W W R/W S/R 1 MVL(Auto/Manual switch : Auto, Manual) or Manual MVL (Auto/Manual switch : Manual) 61 2 Control blocks <002> 3-position ON/OFF 001 to 032 Data for host display *1:On the CX-Process Monitor, the R/W mode is indicated in the Tuning screen or in the Control screen. COLD R/W Mode start R: Read, W: Write, R/W: R/W-enabled, initializ -: R/W-disabled ation Note: r and r/w: Read and read/write for ...
- マニュアル
... Relay Units and 2 PCU Connecting Cables are required. • When using in combination with the CS1W-NC213/NC233 (2-axis control), 2 Servo Drive Connecting Cables are required. • When using in combination with the CS1W-NC413/NC433 (4-axis control), 4 Servo Drive Connecting Cables are required. ...
- マニュアル
...INT(89) (Mask) INT(89) (Read mask) INT(89) (Clear) Minimum pulse width Count mode CPM2C-S Incrementing counter Decrementing counter 2 kHz Contains counter PV. Read SR 244 to SR 247. Execute PRV(62). Execute INI(...
- マニュアル
... pins 40 pins XW2B-40G4 XW2D-40C6 Size Miniature Standard Standard Miniature The recommended size for cable wires is AWG 24 to 26 (0.2 to 0.13 mm2). Use a cable with an outer diameter of less than 1.61...