全 2268 件が検索されました。(781 - 800件を表示)

  • マニュアル

    ... the following types of input can be used: thermocouple, platinum resistance thermometer, infrared sensor, analog voltage, or analog current. • Either standard or heating/cooling control can be performed. • Both auto-tuning and self-tuning are supported. • Event inputs can be used to switch set points (multi-...

  • マニュアル

    ... long The command is too long. 2203 Operation error EEPROM error 2.3 Detailed Description of the Services ■ Operation Command This service performs operations such as run/stop, communications writing, write mode, save RAM data, AT (auto-tuning) execution/cancel, multi-...

  • マニュアル

    ... the information being provided applies to all E5CSV and E5CS-U Digital Temperature Controllers. Meanings of Abbreviations The following abbreviations are used in parameter names, figures and in text explanations. These abbreviations mean the following: Symbol Term PV Process value ...

  • マニュアル

    ... in parameter names, figures and in text explanations. These abbreviations mean the following: Symbol TC4/TC2 Term Four-channel and Two-channel Basic Units CH HFU Channel Advanced Unit EDU PV End Unit Process value ...

  • マニュアル

    ... except for function blocks. xvii Meanings of Abbreviations and Terms The following abbreviations and terms are used in this manual. Abbreviation or term AT EDU EU HB HS LBA LSP OC PV RSP SP TC4/TC2 Temperature Controller Configurator Meaning Autotuning EJ1 End Unit Engineering unit (See note.) Heater burnout Heater short Loop burn alarm Local ...

  • マニュアル

    ... the following types of input can be used: thermocouple, platinum resistance thermometer, infrared sensor, analog voltage, or analog current. • Either standard or heating/cooling control can be performed. • Both auto-tuning and self-tuning are supported. • Event inputs can be used to switch set points (multi-...

  • マニュアル

    ...-18 Name Description 1001 Command too long The command is too long. 2203 Operation error EEPROM error 2.3 Detailed Description of the Services ■ Operation Command This service performs operations such as the following: • RUN/STOP • Multi-...

  • マニュアル

    ... (ST): Indicates the Self-tuning parameter. ←Default setting is on (ON): Enabled. Change the set value with the Keys. (Up and Down) You cannot set the following parameters while self-tuning is enabled. • Adjustment Level: MV Upper Limit, MV Lower Limit, and ...

  • マニュアル

    ... communications.) • User calibration of the sensor input is supported. • User calibration of transfer output is supported. (Applicable to E5CN-HT, E5AN-HT, and E5EN-HT models with transfer outputs.) • Use position-proportional control. (Applicable to the E5AN-HT and E5ENHT.) • Use a remote ...

  • マニュアル

    ... Command This service performs operations such as the following: • Run/Reset • AT Execute/Cancel • Write Mode • Save RAM Data • Software Reset • Move to Setup Area 1 • Move to Protect Level • Auto/Manual Switch • Parameter Initialization • Alarm Latch Cancel • ...

  • マニュアル

    ... on parameters (“Function,” “Setting,” “Monitor,” and “Reference”) are explained in Section 8 Parameters. ● Abbreviations Abbreviations used in the parameters, illustrations, and text are listed in the following table. Abbreviation Meaning Abbreviation Meaning PV Present value ch Channel ...

  • マニュアル

    ...】 ー,M`、ーーコ]」 §,,づ ● ---------------------[End of Page 4269]--------------------- 一圃ControlCircuitTerminals ●lnputTe『minals Termlna】 symbol S1 SC Nameanddescrlptlon Multl・functloninput(seenotesland2) Multlヰunotlo川nputcommon lnputcemmonforS1 lntertace -C ...

  • マニュアル

    ...Chapter5 5図4 M◎nit◎rFunc輔on HAILA,U「r,UE SelectingtheServoDriverfromthescreenautomaticailydisplaystheMonitorDisplay screen.Thefollowingexplainshowtousethefourscreens(onlinemode).Forinformationoneachmonitor,refertotheappropriateproductoperationmanual. ≡輪∩itorPararDeterAlam Sモatus㎞置or 8aseBi◎dく ForwardOvertravel Re∨erse〔トvertravel AIam hainP㈱r ...

  • マニュアル

    ...circuit is malfunctioning. Short-phase input (SPI) The DC voltage of the main circuit fluctuates excessively while the Inverter is not affected by regenerative energy. (The input phase loss detection level and time are set with n080 and n081.) ...

  • マニュアル

    ...). Set by constant n036 (external error a). Set by constant n037 (error reset). Set by constant n038 (multi-step speed reference 1). S6 Multi-function input 5 (S6) Set by constant n039 (multi-step speed reference 2). SC SS ...

  • マニュアル

    ... 22 kW or More 1-10 3 1 U/T1 V/T2 W/T3 Confirmations upon Delivery nTerminal Arrangement for European Models Views with the terminal cover removed are shown in Figs. 1.7 and 1.8. SN SC SP A1 A2 +V AC -V MP AC RP R+ RE(G) S1 S2 S3 S4 S5 S6 S7 FM AC AM IG S+ S- M5 M6 MA MB MC M3 M4 M1 M2 E(G) Control circuit terminals Main circuit terminals Charge indicator Ground terminal Fig 1.7 18.5 kW or Less Control circuit terminals Charge indicator Main ...

  • マニュアル

    ...: PIDC (PID integral reset) 27: UP (UP/DWN function accelerated) 28: DWN (UP/DWN function decelerated) 29: UDC (UP/DWN function data clear) 31: OPE (forced operator) 50: ADD (frequency addition) 51: F-TM (forced terminal block) 52: RDY (ready function) 53: ...

  • マニュアル

    ...: PIDC (PID integral reset) 27: UP (UP/DWN function accelerated) 28: DWN (UP/DWN function decelerated) 29: UDC (UP/DWN function data clear) 31: OPE (forced operator) 50: ADD (frequency addition) 51: F-TM (forced terminal block) 52: RDY (ready function) 53: ...

  • マニュアル

    ...-3 Names of Parts and Functions Features and System Configuration 1 1-3 Names of Parts and Functions Servo Drive Part Names Display area Unit No. switch Settings area Analog monitor 1 check pin (IM) Analog monitor 2 check pin (...

  • マニュアル

    ... 8 0 1 2 3 Features and System Configuration 1-3 Names of Parts and Functions 4 5 6 1 X10 COM X1 MECHATROLINK-II communications status LED indicator RS-232 Analog monitor check pins (SP, IM, G) SP IM G communications connector (CN3) MECHATROLINK-II communications connector (CN6A, CN6B) Main-circuit power terminals (L1, L2, L3) Control-circuit power terminals (L1C, L2C) External Regeneration Resistor connection terminals (B1, B2, B3) Control I/O connector (CN1) Servomotor connection terminals (U, V, W) Protective ground terminals 1-3 Encoder connector (CN2) 1-3 Names of Parts and Functions 1  ...