全 2268 件が検索されました。(761 - 780件を表示)

  • マニュアル

    ...Outputunit Insta{lthisonthesecketsinsidethemaiR unit、SeieCttheouゆutun睡ma言ch8dto theoutputspec浦ca60n. tThisisalreadyinstail轡donposltionproponionalcontro‖ers{ESIOOX・RRP〔〕・・口). 重一3 ---------------------[End of Page 9054]--------------------- ■F『ontpanei No.1display DisplaysparametersymbolswhensettingParameters.Duringsettingofparameters,the PVandSPLEDsdenotlight. Displaystheprocessvalue(PV)orthesetpoint(...

  • マニュアル

    ...(CA) 0017 Analogusefbuf允r3 0018 Analoguserbuf允r4 0019 Analoguserbuf允r5 001A Analoguserbuf飴r6 001B Analoguserbuffer7 001C Anal◎guserbuffer8 0029 Ana夏oginpu杜 002A Anabginp成2 0033 SP 0034 LocalSP 0035 FixedSP 0036 Deviation 0037 PIDmξmipulatedvariable Numerlcal Read◎嬢y 0038 Secondary夏oopSP va1埠 0039 SecondaryloOP費xedSP 003A Secondaryloopdeviation 003B ManualMV 003C Manipulatedvariable 003D Vaiveope血9Posltion 003E ValveOpeningf6rcontrol 003F Heatercurr頗t 0000 ...

  • マニュアル

    ... for your purchase of your E5CK compact, intelligent digital controller. The E5CK allows the user to carry out the following: • Select from many types of temperature and analog input (multiple input) • Select output functions such as control output or alarm (output assignment) • Use two setpoints (multi-...

  • マニュアル

    ... from many types of temperature and analog input (multiple input) • Support position-proportional control (position-proportional type controllers only). • Select output functions such as control output or alarm (output assignment) • Use the HBA (heater burnout alarm) function (standard type controllers only). • Use four setpoints (multi-...

  • マニュアル

    ... from many types of temperature and analog input (multiple input) • Support position-proportional control (position-proportional type controllers only). • Select output functions such as control output or alarm (output assignment) • Use the HBA (heater burnout alarm) function (standard type controllers only). • Use four setpoints (multi-...

  • マニュアル

    ...on the front cover. I E5AK Conventions Used in This Manual J Meanings of Abbreviations Sometimes the following abbreviations are used in parameter names, figures and in text explanations. These abbreviations mean the following: Symbol Term PV Process value ...

  • マニュアル

    ...on the front cover. I E5EK Conventions Used in This Manual J Meanings of Abbreviations Sometimes the following abbreviations are used in parameter names, figures and in text explanations. These abbreviations mean the following: Symbol Term PV Process value ...

  • マニュアル

    ... the front cover. I E5CK Conventions Used in This Manual JMeanings of Abbreviations Sometimes the following abbreviations are used in parameter names, figures and in text exĆ planations. These abbreviations mean the following: Symbol Term PV Process value ...

  • マニュアル

    ...function is abbreviated to E5EK-DRT. • Use the CompoBus/D (DeviceNet) for communications. • Select from many types of temperature and analog input (multiple input) • Select output functions such as control output or alarm (output assignment) • Use the HBA (heater burnout alarm) function. • Use remote ...

  • マニュアル

    ...Indicates lists of one sort or another, such as procedures, checklists, etc. v Conventions Used in This Manual Meanings of Abbreviations The following abbreviations are used in parameter names, figures and in text explanations. These abbreviations mean the following: Symbol PV ...

  • マニュアル

    ... affect the performance of the E5GN. IV E5GN Conventions Used in This Manual JMeanings of Abbreviations The following abbreviations are used in parameter names, figures and in text explanations. These abbreviations mean the following: Symbol Term PV Process value ...

  • マニュアル

    ... status of the controller. 08 01 Echoback test This service carries out the echoback test. 30 05 Operation instructions This service carries out run/stop, communications writing, write mode, save RAM data, AT (auto-tuning) execution/cancel, multi-...

  • マニュアル

    ... adversely affect the performance of the E5EN. IV Conventions Used in This Manual J Meanings of Abbreviations The following abbreviations are used in parameter names, figures and in text explanations. These abbreviations mean the following: Symbol Term PV Process value ...

  • マニュアル

    ...ately turn the E5AN OFF. IV E5AN Conventions Used in This Manual JMeanings of Abbreviations The following abbreviations are used in parameter names, figures and in text explanations. These abbreviations mean the following: Symbol Term PV Process value ...

  • マニュアル

    ...for errors or omissions. Neither is any liability assumed for damages resulting from the use of the information contained in this publication. v Abbreviations The following table lists the main abbreviations used in parameters, diagrams, and in the text itself. Abbreviation PV ...

  • マニュアル

    ...andsom餐…operatinginstructions. Thesefunction$aiiowsyoutousetherequiredc◎ntrdparametersor cOntrd◎peratinginstructionswhile¢h白CkingC◎ntrolstatuS◎nscreenwhite theprograrn(bank)isrしmning. ●Trendgr劉ph Changesinthscurrentpr◎cessvalue(PV)andrnanipulatedvariable{M∨) canbemonitor白donES∫TO◎LSingraphs.Thesegraphsareca‖ed"trend 9「aphs." Fivedataitems(e.g.PV,...

  • マニュアル

    ... IN Area is divided into two areas, however, the total number of words that can be used for the IN Area is still 100 words (200 bytes). CPU Unit DeviceNet Unit Remote I/O communications output area PLC Unit 0, Ch 1 ...

  • マニュアル

    ... communications with the default data allocation parameters. 1-3 Overview Section 1-1 Features Section 1-1 Features Overview Note The Communications Write setting is ON by default. Master Write Area Write data Output Enable Bit ...

  • マニュアル

    ... the following types of input can be used: thermocouple, platinum resistance thermometer, infrared sensor, analog voltage, or analog current. • Either standard or heating/cooling control can be performed. • Both auto-tuning and self-tuning are supported. • Event inputs can be used to switch set points (multi-...

  • マニュアル

    ... long The command is too long. 2203 Operation error EEPROM error 2.3 Detailed Description of the Services ■ Operation Command This service performs operations such as run/stop, communications writing, write mode, save RAM data, AT (auto-tuning) execution/cancel, multi-...