全 31668 件が検索されました。(781 - 800件を表示)

  • マニュアル

    ...│AlwaysO /TIM-\/OOOO、TlMH::CNT-:二CNTROO47 ` Dataarea, 口 IIllliWord lFCSl 口唱●X103×102×101×100 $1 一− CIO-_.IRarea HR-一._HRarea DM-一._DMarea CON,一・…Constant ResponseFormat 4-23F◎RCEDSET ForcedsetsabitinanIR,...

  • マニュアル

    ...butthat◎utputbitsandtimersareheld. 31 ---------------------[End of Page 8707]--------------------- ActionBlocks Seetion3■5 ActionsDefinedasBits lttheAQisN,thenthebitwillturnOFFatpOintA.IftheAQisNH,thenthebitwUl notturnOFFatpointAandstatuswillbehelduntiltheyaretumedOFFelsewhereintheprogram(eg.,usjnganactionwithanRAQ,asshownbelow). A ActivgstatUs 'Relay timer Non・he}dAQ HeldAQ Nl ・・` ;; =: ;】t' .' ...

  • マニュアル

    ... added to table. Page 13: Special I/O Units readable/writeable on Slave Racks corrected. Page 21: NC222 added to Slave Racks column of C500 Special I/O Units row. Page 27: Default communications settings changed and note added. Page 34: Descriptions of ...

  • マニュアル

    ... Configuration: PC Links Up to four PCs can be linked with a Link Adapter to increase the number of I/O points to 80 maximum. Although each PC still operates on its own program, no special programming is needed to transfer data between the PCs via ...

  • マニュアル

    ..."V:Compare"fromtheTransferDataLinkTablemenutostartcom・ paringthedatalinktables.Amessagewillflashduringthecomparisonand thefollowingdisplaywillappearwhenthecomparisoniscompiete.Unmatchingdataitemswillbedisplayedwiththedatainthecomputerρntop andthedataintheSYSMACNETLinkUnitunderneath. (》 ト』tLJレ:εりdr=【0〔Nヨ・】Nedee《tdv=【0{ヨ9】 一働囲■■■■固頭匿詞曲■田 Upper:Com晒◎wer:SVI' トピリ卓口ad《...

  • マニュアル

    ... CCL㈹ CCS㈹ MARK RεGL㈹ 曜GS㈹ Tracθ TRACE SELECT LOAD SAVE MARK LOAD SAVERE(キ ln6tructi加8 MEMORY DMBANK FLAGS FLAGS TRACE RεGISTεR lS正R Sp8c回 ln8tructbn8 同LR㈹ 剛w㈹ 臼LP㈹ FLSP㈹ IORF㈹ lOSP(旬 IORS IODP㈹ Flb R∈AD WRITE READ・ CHANGE uo DISABLε εNABLE VODIS・ Proc臼8ing DAIAFILE DATAFILE PROGRAM STEP RεFRESH ACCESS ACCESS PLAy In8tr"tbn8 FILE PROGRAM and REAO WRIT S酬D㈹ Rεcv㈹ CMND㈹ MSG㈹ ぬ READ〃O WRITEレO NETWORK NETWORK DEuVER MεSSAGE Proces副ng SEND RECεIVE COMMAND lnstωctbn8 Touτ SFC TRANSI・ Control TION 1nst...

  • マニュアル

    ...necessary. If the CVSS is not installed, the data are only displayed, and not saved. Command: L Function Loads (reads) a section of memory from a file on the memory card or from the port to which a terminal is connected. Syntax ...

  • マニュアル

    ...+1SHigh-orderbyte lslD }一悪blt15bi{s Sinle・recii◎nFl◎ain・oinVariable Singie-precisionfloating-pointvaluesarestoredinIEEE32-bjtformat: 70S:slgnbit(0:positive,1:negative) Elexponent(withl27effsets) +OLow-orderbyte Mlmantissa(withMSBalways1) +1 310 +2High-orderbyte,, .3-...コ }L-T-一−...

  • マニュアル

    ... 14 Bit 15 DM 0 0 0 0 digit value IR or SR 0 0 1 8 HR 0 1 0 4 AR 0 1 1 C LR 1 0 0 2 TC 1 0 1 A As an example, a value of C007 would specify AR 007 as the first input word. Input data for the second input would be contained in AR 008, and so on. Number of Outputs Bits IR 1n200 to IR 1n203 specify the number of outputs (results of fuzzy logic processing) that are read from the Unit. The number must be BCD, between ...

  • マニュアル

    ... #2 Node #4 Node #5 Node #3 Node #6 Node #7 Node #8 Node #4 Node #2 Section 5-3 Automatic Generation of Data Link Tables Note *When combining CV-series PCs in data links with C-series PCs, LR 00 to LR 63 in C-series PCs correspond to CIO 1000 to CIO 1063 in CV-series PCs and DM 0000 to DM 0127 correspond to D00000 to D00127. Data Flow This example shows data flow resulting from automatic generation with four PCs exchanging 16 Link Area words each. The DM Area words are not shown. Shading indicates ...

  • マニュアル

    ...ClOArea B'raddrθss Wbmladヒ「rθss 川nputlQ:Outputで Cou献erArea CNTCoびη∼erηびmbθr CNTCoαηrθmμmbθr C Constant(4-digit> . #,レ白1uθ # Constant(8-digit> CTRL+#,レa加θ # CPUBusLhkArea SHIFT+LR,B∫faddrθss SHIF了+...

  • マニュアル

    ...) Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . LR (Link Relay) Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Program Memory . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . TR (Temporary Relay) Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 4 Writing and Inputting the Program . . . . . . . . . . . . . . . . . 4-1 4-2 4-3 4-4 4-5 4-6 4-7 4-8 4-9 4-10 4-11 Basic Procedure . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Instruction Terminology . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Program Capacity . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Basic Ladder Diagrams . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . The Programming Console . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Preparation for Operation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Inputting, Modifying, and Checking the Program . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Controlling Bit Status . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Work Bits (Internal Relays) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Programming Precautions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Program Execution . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . vii TABLE OF CONTENTS SECTION 5 Instruction Set . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-1 5-2 5-3 5-4 5-5 5-6 5-7 5-8 5-9 5-...

  • マニュアル

    ... is the unit number set on the Unit. Allocation for Remote I/O Master and Link Units Remote Master I/O Units, SYSMAC LINK Units, SYSMAC NET Link Units, and Host Link Units do not use I/O words, and the PC Link Units use the ...

  • マニュアル

    ... (SR area) 192 bits (IR 24400 to IR 25515) Temporary bits (TR area) 8 bits (TR0 to TR7) Holding bits (HR area) 1,600 bits (HR 0000 to HR 9915) Auxiliary bits (AR area) 448 bits (AR0000 to AR 2715) Link bits (...

  • マニュアル

    ... PC being used. Refer to your PC’s operation manual for specific limits. 58 Memory Area Designations Memory area Data Section 3-2 Address used in communications Data area address 1st and 2nd bytes CIO area ...

  • マニュアル

    ... 1000 to DM 1021) HR area (HR 00 to HR 19) Counter area (CNT 000 to CNT 127) Flash memory User program Read-only DM area (DM 6144 to DM 6599) PC Setup (DM 6600 to DM 6655) 1. The IR, TR, LR, and timer areas are not normally backed up when power is turned OFF and all contents will be cleared the next time power is turned ON. (The PC Setup setting in DM 6601 can be used to back up this data. Refer to details on the PC Setup later in this manual for details.) 2. The ...

  • マニュアル

    ...) Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . LR (Link Relay) Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . UM Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . TR (Temporary Relay) Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 4 Writing and Inputting the Program . . . . . . . . . . . . . . . . . 4-1 4-2 4-3 4-4 4-5 4-6 4-7 4-8 4-9 4-10 4-11 Basic Procedure . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Instruction Terminology . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Program Capacity . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Basic Ladder Diagrams . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . The Programming Console . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Preparation for Operation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Inputting, Modifying, and Checking the Program . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Controlling Bit Status . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Work Bits (Internal Relays) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Programming Precautions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Program Execution . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . vii TABLE OF CONTENTS SECTION 5 Instruction Set . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-1 5-2 5-3 5-4 5-5 5-6 5-7 5-8 5-9 5-...

  • マニュアル

    ... possible using the RS-232C connector built into the C200HS-CPU21-E/CPU21-EC/CPU23-E/CPU31-E/CPU33-E CPU. By using the TXD and RXD instructions, RS-232C communications is possible without using time-consuming procedures. A 1-to-1 link using the ...

  • マニュアル

    ... 252 HR AR HR 00 to HR 94 AR 00 to AR 22 HR 00 to HR 99 AR 00 to AR 27 HR 00 to HR 99 AR 00 to AR 27 LF Timer/ Counter DM LR 00 to LR 58 --- LR 00 to LR 63 TIM/CNT 000 to 511 LR 00 to LR 63 --- DM 0000 to DM 6138 DM 0000 to DM 6655 DM 0000 to DM 6143 EM Indirectly addressed DM Indirectly addressed EM EM 0000 to EM 6138 EM 0000 to EM 6143 *DM 0000 to *DM 6655 EM 0000 to EM 6143...

  • マニュアル

    ... clear the display and cancel Programming Console operations. Key functions are described in detail in the next section. 3-3-1 The Keyboard Key FUN NOT SHIFT AND OR LD OUT TIM CNT DR LR CH * CONT Function Function Key Designates instructions via function codes or designates Programming Console functions. NOT Key Pressed after the Load, AND, or OR Key to designate a normally closed condition with the LOAD, AND, or OR instructions. Shift Key Designates the upper function on keys that have two functions. Used with the CH/* Key, the Bit/Constant Key, or Numeric Keys 0 through ...