全 31668 件が検索されました。(821 - 840件を表示)
- マニュアル
... to SR 25515 Same as CPM2C. HR (Holding Relay) area 320 bits: HR 0000 to HR 1915 AR (Auxiliary Relay) area 384 bits: AR 0000 to AR 2315 Same as CPM2C. 256 bits: AR 0000 to AR 1515 LR (Link Relay) area Same as CPM2C. Same as CPM2C. Timer/Counter area 256 bits: ...
- マニュアル
... on the Serial Communications Board. TXD(––) or RXD(––) instructions Bar–code reader 1:1 Data Link System Printer If two PCs are linked one-to-one by connecting them together through their RS-232C ports, they can share up to 64 words of ...
- マニュアル
...External device with RS-232C port RS-232C OR Data only 1-2-4 PC 1:1 Data Links Two PCs can be connected via RS-232C cable to create a data link between them of up to 64 words in the LR area. The link words written by one PC are automatically transferred to the other PC for reading. One of the following three ranges of words can be set to be linked: ...
- マニュアル
...: 1 CIO: 32 Wds, DM: 64 Wds Node 1 Node 2 Node 3 Node 2 Node 4 When using a data link that combines C-series SYSMAC LINK Units, CSseries SYSMAC LINK Units, and CVM1/CV-series SYSMAC LINK Units, LR 00 to ...
- マニュアル
... the use of communications programs on the PLC (CPU Unit) or IBM PC/AT or compatible computer. Data written in the send area of the local node will be automatically sent to the receive area of other nodes. The I/O area (CIO area), link area (...
- マニュアル
... to SR 25515 8 bits (TR0 to TR7) Holding bits (HR Area) Auxiliary bits (AR Area) 320 bits: HR 0000 to HR 1915 (Words HR 00 to HR 19) 384 bits: AR 0000 to AR 2315 (Words AR 00 to AR 23) Link bits (LR Area) Timers/Counters 256 bits: ...
- マニュアル
... input words and 32 output words) can be allocated to the DeviceNet Master’s I/O. The Master’s I/O can be allocated to the following data areas. IR 000 to IR 049 IR 200 to IR 227 DM 0000 to DM 2047 LR 00 to ...
- マニュアル
... DM Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . LR Area. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Difference between I/O Refreshing in Customizable Counter Units and That in Other Special I/O Units . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 5 Unit Setup Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-1 Unit Setup Area. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 60 63 67 71 72 77 78 vii TABLE OF CONTENTS SECTION 6 I/O Memory. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6-1 6-2 6-3 6-4 Overview . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Details . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SR Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . AR Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 85 86 89 93 98 SECTION 7 Special Functions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 119 7-1 7-2 7-3 7-4 7-5 7-6 7-7 7-8 7-9 7-10 7-11 7-12 7-13 7-14...
- マニュアル
... words) words x 1) 1,024 pts (32 input/32 output words) CQM1-DRT21 32 pts (1 input/1 output word) CS1W-DRM21(-V1) CJ1W-DRM21 C200HW-DRM21 CIO, WR, DM, EM, HR CQM1-DRT21 CIO CIO, DM, EM, AR, LR, T/C 5 Section 1-1 Overview of DeviceNet Message Communications Function [ CMND ... ] Master Master Special Slave Item Communications Instructions Master CS Series CJ Series CVM1, CV Series CS1W-DRM21(-V1) CJ1W-DRM21 DVM1-DRM21-V1 SEND(192) SEND(192) SEND(192) RECV(193) RECV(193) RECV(193) FINS commands CMND(194) CMND(194) CMND(194) CS Series,...
- マニュアル
...x 1) input/100 output words) 1,024 pts (32 input/32 output words) CQM1-DRT21 32 pts (1 input/1 output word) CS1W-DRM21(-V1) CJ1W-DRM21 C200HW-DRT21 CIO, WR, DM, EM, HR CIO, DM, EM, AR, LR, T/C CQM1-DRT21 CIO CS1W-DRM21(-V1) 7 Overview of DeviceNet Section 1-1 Message Communications Master Master RS-232C Interface Unit Communications Instructions Master CS Series CJ Series CVM1, CV Series CS Series, C200HX/HG/HE C200HS Item Max. No. of nodes per Master for message communications using FINS commands Max. No. of nodes per Master for message...
- マニュアル
...Automatic setting can be used to create simple data links. • Using a Programming Device (such as a Programming Console), set the automatic data link mode in the DM parameter area of the startup node. • Area 1 can be selected from bit areas (i.e., IR, CIO, and ...
- マニュアル
... AR 27 AR 0000 to AR 2715 These bits serve specific functions such as flags and control bits. TR Area 8 bits --- TR 0 to TR 7 These bits are used to temporarily store ON/OFF status at program branches. ...
- マニュアル
... data links can be created to automatically transfer large amounts of data as listed below. Item Number of send words per node Number of send and receive words per node Specifications 508 words max. (254 words max. in the CIO/...
- マニュアル
...Command mode DIO1 to DIO8 UNL TA LA Data mode A B C ... Delimiter DAV ATN UNL: Unlisten command TA: Talker address LA: Listener address 8 A, B, C ...: Data Delimiter: CR + LR, CR, etc. (selectable) Section 1-4 Comparison with other OMRON Units’ GP-IB Functions 1,2,3... 1. The Controller sets the ATN line to “L” and sends the UNL command. This command inactivates the connected GP-IB devices. 2. The Controller sends the TA (Talker address) and LA (Listener address). Two or more Listener addresses can be specified. This step determines the new Talker and Listener(...
- マニュアル
.... Custom - Select this button to make your own settings. Write: These setting are the same as Read, but without the option of selecting the 'AR' memory area. ♦ Area - This option defaults to IR area 1, but can be set to IR area 2, DM area, ...
- マニュアル
.... Custom - Select this button to make your own settings. Write: These setting are the same as Read, but without the option of selecting the 'AR' memory area. ¨ Area - This option defaults to IR area 1, but can be set to IR area 2, DM area, ...
- マニュアル
...CVM1-LK401 is the PC Link Unit for SYSMAC CVM1/CV-series PLCs. Exchange Data between PLCs without Programming Extra programming is not required to communicate through the PC Link System. PLCs with PC Link Units mounted can exchange data through their shared ...
- マニュアル
.... Custom - Select this button to make your own settings. Write: These setting are the same as Read, but without the option of selecting the 'AR' memory area. ♦ Area - This option defaults to IR area 1, but can be set to IR area 2, DM area, ...
- マニュアル
...shown in parentheses.) --- --- --- Not supported in function blocks TB: 1st stack address --- --- Not supported in function blocks D: Destination word --TB: 1st stack --address ----- D: Destination word --N: Table number # + decimal only ...
- マニュアル
.... (unit Ver. 1.2 or later) 12,000 words max. (pre-Ver. 1.2) C200HX/HG/HE, CVM1/CV, CQM1H: 8,000 words max. Personal computer: 32,000 or 62,000 words max. (See note 2.) Bit-access areas (IR, AR, LR, CIO), DM Area (DM), and extended DM Area (EM) 2,012 bytes max. (including the header) Polling node backup function Self-diagnosis function (hardware checking at startup) Echoback test and broadcast test (using the FINS command) Watchdog timer Error log function Note (1) At least one Repeater Unit (CS1W-RPT01) is required to construct networks that uses ...