全 31668 件が検索されました。(721 - 740件を表示)
- マニュアル
...渉防止機能付セ ンサを使用する (回帰反射形E3Z-R□□シ リ ーズな ど) • レ ーザ タ イ プのセ ンサを使用する(レーザ タ イ プE3Z-LR□シ リ ーズな ど) • 干渉源 と な る セ ンサ と の距離を離す • 干渉 し ないよ う に互いの光軸をず ら す (高 さ を変え る、 斜めに設置...
- マニュアル
... DC external and GR terminals: AC1000V 50/60Hz 1min. /Leak current: 10mA or less Between DC external and GR terminals: 20MΩ or more (Using a 500 VDC megger) UL508/CE/UKCA/C22.2 No.107.1-01 EN61000-6-4/FCC/ICES/RCM/KC ...
- マニュアル
...PT settings, displaying, 58 Transmit Mode, 53 troubleshooting, 68 R RS-232C connector, 9 RS-232C interface, 6 connector, 26 RS-422 interface, 7 80 W wiring ALM OUTPUT terminals, 25 HOST RUN INPUT terminals, 24 ...
- マニュアル
...,theycannotbeloadedwithdirectconnectionturnedOFFintheTool Settingsandcamotbeconvertedbackforusewith◎utdirectconnection. DisplaysontheFileSelectionDisplayandtheScreenSelectiondisplaywill indicatewhetherornotdirectconnectionhasbeenset.lfdirectconnectien hasbeenset,"-O"(forOMRON)wiltbeaddedafterthePTmodelnamefollowingthe"FileList"titieontheFileSelectionDisplay.Thehelpmessage areaontheScreenSelectionDispSaywillalsoindicatewhetherornotdirect connectionhasbeenusedtogetherwiththefiiesize. SpecifyingPCAddressesforDirectConnection ThefunctionkeysareallocatedasshowninthefollowingtablewhenspecifyingbitandwordaddressesinPCmemory.ThevaluesinparenthesesindicatethemaximumwordaddresspossiblefortheIargestPCmemory.Actual memorysizesvary,however,withthemodelofPC.RefertoyourPC'soperationmanualforspecificlimits. Key Area F1 AR(511) F2 HR(99) F3 ...
- マニュアル
.... Thehostcomputerisnotifiedeachtimeatouchswitchstatuschanges. 5・ゑ・8LampandTbuchSwitchDisplayStatusResp◎nse Format iESCISmlnln2 巨Bss・*1*1… 40 ---------------------[End of Page 6092]--------------------- CommandsSentbthePT Section5●2 Ml=DiSPIaystatus m1 NT20M,NT600M 0(30H)' Notlit{normaldisplay} 1(31H) La 2(32H) Flashinginvgrse(lamps)...
- マニュアル
...f f DM Data Memory CH Internal/Special Relay TIM Timer CNT Counter HR Holding Relay f f f – AR Auxiliary Relay f f f Auxiliary Relay LR Link Relay f f f – f f Allocated Word Allocated Bit Area Name Timer Counter f: OK : 1 word only : NG When allocating a memory table to words, the allocation must not exceed the word area. Since the special auxiliary relays of the CV series PCs are allocated to the system, they cannot be used for purposes other than the system use. However, reading from them is possible. 152 Overview of Direct ...
- マニュアル
...1 word only NG Counter NG 1 word only NG HR Holding Relay OK OK OK – AR Auxiliary Relay OK OK OK Auxiliary Relay OK OK NG LR Link Relay OK OK OK – Reference One allocation word of the memory table can use continuous areas of up to 2 words in the case of numeral memory table or 20 words in the case of characterstring memory table. Reference When allocating a memory table to words, the allocation must not exceed the word area. Since the special auxiliary relays of the CV series PCs are allocated to the system, they cannot ...
- マニュアル
...Allocated DM Datamemoワ Datamemory ○ CH 1/Orelay 1/Orelay O TlM ■merpresentvalue Timerpresentvalue × CNT Counterpresentvalue Counterpreserltvalue × HR Holdingrelay 一 ○ AR Auxiliarystoringrelay Specialauxiliaryrelay △ ...
- マニュアル
...× CNT Counter present value Counter present value × f: Possible (1/2 CH for numeric value) HR Holding relay – f : Possible for C series Impossible for CV series ×: Impossible AR Auxiliary storing relay ...
- マニュアル
...Timer NG 1 word only NG CNT Counter Counter NG 1 word only NG HR Holding Relay --- OK OK OK AR Auxiliary Relay Auxiliary Relay OK OK NG (∗) LR Link Relay --- OK OK OK (∗)“OK” when the C200H I/F unit is used. Note The Auxiliary Relay area of the CVM1/CV-series PC is for limited use of the system and cannot be used for any other purpose. The range of each memory area differs according to the PC type. Refer to Appendix B PC Memory Map for more details. 64 Display Element Control and Notification Section 5-2...
- マニュアル
... apply to bit and word input. S Even if lower case letters are input, the characters will be upper case. S If nothing is input, this will be interpreted as “no bit or word”. S Symbols that indicate the type of bit or word, such as “AR”, “...
- マニュアル
...Data Memory f CH Internal/Special Relay f Internal/Special Relay f TIM Timer Timer CNT Counter Counter HR Holding Relay f – AR Auxiliary Relay f Auxiliary Relay LR Link Relay f – f: OK : NG The Auxiliary Relay area of CVM1/CV series PC is used exclusively for special application in the system, and cannot be used for other application. When the Data Memory (DM) is specified, a bit number (00 to 15) is also specified in conjunction with a channel number. 4-5 Graphs The contents of the numeral memory tables of the NT620S/620C can be displayed as ...
- マニュアル
...IR Area f CIO Area f CIO Area f TIM Timer Area Timer Timer CNT Counter Area Counter Area Counter Area HR HR Area f AR AR Area f LR LR Area f – – Auxiliary Area – HR Area Auxiliary Area – – – The Auxiliary Area of CV series PC is used exclusively for special applications in the system, and cannot be used for other application. When specifying the DM Area, specify the bit number (00 to 15) along with the word address. 4-5 Graphs The contents of numeral memory table entries of the NT30/30C can be displayed as graphs as well ...
- マニュアル
... any area or position by the NTH Screen Data Converter.) Trend graph control area 4 words (Can be set to any area or position by the NTH Screen Data Converter.) None Addresses allocatable to control area DM, CH DM, CH, HR, AR, ...
- マニュアル
...T [0-9999] 4 CNT [0-32767] C [0-9999] C [0-9999] 5 HR [0-32767] L [0-9999] * 6 AR [0-32767] * S [0-9999] 7 LR [0-32767] B(16) [0-270F] * 8 10 * 11 EM [0-32767] W(16) [0-270F] X(16) [0-270F] Y(16) [0-270F] R [0-9999] * 9 W [0-32767] * 12 * * * 13 * * * 3 Mitsubis hi Fx D [0-9999] X(8) [0-23417] Y(8) [0-23417] * Memory Link * Siemens Modicon * M [1-9999] CH [0-9999] M [0-255] 4: Holding Register [1-9999] * * * T [0-127] * * * C [0-...
- マニュアル
... is also represented by a T.) L: Lamp T: Touch switch The second character represents the area type of PC (PLC) addresses. Example (PLC Vendor: OMRON) Blank: CIO area H: HR area A: SR area L: LR area D: DM (Data Memory) area E: EM Current Bank For characters that indicates area type of Mitsubishi, refer to page 131. Types of Screens, Common Dialog Box Settings and Operations Information Displayed on the Screen Section 5-1 Description Table No. The table entry number of the Numeral or Character String Memory Table (String Table) that is referenced for a numeral ...
- マニュアル
...Allocation None IR Area f CIO Area f CIO Area f H HR Area f --- --- HR Area n A AR Area f Auxiliary Area AR Area f L LR Area f --- LR Area*1 n T TC Area, Timer PVs TU --- C TC Area, Counter PVs CU --- --- --- --- TC Area, Counter Completion Flags W --- --- --- --- WR Area TK --- --- --- --- Task Flags D DM Area f DM Area f DM Area f E EM Area *2, current bank f EM Area, current bank n EM Area, current bank n E0_ to EC_ --- --- --- --- EM Area, EM banks 0 to C n --- Timer Area, Timer PVs --- ---...
- マニュアル
... to IR 81 CS1-series PCs CIO: 0000 to 0235, 0300 to 0511 HR: HR000 to HR099 CIO: 1000 to 1063 (see note) DM: D00000 to D05999 C200HE-CPU11(-Z) IR: 0000 to 0235, 0300 to 0511 HR: HR000 to HR099 LR: LR00 to LR63 DM: DM0000 to DM4095 Other C200HX/HG/HE PCs IR: 0000 to 0235, 0300 to 0511 HR: HR000 to HR099 ...
- マニュアル
...OK CIO Area OK CIO Area OK H HR Area OK --- --- HR Area Not for Host Link A AR Area OK Auxiliary Area No AR Area OK L LR Area OK --- --- LR Area*1 Not for Host Link T TC Area, Timer PVs No Timer Area, Timer PVs No TC Area, Timer PVs No TU --- --- --- --- TC area, Timer Completion Flags No C TC Area, Counter PVs No Counter Area, Counter PVs No TC Area, Counter PVs No CU --- --- --- --- TC Area, Counter Completion Flags No W --- --- --- --- WR Area TK --- --- --- --- Task Flags No D DM Area OK DM Area OK DM Area...
- マニュアル
... words max. (16,000 bytes) · Send/receive data link areas per personal computer: 32,000 words max. (64,000 bytes) · Total send data link words on entire network: 32,000 words max. (64,000 bytes) Data link areas Bit (CIO, and ...