全 863 件が検索されました。(781 - 800件を表示)

  • マニュアル

    ... modes are switched Terminal mode and expansion terminal mode Terminal mode Connection method Direct connection to C200HS. Connection via Peripheral Interface Unit or Host Link Unit. Cable for personal computer CQM1-CIF02 Peripheral Devices SYSMAC Support Software (SSS) ...

  • マニュアル

    ...-CPU42-EV1 CQM1-CPU43-EV1 CQM1-CPU44-EV1 Section 1-4 Word Allocation 1-3-2 Remote I/O Master The CQM1-LK501 I/O Link Unit connects to the following SYSMAC BUS Master Units. Model 1-4 PC C500-RM201 C2000H C1000H (F) ...

  • マニュアル

    ... SR word (0300) whether a communications error has occurred. For details, refer to the SYSMAC C Series Remote I/O Unit (Wired Type) Operation Manual for details. 132 Section 5-5 Troubleshooting Communications Errors 5-4-1 RM Unit SR Area C120/...

  • マニュアル

    ...fromeachgroupmustsatisfyboththefollowingequations: 3A+B+2C+6D≦12 A+B+C+D≦8 2.OtherUnitscanbeaddeduntilthetotainumberofUnitsreachesten.lfPC LinkUnitsareused,thenumberefUnitsincludingthePCLinkUnitsmust notexceedten. P『ecaUttons TheIRareaoftheC200HSpeciall!OUnitisallocatedaccordingtethesettingof theunitnumberswitchonthefrontpanel,nottheaddressoftheslotwherethe unitismounted.Referto4・1MθmoryAlloCatiOnfortheallocationofthememOry area. LeavethetwoslotsnexttotheCPUfree.ltisnotpossibletotLsedev▲cesconnectedtotheCPU(suchastheProgrammingConsole)iftheseslotsareOccupied. lftheC200HSIaveRackisconnectedtoanotherSYSMACmodelRemotel/O MasterUnit,suchastheCl20,...

  • マニュアル

    ... to the CPU free. It is not possible to use devices connected to the CPU (such as the Programming Console) if these slots are occupied. If the C200H Slave Rack is connected to another SYSMAC model Remote I/O Master Unit, such as the C120, ...

  • マニュアル

    ...etotheC20HBPleasebesuretousethese manualSwhenopera頴gtherelev即tUnitS,. UnH Mod別皿rnber Manu31name Catalognumbor PC C20H/C28Hκン10HIC60H lnstallatbnGuidθ W175 ◎pe【ationMa国al W176 FIT10 FIT10・MFIO1-EV6 OρeratbnMa龍al W150 LSS ...

  • マニュアル

    ... programmed and operated either from an IBM PC/AT or compatible running the LSS/SSS or from a Programming Console. Connect the computer using the illustrated cables. The computer must run the Ladder Support Software (LSS) version 3 or later (on 3.5” floppy disks: ...

  • マニュアル

    ...(selfholdir19). Push-buttonswitch(self-resetting).Whenitispressedin manualmode,allaxesareservo-tocked. Push-buttonswitch{self-resetting).Whenitispressedin automaticmode,theMCprogramisexecuted, Push-buttonswitch(self-resetting).Whenitispressedin manualmode,theMCprogramisexecuted. Push-buttonswitch(self-resetting).Whenitispressedin manualmode,joggingisexecutedineitherthepositiveor negativedirectionwhilethebuttonisbeinghelddown. Aftertheswitchboxhasbeenprepared,wireittothelnputUnitasshownbelow. SwitchBox べ lManuallAutomatic10perationlStart8. ...

  • マニュアル

    ... Master Control Units Item RS-232C port Specifications 1 port (SRM1-C02-V2 only) Host link, NT link, 1:1 PLC link, ASCII data transfer with XON, XOFF flow control Programming Console (CQM1-PR001-E/C200H-PR027-E) SYSMAC Support Software ...

  • マニュアル

    ... each slot. There are 3, 5, 8, or 10 slots available on the Backplane depending on the model of Backplane used. 5. Unit Connectors Connect I/O Units, Special I/O Units, Interrupt Input Units, and/or Analog Timer Units. Note Attach a ...

  • マニュアル

    ... the encoder to the High-speed Counter Unit through a long cable or to wire the cable in places where noise may be generated. An open collector output from an encoder can be connected as a line driver input to the High-speed Counter Unit through the ...

  • マニュアル

    ...4-2 CPU Backplane C200HW-BC031/BC051/BC081/BC101 Teaching Box CVM1-PRS71 Personal computer for SYSMAC Support Software IBM PC/AT or compatible SYSMAC Support Software Personal computer for MC Support Software MC Support Software ...

  • マニュアル

    ...-232C Adapter Converts to Peripheral Port format level communications. CPM1-CIF01 Connecting Cable Used to connect IBM PC/AT or compatible computers. (Length: 3.3 m) CQM1-CIF02 SYSMAC Support Software For IBM PC/AT or compatible computers (3.5” disks, 2HD) ...

  • マニュアル

    ...C200H-CN422 C200H-ATT01 WS02-CXPC1-E C200H-PRO27-E Connecting g C bl Cable Cable length: 2 m Cable length: 4 m For panel mounting. MS-Windows 95/98 (CD-ROM) for Ver. 2.0 or higher C500-ZL3AT1-E SYSMAC Support Software 3.5”, 2HD for IBM PC/AT compatible WS01-CPTB1-E SYSMAC-CPT For IBM PC/AT or compatible computers (3.5” disks (2HD) and CDROM) CPM1-EMU01-V1 Expansion Memory Unit Uploads the ladder program and DM 6144 to DM 6655 from the PC to the EEPROM and downloads the ladder program and DM 6144 ...

  • マニュアル

    ... Connected Model 3-3 3-3 Selecting the Connected Model Set the model that the Teaching Box is connected to. Select “MC Series” out of the following: • Servodriver (Position Driver) • MC Series (Motion Control) • 3G2A5-NC111-EV1 Position Control Unit • ...

  • マニュアル

    .... . . . . . . . . . Editing Sequence Data: C200HW-NC113/213/413 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Editing Positioning Actions: C500-NC113/211 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Editing Speed Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Editing Acceleration/Deceleration Time and Pattern Data . . . . . . . . . . . . . . . . . . . . . . . . Editing Dwell Time Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Editing Zone Data: C200HW-NC113/213/413 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 5 Transferring and Verifying Data . . . . . . . . . . . . . . . . . . . 5-1 5-2 5-3 Transferring Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Verifying Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Writing Data to Flash Memory/EEPROM . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 6 Monitoring the Position Control Unit . . . . . . . . . . . . . . . 6-1 6-2 6-3 6-4 6-5 Overview . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . PCU Monitor Screen . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Multimonitor (C200HW-NC113/NC213/NC413) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Command Status (...

  • マニュアル

    ... adjacent to the CPU Unit. Doing so would prevent peripheral devices such as the Programming Console from being connected. Special I/O Units cannot be used on a C200H Remote I/O Slave Rack if the Slave Rack is connected to different PC (i.e., ...

  • マニュアル

    ...SIOUUnits (ReadOn]y) Group2]【ノO Units(Read Only) LocaERacks SYSBUS RemoteRacks SYSBUS RemoteU㎡ts SYSBUS12 GrouplU皿its SYSBUS/2 Gmup2Units SYSBUS/2 Group3U皿its Rack Type C200H C500 58M 54M 122M CV CVM1 LK,SN,SL,BA,ET, MC,VP,SM,ME,MI, IS,DN,RM# ."譲纏㌶ 難 ㌶灘熱灘 ㌶"・."、÷◇w 鱗 、. 、. ぺ. 熟 ". " シ芯糠襟鍵 〆 ・懸・懸 s.・、㌔NN.'弍⇔LR.:〉 灘 o,i,O,1,00,H, OOOO,皿OI,OOII GG N,NN,NNNN LL,GL HH INTn RMn #[SIOU] 難懸議酬 、、㌔ 黙蕊愚...

  • マニュアル

    ... slots, it will not be possible to mount tools such as the Programming Console. • Special I/O Units cannot be used with C200H Remote I/O Slave Racks that are connected to Remote I/O Master Racks for other SYSMAC Programmable Controller models (such as C120, ...

  • マニュアル

    ... Table Operations No. of Remote Terminals Verification Error The following display indicates that the number of Slaves (RT) connected to the Master does not match the number registered in the I/O table. 000000I/O VRFY RM1 CONECT RT Master C200H/...