全 863 件が検索されました。(761 - 780件を表示)
- マニュアル
...ControlSystemincludesthePCSystem,thePCprograms,anda│日/Odevices thatareusedtocontrolorobtainfeedbackfromthecontrolledsystem. ThedevicesthatarebeingcontrolledbyaPCSystem. ALinkAdapterusedtoconvertbetweendifferenttypesofopticalfibercable,differenttypesofwirecable,orbe{weenopticaltibercableandwirecable.Such conversionisnecessarytoconnectUnitsthatusedifferentformsOfCommuniCation。 See()θntra/ρrocessingunit. ABackplane.usedtocreateaCPURack. AspecialUnitusedwithCV-seriesPCsthatmountstotheCPUbus.ThisconnectiontotheCPUbusenabiesspecialdatalinks,datatransters,andprocesslng・ ThemainRackinabuilding-blockPC,theCPURackcontainstheCPU,aPower Supply,andotherUnits.TheCPURack,alongwiththeExpansionCPURack, providesbothanI/ObusandaCPUbus. SeeAGE AnyofthetollowingPCs:C2000H,ClOOOH,...
- マニュアル
...Expansion CPU Backplane No No Yes Yes CV500-IC@01 CV500-BI111 Expansion I/O Backplane No Yes 16-/32-/64-point I/O Units Yes No CV500-BI042, CV500-BI062, CV500-BI112, CVM1BI114, and CVM1-BI064 (C500 Expansion I/O Racks can be used with certain limitations.) --- Special I/O Units Yes No Motion Control Units No Yes Applicable Units include Analog Input, Analog Output, High-speed Counter, PID, Position Control, Magnetic Card, ASCII, ID Sensor, and Ladder Program I/O Units. (The ...
- マニュアル
...An operation that searches the program for usage of a specific data area bit or word to see where and how the bit or word is being used. Used during program changes and debugging. C-series PC Any of the following PCs: C2000H, C1000H, ...
- マニュアル
...thatareusedtocontroiorobtainfeedbackfromthecontrolledsystem. ThedevicesthatarebeingcontrolledbyaPCSystem. Thesignalcountedbyacounter. Adedicatedgroupofdigitsorwordsinmemoryusedtocountthenumberof timesaspecificprocesshasoccurred,oralocationinmemoryaccessed throughaTCbitandusedtocountthenumberoftimesthestatusofabit◎ran executionconditionhaschangedfromOFFtoON. Seeoθノ7traiρroce5singunit. AspecjaiUnitusedwithCV-seriesPCsthatmountstotheCPUbus.ThisconnectiontotheCPUbusenablesspecialdatalinks,datatransfers,andprocessing. ThemainRackinabuilding-blockPC,theCPURackcontainstheCPU,aPower Supply,andotherUnits.TheCPURack,alongwiththeExpansionCPURack, providesbothanl/ObusandaCPUbus. Anoperationthatsearchestheprogramforusageofaspecificdataareabitor wordtoseewhereandhowthebitorwordisbeingused.Usedduringprogram changesanddebugging. AnyofthefollowingPCs:C2000H,ClOOOH,...
- マニュアル
...End・ ■●臼 PresstheShift+FIOKeysfromany◎therscreentogretumtotheBasicRackscreen.PresstheShiW+臼OKeysfromtheBasicRackscreentochθcktheinpしdVOtablecreatedon-screenandsave口totheworkdisklfnoerrorsarefound.Thel/Otablew‖lnotbgw巾tentotheworkd│skandanerrormessagetablewillbedisplayediferrorsarefound.PressthgEscKeyt◎returntotheoriginal㏄reen.CorredtheθrrorsandpressthgShift+F10Keysagain. Home Clear **** Clearstheallocationdisplayedatth白cursorp◎sition.PresstheShift+臼OKeysfromtheBasicRackscreentosavethechanges. AllocatlonsRequiredforC・seriesSpeciall!OUnRs Model AllocaUons ModeI AlIocations ...
- マニュアル
... V 2 pts 3G2A5-AD005 4 to 20 mA, 1 to 5 V 4 pts 3G2A5-AD006 0 to 10 V 4 pts 3G2A5-AD007 0 to 10 V, 0 to 20 mA (4-word operation only) 8 pts C500-AD101 4 to 20 mA, 1 to 5 V 2 pts 3G2A5-DA001 0 to 10 V 2 pts 3G2A5-DA002 0 to 5 V 2 pts 3G2A5-DA003 –10 to 10 V 2 pts 3G2A5-DA004 –5 to 5 V 2 pts 3G2A5-DA005 4 to 20 mA, 1 to 5 V, 0 to 10 V 4 pts...
- マニュアル
...) signal. Part of the cable wiring must also be changed. RS-422 Port Signal SG C-series Host Links Used by some models: SG Used C200H-LK202-V1 3G2A6-LK202-EV1 3G2A5-LK201-EV1 SG Not Used C500-LK203 4 CVM1/CV-series Host Links Not used. Section 1-2 System Configuration 1-1-5 New/Improved Commands for the CPU Host Interface New C-mode commands have been added for the CPU Host Interface and the functionality of existing commands has been improved as follows: New Commands • RL/WL: Read and write commands for the CIO Area. • RH/...
- マニュアル
...(RS-422) Centronics BSC11/BSC21 Computer (with terminal mode), display terminal, printer, display BSC31/BSC41 BSC51/BSC61 Computer (with terminal mode), display terminal, printer, display Computer (with terminal mode), display terminal, printer, display NA Host Link Unit (...
- マニュアル
...cyc{ic(data}transfer DAC DataACCeSSConsole dataarea datalink dataregister datatransfer debug decimal decimalintegerCOnstant 146 Glossar AspecialUnitusedwithCV-seriesPCsthatmountstotheCPUbus.ThisconnectiontotheCPUbusenablesspecialdatalinks,datatransfers,andprocessing. ThemainRackinabuilding-blockPC,theCPURackcontainstheCPU,aPower Suppiy,andotherUnits,TheCPURack,aiongwiththeExpansionCPURack, providesbothanl!ObusandaCPUbus. AnyofthefollowingPCs:C2000H,C1000H,...
- マニュアル
... in an Expansion I/O Rack or Slave Rack like other Special I/O Units. A total of 10 Special I/O Units can be controlled by a single C200H CPU and up to 4 Special I/O Units can be mounted on a Slave Rack. ...
- マニュアル
... slots on the CVM1-BC103. CPU Rack (CVM1-BC103) CPU PS 6 slots CPU Rack (CVM1-BC053) CPU PS 3 slots 11 Section 2-4 Unit Dimensions 2-4 Unit Dimensions Optical SYSMAC LINK Units (C500-SLK11) Coaxial-cable SYSMAC LINK Units (...
- マニュアル
...} 161 ---------------------[End of Page 806]--------------------- ---------------------[End of Page 807]--------------------- AppendlxA S量a髄dardM◎dels GraphicPy◎grammingC◎ns◎le(GPC) TousetheGPCwithaCV-seriesPC,youwillneedtheGPCitself,aCV-seriesMemoryPack,andaCV・series Keysheet.YbuwillalsoneedaMemoryCardAdapterifyouwanttouseMemoryCardsandaPCConnecting CabletoconnecttheGPCtothePC. GPC(MainUnit》 Model Operatingvo瞳age ...
- マニュアル
...., instructions that use specified operands). CHANGE ADDRESSES PRINT LISTS EPROM FUNCTIONS Globally changes bit and word addresses in the user program. Prints lists, ladder diagrams, and mnemonics. Writes, reads, and compares the user program between the PROM Writer and system work disk. ...
- マニュアル
... error will result and the internal circuitry may be damaged. Note A memory error might occur when a RAM Unit is installed in a C200HCPU21-E/23-E/31-E CPU Unit with data written using a C200HCPU01-E/03-E/11-E CPU Unit or a GPC and ...
- マニュアル
... next to the CPU free. It is not possible to use devices connected to the CPU (such as the Programming Console) if these slots are occupied. If the C200H Slave Rack is connected to another SYSMAC model Remote I/O Master Unit, such as the C120, ...
- マニュアル
... slots next to the CPU free. It is not possible to use devices connected to the CPU (such as the Programming Console) if these slots are occupied. If the C200H Slave Rack is connected to another SYSMAC model Remote I/O Master Unit, such as the ...
- マニュアル
...-6 Cable Preparation (Connector Type) Prepare the cable for connector-type I/O Units as explained below. Recommended Connectors (Cable Side) Connector type Model (by Fujitsu) Set (from OMRON) Soldered Socket: FCN-361J040-AU Connector cover: FCN-360C040-J2 ...
- マニュアル
...* x 161 x 160 x 161 x 160 End code Model code FCS ↵ Terminator Model Code “Model code” indicates the PC model in two digits hexadecimal. Model code Model 01 C250 02 03 C500 C120 0E 10 C2000 C1000H 11 12 C2000H/CQM1/CPM1/CPM1A/SRM1 C20H/C28H/C40H/C200H/C200HS 20 21 CV500 CV1000 22 40 CV2000 CVM1-CPU01-E 41 42 CVM1-CPU11-E CVM1-CPU21-E 6-3-29 TEST–– TS Returns, unaltered, one block of data transmitted from the host computer. Command Format @ x 101 x 100 Node no. Response Format x 101 x 100...
- マニュアル
... slots adjacent to the CPU. Doing so would prevent peripheral devices such as the Programming Console from being connected. Special I/O Units cannot be used on a C200H Remote I/O Slave Rack if the Slave Rack is connected to different PC (i.e., ...
- マニュアル
...A Connecting Cable is provided with the CQM1-PRO01-E. Connecting Cable Programming Console IBM PC/AT with LSS An IBM PC/AT or compatible computer can be connected as shown in the following diagram. The LSS is available on either 3.5” disks (...