全 863 件が検索されました。(741 - 760件を表示)
- マニュアル
...Positiondata Positiondata ::…. 、 6-52 ---------------------[End of Page 7164]--------------------- Basicoperation 6.3Localmode lnthismode,thepositioncontrolunitisfunctionailydetachedfromthePC andoperatesunderthecontroloftheteachingbox.Also,inthismode, settinganddisplayareperformedbytheteachingboxinmmunits. Settinganddisptay inmm'units RS・422cable ' …「1 篇〔㌫臨 ●●●●●◆●● 佐芯蝋書函 SYSMAC-...
- マニュアル
...Memory Pack by using an appropriate peripheral device (refer to Appendix C Standard Models). The EPROM Chip may be programmed using a PROM Writer or a FIT Ladder Pack. Then the EPROM Chip must be mounted inside the EPROM Pack. Note Only PROM Writer Model ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . C500 Systems . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . C1000H and C2000H Systems . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . C200H Systems . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . xi xii xii xii xiii xiii xv 1 2 4 7 8 14 16 17 18 21 22 25 39 41 45 46 53 55 56 60 61 62 64 69 70 70 71 72 vii TABLE OF CONTENTS SECTION 7 Error Processing . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7-1 7-2 7-3 7-4 7-5 7-6 7-7 Self-Diagnosis . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Error Codes and Monitoring . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Locating Transmission Errors . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . CONTINUE and STOP Mode Operation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Recovery in STOP Mode . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . I/O Table Creation Problems . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Slave Unit Numbers with Multiple Terminators . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 75 76 81 91 92...
- マニュアル
... slots adjacent to the CPU. Doing so would block peripheral devices such as the Programming Console from being connected. Special I/O Units cannot be used on a C200H Remote I/O Slave Rack if the Slave Rack is connected to different model PC (i.e., ...
- マニュアル
...., instructions that use specified operands). CHANGE ADDRESSES Globally changes bit and word addresses in the user program. PRINT LISTS Prints lists, ladder diagrams, and mnemonics. EPROM FUNCTIONS Writes, reads, and compares the user program between the PROM Writer and system work disk. ...
- マニュアル
...cannot be used in the C2000H Duplex System. The table below summarizes the output capacity of the three models and the current available for I/O Units mounted on the CPU Rack. Model 3G2A5-PS221-E 3G2A5-PS223-E 3G2A5-PS211-E ...
- マニュアル
...CPU is defective. Output indicator does not light. 292 Indicator is defective. Replace defective Unit. Appendix A Standard Models CPU Backplane Name Backplane Remarks C1000H Model 9 I/O slots (see note) 6 Link slots ...
- マニュアル
...Shielded twisted pair cable Input A + A+ – A– + B+ – B– + C+ – C– Input B Input Z E The following wiring example shows connections between an open-collector encoder and an Encoder Adapter (C500-AE001), and between the Encoder Adapter and inputs A, B, and Z. Connections should be wired so that Counter Unit inputs go ON when encoder outputs go ON. Because the ...
- マニュアル
...10 SWBrise 11 Parameterandspgedtransferθnd 12 DatatransferendwhenSW-AON 13 DatatransfθrendwhenSW-BON 糾 Program Onceyouhavecompletedthepreparationsdesc目bedonthelastfewpages, wr旋ethefollowingProgramtoPCmemoryviatheProgrammingConsole・ ThePCmustbemPROGRAMmodewhenwr口ingaprogram.Whenthisprogramisexecuted,thedatastoredintheDMareaissequentia‖ytransferred fromthePCtothePositionControlUn口. 101 ---------------------[End of Page 9666]--------------------- Proam ExamPlefo『...
- マニュアル
... setting and check to be sure that the expanded portion of DM area is held in RAM. 255 Appendix A Standard Models CPU and Associated Units Name CPU Backplane Specifications 8 slots 5 slots Model 3 linkable slots ...
- マニュアル
... product, or product failure. Please read each section in its entirety and be sure you understand the information provided in the section and related sections before attempting any of the procedures or operations given. ix PRECAUTIONS This section provides general precautions for using the ...
- マニュアル
...14 21 22 The following table lists the applications and applicable models for each of the OMRON crimp connectors shown above. Model Number Application Applicable Models Connection S3200-COCH62M SYSMAC NET Link nodes S3200-LSU03-01E Line Server, ...
- マニュアル
...'tbeingcarriedoutintheothernode. 5.Processingisn'tcorrectintheloca】node(amalfunctionduetonoise,forex・ ample}. ltisimportantteperformothertestssuchastheechobackandbroadcasttests andusetheseresultsinconjunctionwiththediagnostictableinformation. RediSPIay ComparisonDisplay SoftwareCompatibility If"R"isenteredatthediagnostictabledisplay,thediagnostictablewillbedis・ playedagainforthenodespecifiedinstep3intheprocedureabove. lf℃"isenteredatthediagnostictabledispiay,thediagnostictablewillbedisplayedagainforthenodespecifiedinstep3intheprocedureab◎ve.三「hedifferencebetWeenthepreviousresultsandthenewresultswillalsobedisplayed. ThefoIlowingtableshowstheUnitsthatsupporttheDiagnosticTabieRead operation・A"Yes"inthetableindicatesthatthediagnostictablecanberead fromthatUnit(NSB). IModel 一 -DlagrlostlcTab!eRead ▼...
- マニュアル
...AS伽dardModcls BSpecifications 0ーユ 44 ---------------------[End of Page 8279]--------------------- A Star dardM◎dels Name Model UneServer S3200-LSUO3-01E NetworkSupportBoardandso費ware S3200-NSB11-E NetworkSupPortBoardforFIT FlT10-lF401 NetLinkUnitforC500,C1000H.C2000H ...
- マニュアル
...SYSMACNetptoductsar61ist6dbelowwilhmodelnUmbets, 一 N日mo 一〇●剛pll。 n ・一−P87tnumbgr -一−LingSgrv6rU耐 Cfealθggnd『non目6r5i}igto}《on;onoUn‖「θqul「θdfo「gachngtworkloop.A6goondUnitlmayalsob6s9110fundlon83rgPθa拍「, ・.SYSMAGNETUnkUni1 一一…一・・N③two{ki耐olねc6brC・sgri6⑨PC8. ・一・...
- マニュアル
...3-2 Self-diagnostic Function. 49 Section 2-8 Switch Settings System Configuration Example In the diagram below, a C20 CPU, a C40P CPU, a C20 I/O Unit and two I/O Link Units can exchange data over a distance with a ...
- マニュアル
... SYSMAC LINK Unit and one Rack-mounting Host Link Unit In addition to the Units in the above combinations you may also mount one CPU Unit-mounting Host Unit or up to two PC Link Units. Only one PC Link Unit can be mounted on the ...
- マニュアル
... the Peripheral Interface Unit/Host Link Unit to the CPU by tightening the mounting screws. The RS-232C interface can be used to connect a Mini H-type PC to a variety of devices equipped with an RS-232C interface, including computers, display devices (e.g., the ...
- マニュアル
... jacks on the Programming Console, although it is possible to connect a cassette recorder to the GPC to store, retrieve, and verify programs on tape. The GPC not only allows programs to be stored and retrieved from tape, but also allows programs written for the C120 and ...
- マニュアル
...POWεRON†o ㏄POWεR NCDL刑ESERVER 9CD DCPOWER GD LitwhenoperationaS LitwhentOkenisdetected. Notlitduringlooperrors. ArepeaterisrequiredwhenthedistancebetweentwonodesofthenetWerk loopexceedslkm.Whenarepeaterisrequired,aLineServerjssettofunc・ tionasarepeater.Whenfunctioningasarepeater,theLineServeronlyre・ ceivesandre-transmitsthetokenordatagram.ThenetWorkloopcanhave uptotwoconsecutlverepeaters・ 2-"2 SYSMACNETLinkUnits TheSYSMACNETLinkUnitisusedtoconneCtaPCtotheSYSMACNET. OncethePCisonthenetWork,itcansenddatatoandreceivedatafrom othernodes. TheSYSMACNETLinkUnitismountedtoaC200H,...