全 425 件が検索されました。(61 - 80件を表示)

  • マニュアル

    ....plc. 4 In the programming area of the plc1.plc tab page, write a program as shown on the right. This example program turns a servo ON, starts user program 1 for the motor, then exits periodic open plc 1 while(...

  • マニュアル

    ...frequency and rotation direction of the 3G3AX-MX2-ECT motor with the interval of 3 seconds. * In this example, PDO mapping is assumed to be the default setting. If you want to change PDO mapping, rewrite open plc 1 while(...

  • マニュアル

    .... 1 In the Solution Explorer pane, open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the plc1.plc tab page, write a program as show on the right. open plc 1 while(...

  • マニュアル

    ... Explorer pane, open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the plc1.plc tab page, write a program as show on the right. This sample program blinks the open plc 1 while(...

  • マニュアル

    .... 1 In the Solution Explorer pane, open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the plc1.plc tab page, write a program as shown on the right. open plc 1 while(...

  • マニュアル

    ..., open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the plc1.plc tab page, write a program as shown on the right. This sample program substitutes slave data open plc 1 while(...

  • マニュアル

    .... 1 In the Solution Explorer pane, open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the plc1.plc tab page, write a program as shown on the right. open plc 1 while(...

  • マニュアル

    ..., write a program as shown on the right. This sample program blinks the GX-OD1611 output indicator every second. * In this example, PDO mapping is assumed to be the default setting. If you want to change open plc 1 while(...

  • マニュアル

    ... is safe if the motor rotates before the setting. 1 3-8 Open the global definitions.pmh under PMAC Script Language ‒ Global Includes in the Solution Explorer. CK3M/CK5M Series Startup Guide DirectPWM Interface (O047) 3 DirectPWM Interface Connection Procedure 2 ...

  • マニュアル

    ...Includes in the Solution Explorer. 3 CK3M/CK5M Series Startup Guide Sinusoidal Encoder (O048) 3-7 3 Sinusoidal Encoder Connection Procedure 2 Write the text on the right to the global definitions.pmh. • To use the hardware-interpolated sinusoidal encoder position ...

  • マニュアル

    ...[5].AdcAmpStrobe 21 – 24 $91420C 6 Gate3[6].AdcAmpStrobe 25 – 28 $91820C 7 Gate3[7].AdcAmpStrobe 29 – 32 $91C20C Additional Information • Dollar ($) sign indicates hexadecimal value in PMAC script language. • The explicit address is found by subtracting ...

  • マニュアル

    ...PMAC Script Language – Global Includes in the Solution Explorer. 3 2 Write the text shown on the right to the global definitions.pmh. The settings are based on the following conditions. • Phase frequency: 8 kHz • Servo period: 2 kHz ...

  • マニュアル

    ... connection information from control is removed Note Power PMAC IDE User Manual 33 IDE Layout Alarm Indicator The Alarm indicator is always visible to clearly indicate to the user any Alarm as they are triggered. This view monitors the global status elements (...

  • マニュアル

    ... declared pointer variables. Many users will want to use these defaults, and declare the variables to be available to the server at the top of the project file global definitions.pmh. For example, if the first pointer-variable declarations in this file are: ptr ServoCyc->...

  • マニュアル

    ...Timings - Constant Cycle Time Timings - Scheduled Interrupt Interval Timings - Schedule Interrupt Interval Timings - CPU Bus Link Service None Hold - Enable Hold Area None Hold - CPU Set the hold status of Rack 0 to 7. ・...

  • マニュアル

    ...EIP002_Status_IN [15] to [0] 15 14 13 12 11 10 9 Resv Resv Resv Resv Resv Resv Resv 8 7 6 5 4 3 2 1 0 RF_W SYS_ RF_E CMD_ NOR READ FRIC ERR BUSY AR ERR RR ERR M Y Precautions for Correct Use If the data size of tag data links for Destination Device is an odd-numbered byte, use BYTE type to define, do not use BOOL type. Additional Information With Sysmac Studio, two methods can be used to specify an array for a data type. After specifying, (1) is converted to (...

  • マニュアル

    ... Data : D10019 ■Details on input area Address D10100 Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 RF_W SYS_ RF_E CMD_ NOR READ Resv Resv Resv Resv Resv Resv Resv FRIC ERR BUSY AR ERR RR ERR M Y D10101 Error Code D10102 Response Information 1 D10103 Response Information 2 D10104 : Response Data D10119 Additional Information For the allocation of tag data links of RFID Reader/Writer, refer to Memory Assignments in EtherNet/IP Communications Protocol in Section 5. Host Communications Specifications of the V680S Series User’s Manual (...

  • マニュアル

    ...Perform the settings for connecting the Controller to the Servo Drive. Open Global Definitions.pmh located under PMAC Script Language-Global Includes in the Solution Explorer. 3 2 Write the text on the right to Global Definitions.pmh. • For CK3W-AX1414£ ...

  • マニュアル

    ...Perform the settings for connecting the Controller to the Servo Drive. Open Global Definitions.pmh located under PMAC Script Language-Global Includes in the Solution Explorer. 3 2 Write the text on the right to Global Definitions.pmh. • For CK3W-AX1414£ ...

  • マニュアル

    ... encoder with the following conditions a) b) c) d) e) 24 position bits No parity check Gray code format 2.0 Mbps (Maximum data rate is 2.0 Mbps) Trigger on the rising edge of servo clock (no delay) Sys...