全 65 件が検索されました。(61 - 65件を表示)

  • マニュアル

    ... PCs through their LR areas. Refer to 3-2-5 LR Area for details on LR bits. SP10-AL001 Link Adaptor SP10-PRO01-V1 Programming Console SP10-CN__1 Connecting Cables SP__ #0 8 SP__ #1 SP__ #2 SP__ #3 PC Configuration Section 1-4 Note 1. When two or more PCs are linked, apply power to all of the PCs at once or to PC #0 last. 2. When using a Link Adapter, one PC must be connected to connector number 0 on the Link Adapter. 3. Once CPUs are connected to the Link Adapter and turned ON, ...

  • マニュアル

    .... SP-2 Set point 2 Set point lower limit to set point upper limit (°C/°F) 0 For models incorporating an event input 2 function. Set point lower limit to set point upper limit (°C/°F) 0 SP-3 in-S 20 Setting/Display Range Set point 3 Input shift value –199.9 to 999.9 °C/°F 0.0 Displayed and can be set if the default value is changed on the engineering level. For models incorporating an event input 2 function. Displayed and can be set if the default value is changed on the engineering level. Displayed ...

  • マニュアル

    ... Use this setting to assign output content to outputs. Function Setting Setting range Units Default value Disable (0) CH1 control output (heating or open) For control output (1) CH1 control output (cooling or close) For control output (2) CH1 ...

  • 商品情報

    ...目設定値例 イベント入力1(EV-1) MSP0イベント入力2(EV-2)MSP1目標値0(SP-0)0(℃)目標値1(SP-1)10(℃)目標値2(SP-2)20(℃)目標値3(SP-3)30(℃) ■操作手順はこちら以下の手順で設定を行ってください。1.イベント入力の設定をする キー操作表示操作内容   ...

  • 商品情報

    ...ます。 レベル 設定項目 設定値 初期値 ① 初期設定レベルマルチSP使用数(EV-M)1または2 *5 1 ② 調整レベル目標値0~3(SP-0~SP-3)任意の設定値 *5 0 *5 使用する目標値が 2点の場合  マルチSP使用数は「1」、目標値0、目標値1を設定します。 使用す...