全 309 件が検索されました。(61 - 80件を表示)

  • マニュアル

    ...の LVS-95□□バーコード検証機を使用しない場合)、[カメラ]セクションに表示されるのは[オフ]と[オン]です。 LVS-9580 と LVS-9510 (5 MP)を併用する場合は、両方のカメラが[カメラ]セクションに表示されます。 [9510] を選択します。 注: Windows の[カメラ]設定で、[アプリがカ...

  • マニュアル

    ...品) RAM: 4 GB 解像度: 800×600 USB 2.0 ポート×1(補助リードヘッド(Auxiliary Readhead) 1 台の使用につき 1 つの追加ポートが必要) 5.0 MP 補助リードヘッドに接続するユーザ使用コンピュータでは、LVS-95□□ソフトウェアバージョン 3.0.8 以降を実行する必要があ...

  • マニュアル

    ...外部照明なし R 赤色 W 白色 P ハイスピード、プラスモード X ハイスピード、Xモード 2a) V420-F 0.3 MP モノクロオートフォーカスカメラ(50∼300mm):選択可能な組み合わせ V420-F000[Y]03M-[L][C][P] 記号 分類 コード 意味 Y 視野 W 広視野(5.2mm焦点距離レン...

  • マニュアル

    ...焦点カメラ c.) F420-F 120万画素モノクロ固定焦点カメラ(狭視野レンズ) 2. オートフォーカスカメラ a)F420-F 0.3 MPモノクロオートフォーカスカメラ(50-300 mm) b)F420-F 1.2 MPモノクロオートフォーカスカメラ(ワイドおよびミディアムレンズ...

  • マニュアル

    ...たモデルの選定オートフォーカスの VHV5-F シリーズには 6 つのモデルがあります。 画像センサの解像度には、2.3 MP と 5.0 MP の 2 種類があります。 以下の表は、2 種類の画像センサと 3 種類のレンズ(中視野、狭視野、および超深度・長距離)の...

  • マニュアル

    ... objects was display color inversion. Improved alarm/event summary and history display Fonts xii New version Version 2.1 Version 7.0 It is now possible to connect NS-series PTs to the following devices. • OMRON Trajexia Motion Controllers • Yaskawa ...

  • マニュアル

    ...ASCII Appendix L Hayes Modem AT Command Protocol Setting Example When send data is THIS IS SAMPLE. 0009 0014 5448 4953 2049 TH IS I 5320 S 5341 4D50 4C45 SA MP LE Character string length of send data sent to modem (bytes) Code length of PMCR when it is used (words) A maximum of 200 bytes (including the CR) can be received. When the received data is RETURN OK, the content stored in the receive words is as follows: 0006 5245 5455 524E 204F RE TU RN O 4B00 K Length of received character string (words) Note An error ...

  • マニュアル

    ...(The ten-key pad is displayed when the input box is selected. To enable inputting from the ten-key, click the System Info. Button in the Setup Dialog Box, and then change the setting to enable the ten-key. Changing the MV Change the ...

  • マニュアル

    ...CJ1-H No Yes No Yes Yes No Yes (1:1) No No No No No No Peripheral bus No Host Link (SYSMAC WAY) No Yes The WG, MP, and CR commands are not supported. Yes The CR command is not supported. Yes The WG and ...

  • マニュアル

    ... keyboard. (The ten-key pad is displayed when the input box is selected. To enable inputting from the tenkey, click the System Info. Button in the Setup Dialog Box, and then change the setting to enable the ten-key. Changing MV Change the ...

  • マニュアル

    ...mouse), or the keyboard. (The ten-key padis displayed when the input box is selected. To enable inputting from the tenkey,click the System Info. Button in the Setup Dialog Box, and then changethe setting to enable the tenkey. ·Changing MV Change the ...

  • マニュアル

    ... data to left for odd numbers of bytes) ASCII Setting Example When send data is THIS IS SAMPLE. 0009 000E 5448 TH 4953 2049 IS I 5320 S 5341 4D50 4C45 SA MP LE Character string length of send data sent to modem (bytes) Code length of PMCR(260) when it is used (words) A maximum of 200 bytes (including the CR) can be received. When the received data is RETURN OK, the content stored in the receive words is as follows: 0006 5245 5455 524E 204F RE TU RN O 4B00 K Length of received character string (words)...

  • マニュアル

    ... (MPGSetRatios) You can set four ratios in MPG Set Gear Ratios (MPGSetRatios). The values that are set in MPGSetRatios when Enable changes to TRUE are used. The default values in MPGSetRatios are 0. Always set values before you use MPGSetRatios. Select the gear ratio with ...

  • マニュアル

    ...9 1 0 1000 1000 Variables  Internal Variables Name FixedWei ghtVal HoldingM easuringV al Start_Wei ghtCtrl Start_Calc Trigger FallComp Val CalcCount Num Int_FallCo mp SignInver sion Shortage Weight Data Type REAL 0 Comment Fixed weight set value REAL 0 Hold weight value BOOL FALSE BOOL FALSE REAL 0 Start flag for feed weighing Execution flag for fall compensation Fall compensation value UINT 0 Differential memory size AT OmronLib\WC_Toolb ox\WC_FallCompens ation BOOL FALSE Instance of the WC_FallCompensation function block Discharging method BOOL Execution flag for processing additional feed weighing Abort for quantitative...

  • マニュアル

    ...Yes Yes No Yes Yes MicroHAWK V320-F / V330-F / V420-F / V430-F Barcode Reader User Manual A-11 Appendices A-1-3 Field of View Charts Fixed Focus Field of View (mm) - Wide Lens 0.3 MP 1.2 MP 5 MP Distance (mm) Width Height Width Height Width Height 50 49 32 53 39 50 38 64 62 39 66 49 63 47 81 76 49 81 61 78 58 102 95 60 101 75 96 72 133 121 78 129 97 124 92 190 171 109 182 136 174 130 300 266 170 283 213 271...

  • マニュアル

    ... Focus at 300 mm W Wide Field of View - 5.2 mm Focal Length Lens M Medium Field of View – 7.7 mm Focal Length Lens N Narrow Field of View – 16 mm Focal Length Lens 03M 752 x 480 (0.3 MP) Pixel, Mono Sensor, Global Shutter 12M 1280 x 960 (1.2 ...

  • マニュアル

    ...2-1 2-1-1 Check Hardware Basic Hardware Table and Configuration Diagram Important: The configuration shown below is just one example of how a V440-F can be configured in an application. Item Description Part Number V440-F, No Optics, 5 ...

  • マニュアル

    ...STC-B Series example] USB3 Vision STC-M Series USB3 Vision Remote Head Model STC-R Series UVC STC-S133 Series 8 Camera configuration example Pixels # of cameras Connection Maximum Frame rate Type (※) 0.4 ...

  • マニュアル

    ...1 Lighting Illuminates part to be read. Red or white. 2 Autofocus Lens Focuses on part to be read. 6.42, 8.5, 12.5, and 20 mm focal length. 3 Sensor Captures image of part. 2.3 MP and 5.0 MP. 4 Front Window Encloses camera; provides mounting area for filters. Flat for 6.42 and 8.5 mm lens. Focused for 12.5 and 20 mm lens. 5 Filter Accessories Modifies lighting for different applications. None, Diffuser, Full Polarizer, Half Polarizer. 6 Targeting Optics Indicates the center of the reading field of view. 7 360 Degree Pass/...

  • 生産終了品/推奨代替品

    ...モータ式タイムスイッチ H2F-DMFC 2015年3月 推奨代替品の一部形式仕様は生産終了 デイリータイムスイッチ H2E-MP 1995年9月 生産終了 生産終了案内 モータ式タイムスイッチ H2F-DMF 2015年3月 推奨代替品の一部形式仕様は生産終了 モータ式タ...