全 53645 件が検索されました。(6501 - 6520件を表示)
- マニュアル
...143 100 129 ±0.2 (MOUNTING HOLES) 4-3.2Dia. PENETRATION 4-6.5Dia. DEPTH3 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...R25 Tightening torque: 4.30N・m 402 10±0.2 25±0.2 30±0.2 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
... momentarily emits light with the maximum brightness. • When noise gets on the power supply supplied to this product from outside (DC24V), when changing the lighting condition by this product, there is a possibility that the set value isn't renewed, so do the following action. • It'...
- マニュアル
...いでください。 ・廃棄するときは、 産業廃棄物として処理してください。 ・適合照明 (FLVシリーズ) と適合カメラ(FH-Sシリーズ、 FZ-Sシリーズ)、 適合画像センサコントローラ (FHシリーズ、 FZ5シリーズ)のみに接続してください。 専用品以外を使用する...
- マニュアル
... the tab. Doing so may break the wire. Controller side Before removing Controller side Lighting side Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
... force without pressing the tab. Doing so may break the wire. Before removing Controller side Lighting side Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
... to +60℃ (with no icing or condensation) Ambient Humidity Operating and storage: 35% to 85% (with no condensation) Vibration Resistance(destructive) 10 to 150 Hz, (0.7mm double amplitude) 80 min. each in X, Y, and Z directions Shock Resistance (destructive) 150 m/...
- マニュアル
... to +60℃ (with no icing or condensation) Ambient Humidity Operating and storage: 35% to 85% (with no condensation) Vibration Resistance(destructive) 10 to 150 Hz, (0.7mm double amplitude) 80 min. each in X, Y, and Z directions Shock Resistance (destructive) 150 m/...
- マニュアル
... (FQ□-□D31). ■ Contents of label on unit Suitability for Use NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
... cable) Weight Approx. 290 g Suitability for Use NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
.... When charging is finished, the CHARGE LED will turn off. NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
...[5339050-6A] FQ-CR1[][][][][]-M Fixed Mount Multi Code Reader Instruction Sheet (Quick Start Guide) FQ-CR1□□□□□-M * 5 3 3 9 0 5 0 - 6 A * Warning Label -M 1.6 1.6 User's Manual 1.6...
- マニュアル
...) The Sensor emits visible light which may on rare occasions have a harmful effect on the eyes. Do not look directly at the light emitted by the sensor. If the light projects onto a reflective surface, prevent the reflected light from entering a person'...
- マニュアル
...) The Sensor emits visible light which may on rare occasions have a harmful effect on the eyes. Do not look directly at the light emitted by the sensor. If the light projects onto a reflective surface, prevent the reflected light from entering a person'...
- マニュアル
...The Sensor emits visible light which may on rare occasions have a harmful effect on the eyes. Do not look directly at the light emitted by the sensor. If the light projects onto a reflective surface, prevent the reflected light from entering a person'...
- マニュアル
...The Sensor emits visible light which may on rare occasions have a harmful effect on the eyes. Do not look directly at the light emitted by the sensor. If the light projects onto a reflective surface, prevent the reflected light from entering a person'...
- マニュアル
...) The Sensor emits visible light which may on rare occasions have a harmful effect on the eyes. Do not look directly at the light emitted by the sensor. If the light projects onto a reflective surface, prevent the reflected light from entering a person'...
- マニュアル
... the sensor is processing. Turns yellow while the sensor is connected. Turns green when the total judgment result is OK. Turns red when the total judgment result is NG. Turns yellow during RS-232C communications. (FQ-SDU2□ only) A mount to which the Unit'...
- マニュアル
...IN3 IN4 IN5 OUT0 (OR) OUT1 (BUSY) OUT2 (ERROR) Blue I/O 24 VDC Important • When brightness correction mode is ON, the brightness is stable but a delay of 25 ms occurs. Refer to the User's Manual for details. (FQ2-CH1-M) • Use a no-contact output device (e.g., SSR or PLC transistor output) for the TRIG signal. If a contact (e.g., relay) is used, contact bound may cause the trigger to be input again during execution of a measurement. Example 2 Here, a process switching signal is input from an external ...
- マニュアル
...The Sensor emits visible light which may on rare occasions have a harmful effect on the eyes. Do not look directly at the light emitted by the sensor. If the light projects onto a reflective surface, prevent the reflected light from entering a person'...