全 53645 件が検索されました。(6441 - 6460件を表示)
- マニュアル
... [Start] - [All Programs] - [OMRON] - [FH-AP1] [Application Producer]. • CD-ROM: 1 • Instruction sheet (Japanese/English): 1 Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...not avoided, may result in minor or moderate injury or in property damage. WARNING This product is not designed or rated for ensuring safety of persons. Do not use it for such purposes. Apply the latest security updates on your computer'...
- マニュアル
... by Omron. (a) Applications with stringent safety requirements, including but not limited to nuclear power control equipment, combustion equipment, aerospace equipment, railway equipment, elevator/lift equipment, amusement park equipment, medical equipment, safety devices and other applications that could cause danger/harm to people’...
- マニュアル
... by Omron. (a) Applications with stringent safety requirements, including but not limited to nuclear power control equipment, combustion equipment, aerospace equipment, railway equipment, elevator/lift equipment, amusement park equipment, medical equipment, safety devices and other applications that could cause danger/harm to people’...
- マニュアル
...ed dimensions. ・Do not directly connect an electric wire that is simply twisted to the terminal block. ・Use a DC power supply with safety measures against high-voltage spikes(safety extra low-voltage circuits on the secondary side). ●Handling ・Always turn OFF the product'...
- マニュアル
...産業廃棄物として処理してください。 16.8 25 10∼150Hz 片振幅0.35mm 3方向 各8分 10回 (加速度最大50m/s2) 2 150m/s 6方向 各3回 4-M4深さ4 周囲湿度 動作時・保存時:各35∼85%RH (ただし、結露しないこと) 40 30 4-M4深さ4 周囲雰囲気 腐食性ガスのないこ...
- マニュアル
...計測が出来なくなる可能性があります。 10∼150Hz 片振幅0.35mm 3方向 各8分 10回 (加速度最大50m/s2) 22 12 2 150m/s 6方向 各3回 耐衝撃周囲温度 動作時:0∼+40℃ 保存時:−25∼+65℃ (ただし、氷結・結露のないこと) 周囲湿度 動作時・保存時:各35∼85%RH (ただし、結露しな...
- マニュアル
...ーラとカメラケーブル2本で接続する場合、以下のように接続してください。 (カメラ4台接続の場合) カメラ形FH-S□□□ コントローラ形FH CH1 カメラコネクタ0 CH2 カメラコネクタ1 CH1 カメラコネクタ2 CH2 カメラコネクタ3 CH1 カメラコネク...
- マニュアル
...質質量付属品ケーブル長 FH-SM21R FH-SC21R 2.3W以下 (DC13V) 10∼150Hz 片振幅0.35mm (加速度最大50m/s2)3方向 各8分 10回 150m/s 6方向 各3回動作時: 0∼+40℃ 保存時: -20℃∼+65℃ (ただし、 氷結・結露しないこと) 動作時・保存時 各35∼85%RH (ただし、 結露しないこと) 腐食性ガスのない...
- マニュアル
... results of risk assessment. Compliance with the Robot Safety Guide and all of the information contained in our Robotic System Product Information does not guarantee that personal injury or damage to equipment caused by an industrial robot will be avoided. During maintenance, disconnect the robot'...
- マニュアル
... correct the mounting position. (Recommended mounting screw torque: 0.23 N・m) Name plate Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’ ...
- マニュアル
...ーラとカメラケーブル2本で接続する場合、以下のように接続してください。 (カメラ4台接続の場合) カメラ形FH-S□□□ センサコントローラ形FH CH1 カメラコネクタ0 CH2 カメラコネクタ1 CH1 カメラコネクタ2 CH2 カメラコネクタ3 CH1 カメラ...
- マニュアル
...ーラとカメラケーブル2本で接続する場合、以下のように接続してください。 (カメラ4台接続の場合) カメラ形FH-S□□□ センサコントローラ形FH CH1 カメラコネクタ0 CH2 カメラコネクタ1 CH1 カメラコネクタ2 CH2 カメラコネクタ3 CH1 カメラ...
- マニュアル
...量付属品ケーブル長 形 FH-SMX12 形 FH-SCX12 3.6W以下 (DC13V) 10∼150Hz 片振幅0.35mm (加速度最大50m/s2)3方向 各8分 10回 150m/s 6方向 各3回動作時: 0∼+40℃ 保存時: -20℃∼+65℃ (ただし、 氷結・結露しないこと) 動作時・保存時 各35∼85%RH (ただし、 結露しないこと) 腐食性ガスのない...
- マニュアル
... sheet), General Compliance Information and Instructions for EU 5 m max. *1:The temperature of the image sensor in this camera is controlled at 15°C to improve image quality. White spots and noise increase when the temperature of the image sensor (the camera'...
- マニュアル
... mounting screw (M2x7) and correct the mounting position. (Recommended mounting screw torque: 0.23 N・m) Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
... □ Instruction sheet (this sheet) □ Installed marking sticker □ General Compliance information and instructions for EU □ Member Registration Please observe the following precautions for safe use of the products. ·When an abnormal condition occurs, immediately stop operation and turn off the product. Contact an OMRON'...
- マニュアル
... wet due to contact with water, chemicals, oil or other liquids, an accident may occur due to short-circuiting or electrification. Do not use the product when wet. ·When an abnormal condition occurs, immediately stop operation and turn off the product. Contact an OMRON'...
- マニュアル
...Firmware version in the sensor controller : FZ/FH/FJ-XXX VerX.XX YYYY/MM/DD Firmware version after upgrade : FH-XXX-UMLIC-08 Ver.X.XX YYYY/MM/DD Language Setting OK Note) For details, refer to the manual provided on OMRON'...
- マニュアル
... the product with foreign materials attached to or caught in. 2. Others -If anything abnormal occurs, for example, strange smell/sound is detected, the main unit gets very hot, or a smoke comes, stop using the product, turn OFF the product, and consult OMRON’...