全 53645 件が検索されました。(6481 - 6500件を表示)
- マニュアル
...めに、時に軽傷・中程度の傷害を負ったり、あるいは物的損害を受けるおそれがあります。 形FL-MD180MC 形FHシリーズ形FH-Sシリーズ、形FZ-Sシリーズ R:赤(Typ 635nm)、G:緑(Typ 525nm)、B:青(Typ 465nm) LED W,B:リスクグループ2、R,G:リスクグループ1 W,G,B:リスクグ...
- マニュアル
... condition is applied to the immunity test of this product. There are case that Lighting brightness fluctuate Max 10%. Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...:ERR) - Stop light emission - Error output ON (parallel DO1:ERR) NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
...側コネクタ」と「照明接続用コネクタ」の内部の凹凸部分を合わせ、カチッと音がするまで差し込みロックします。 形FH-Sシリーズ、形FZ-Sシリーズ形FHシリーズ最大10W、0.9A (FL-TCC1本体と照明部の合計値) 1 形FL-□シリーズ PWM周波数:100KHz 調光ステ...
- マニュアル
...4.5 貫通 9.9 サ ラサ ゙グリ 90deg. 12- M4皿ねじ×4個を使用 :上面 / 下面取付時に使用 形FL-TCC1PS 形FHシリーズ形FH-Sシリーズ、形FZ-Sシリーズ形FL-PSシリーズ 1台 DC24V±10% (リップル成分を含む) 形S8VK-G12024 (オムロン製 DC24V 5A 120W) 3.0A以下定電流駆動方式電流...
- マニュアル
...・Do not use thinners, benzene, acetone, kerosene to clean the product. ・Please wipe the contamination with a soft cloth included a small amount of alcohol. 3.About diffuser plate of UV Lighting. There is a possibility that diffuser plate discolors by usage state, so it'...
- マニュアル
... maintenance on the Diffusion Board.When removing diffuser plate of UV Lighting, influence of static electricity becomes easy to undergo, so please be careful in particular. 7.About diffuser plate of UV Lighting. There is a possibility that diffuser plate discolors by usage state, so it'...
- マニュアル
... DIRECTION TYPE FLV-BR38037PL HORIZON FLV-BR38037PL-V VERTICAL NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
...55.5 5 19.7 68.5 ●FLV-ATC40405-□ 47.5 15 5.4 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
... type SE type BF type 240V 240V - 36 15 47.5 5.4 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...: (49) 7032-811-199 4.1 ■Connecting AC Input Cable NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
... HOLES) 2-M3 INSERT LIMIT5 Tightening torque: 0.54N・m 50 ±0.2 Suitability for Use 200 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...SCREW HOLES) 4-M4 INSERT LIMIT3 34 EMITTING SURFACE 40 40 6 25 ±0.2 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...37 33 ±0.2 27 EMITTING SURFACE 33 3.5Dia. LENGTH0.8M MINIMUM BEND RADIUS20 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...99.8Dia. 114Dia. P.C.D.105 ±0.2 3.5Dia. LENGTH0.8M MINIMUM BEND RADIUS20 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...) M72 60Deg. 60Deg. Tightening torque: 0.54N・m NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
...41.7Dia. EMITTING SURFACE 20 P.C.D.115 112Dia. 61.86Dia. Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...LENGTH0.8M MINIMUM BEND RADIUS20 36.65 Tightening torque: 0.15N・m Suitability for Use ●FLV-EP0803□ Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
....8M MINIMUM BEND RADIUS20 EMITTING SURFACE ●FLV-FB200200□ NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
...0) (1 8) ( 3) ●FLV-FP130□ 30 (MOUNTING SCREW HOLES) 4-M3 INSERT LIMIT3 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...