全 469 件が検索されました。(401 - 420件を表示)
- マニュアル
... Control Unit will not operate normally if the cycle time of the CPU Unit is less than 8 ms. • If the cycle time is less than 8 ms (e.g., the program execution time is short), increase it to at least 8 ms. • For the C200H, ...
- マニュアル
... assigns the words to the Units. Verify I/O Table Compares the I/O table registered in the PC against the I/O Units actually mounted on the PC. Clear I/O Table (CVM1 PCs only) Deletes the I/O tables (C200H and ...
- マニュアル
...1-2-2 Host Link Communications in the CPM1 Operation Manual or 1-2-2 Host Link Communications in the CPM1A Operation Manual for more details. 1-to-1 Link A data link can be created with a data area in another CPM1, CPM1A, CQM1, or ...
- マニュアル
... of the C200H-AD002 Analog Input Unit and the C200H-DA002 Analog Output Unit and includes the sections described below. The C200H-AD002 Analog Input Unit and the C200H-DA002 Analog Output Unit are analog-digital and digital-analog converters designed to work with the C200H or ...
- マニュアル
... I/O Master The CQM1-LK501 I/O Link Unit connects to the following SYSMAC BUS Master Units. Model 1-4 PC C500-RM201 C2000H C1000H (F) C500 (F) CV2000 CV1000 CV500 CVM1 C200H-RM201 C200H/C200HS C200HX/HG/HE Word Allocation The CQM1-LK501 I/O Link Unit is allocated two output and two input words. Master CQM1H/CQM1 Master's area CQM1H/CQM1's area SYSMAC BUS communication 1-4-1 For input (reading) For output (writing) For output (writing) For input (reading) CQM1H/CQM1 Word Allocation The CQM1H/CQM1 treats the CQM1-LK501 I/O Link ...
- マニュアル
.../SK20-C1DT-D Only Item Specifications Transmission path Two-conductor cable (VCTF 0.75 x 2C is recommended) Transmission speed 187.5K bps Transmission distance Total length of 200 m Connectable PC as host CV, CVM1, C2000H, C1000H, C500, C200H, ...
- マニュアル
... any static built-up. Not doing so may result in malfunction or damage. !Caution The cycle time of the CPU Unit must be a minimum of 20 ms. If the cycle time is too short, the PID Control Unit will not operate properly. • For C200H, ...
- マニュアル
.... . . . . . . . . . . . 70 SECTION 4 Master Unit Specifications and Operations . . . . . . . . . . 4-1 C200HW-SRM21-V1 Master Unit for CS-series, C200HX/C200HG/C200HE-(Z)E, and C200HS PLCs . . . . . . . . . . . . . . . . . . . . . 73 74 4-2 CS1W-SRM21 Master Unit for CS-series PLCs . . . . . . . . . . . . . . . . . . . . . . . . . . 88 4-3 CJ1W-SRM21 Master Unit for CJ-series PLCs . . . . . . . . . . . . . . . . . . . . . . . . . . . 104 4-4 CQM1-SRM21-V1 Master Unit for CQM1 PLCs . . . . . . . . . . . . . . . . . . . . . . . . . 126 4-5 SRM1-C0@-V2 Master Control Units . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 136 4-6 CPM2C-S Series CPM2C-S@@@C (-DRT). . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 140 vii TABLE OF CONTENTS SECTION 5 Slave Specifications and Operations . . . . . . . . . . . . . . . . 145 5-1 Remote Terminals . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 147 5-2 Connector ...
- マニュアル
... with other CPU Units. EPROM Memory Cassette With an EPROM Memory Cassette, the program is written using a PROM Writer. The ROM is mounted to the Memory Casette and then installed in the CPU Unit. I/O data cannot be stored. Model Capacity ...
- マニュアル
.... 295 viii About this Manual: This manual describes the installation and operation of the C200H-ASC11/ASC21/ASC31 ASCII Units and includes the sections described below. These ASCII Units can be used with the C200HX/HG/HE, ZE-version C200HX/HG/HE, C200H, ...
- マニュアル
...Console External appearance Model WS02-CXPC@-EV@ CQM1-PRO01-E C200H-PRO27-E CVM1-PRS21-EV1 Note Applicable PLCs CS/CJ-series, C200HX/HG/HE, CVM1-series, and CQM1H-series PLCs C200HX/HG/HE, C200H/C200HS...
- マニュアル
.... . . . . . . . . . . . . . . . . . . 3 1 Section 1-1 Features 1-1 Features The C200H-CT021 High-speed Counter is a Special I/O Unit for the C200H, C200HS, C200HX, C200HG, and C200HE PCs. The High-speed Counter Unit has the following features. Two Built-in Counters The High-speed Counter Unit has two high-speed increment/decrement counters, each of which can be connected to an incremental encoder with open collector output to count line driver input pulses at a rate of 75,000 cps max. Built-in Line Driver Input Circuit An encoder with RS-422 line driver output can be ...
- マニュアル
...500 grams or less (Connectors excluded) External dimensions 130.0 x 34.5 x 100.5 mm (H x W x D) Voltage g fluctuation tolerance Internal current consumption Specifications other than those shown above conform to those for the SYSMAC C200H/...
- マニュアル
... known as the “PC data area interface.” Allocated Words The interface area varies with the type of the PC to which the MC Unit is mounted. Refer to the following examples. Refer to Section 6 PC Data Area Interface for more details. C200H/...
- マニュアル
... link commands. An RS-232C Adapter is used for 1:1 communications and an RS-422 Adapter is used for 1:N communications. One-to-one PC Link A data link can be created with a data area in another CPM1A, CQM1, CPM1, SRM1 or ...
- マニュアル
...peripheral port. (Use Host Link mode when connecting a PT through an RS-232C Adapter.) The RS-232C port on an SRM1-C02-V2 can be used to connect directly to an IBM PC/AT or compatible computer, OMRON PT, or PC (C200HX/HG/HE, ...
- マニュアル
.... 3. A data backup battery must be used when using an absolute encoder. 5 Section System Configuration C200H-MC221 1-2 The following example shows the system configuration when a C200HZ/HX/ HG/HE PC is used. The C200H and ...
- マニュアル
... be used with the SYSMAC-NCT Support Tool. Applicable Position Control Units Corresponding PCs C200HW-NC113/213/413 C200HX/HG/HE(-Z) PCs C500-NC113/211 C-series and CV-series PCs Note The SYSMAC-NCT Support Tool cannot be used with C200H/...
- マニュアル
... operation of the C200H-AD003 Analog Input Unit, the C200H-DA003/DA004 Analog Output Unit, and the C200H-MAD01 Analog I/O Unit and includes the sections described below. The C200H-AD003 Analog Input Unit converts analog sensor output to digital format and transmits it to C200H, ...
- マニュアル
... mounting more than one Master are the same as those for mounting just one Master. Refer to the previous parts of this section for information on settings and operations. When more than one Master Unit is mounted to a CS1 Series, C200HX/HG/HE, or ...