全 469 件が検索されました。(381 - 400件を表示)

  • マニュアル

    ...[][]H-R and CJ1H-CPU[][]H CPU Units. “CJ1H-H-R” is used to indicate only the CJ1H-CPU [][]H-R CPU Units. C Series CVM1/CV Series Serial Communications Unit Indicates products in the OMRON SYSMAC C Series of Programmable Controllers: ...

  • マニュアル

    ...-E1-@ SYSMAC CPM1A Operation Manual SYSMAC CPM2A Operation Manual W317-E1-@ W352-E1-@ SYSMAC CPM2C Operation Manual SYSMAC C200H Operation Manual (for CPU01/03/11) (Programming) W356-E1-@ W130-E1-@ SYSMAC C200H Operation Manual (for CPU21/23/31) (Programming) SYSMAC ...

  • マニュアル

    ... Applicable PLCs The OMRON PLCs listed below can be connected as hosts using Host Link communications. The connection can be made either directly to the built-in serial port on the CPU Unit or to a Host Link Unit mounted to the PLC. C Series ...

  • マニュアル

    ... Connector Connected to the CompoBus/S Network. The cable connector is mounted in the connector at the factory. RS-232C Connector Connected to Programming Devices. Cannot be used when the Expansion Option Board is connected. Expansion I/O Connector Connected to the ...

  • マニュアル

    ... following PLCs support the C-series Host Link protocol. (Not all of the above FINS commands are supported by each of the PLCs.) C20, C50, C120, C120F, C20H/C28H/C40H/C60H, C20P/C28P/C40P/C60P, C20PF/C28PF/C40PF/C60PF, C500, C500F, C1000H, C1000HF, C2000H, C200H, ...

  • マニュアル

    ... I/O data to event memory and read/write event memory. • Send/receive FINS messages to/from devices on the DeviceNet network (only for devices that support FINS). (Not all devices support FINS communications functions with Open Network Controllers (e.g., C200HX/HE/HG or ...

  • マニュアル

    ...-CPU01-E/CPU03-E/CPU11-E Programmable Controllers Installation Guide C200H Programmable Controllers (CPU01-E/03-E/11-E) Installation Guide Revised January 2001 iv 3232 Notification of and Request Related to Circuit Specification Changes to I/O Units for SYSMAC C200H, ...

  • マニュアル

    ... C200H Master. C200H Slave Rack C200H Slave Rack Remote Interface G7TC I/O Block C200H Slave C500 Master Remote Terminal ! Caution 16 When C200H Slave Racks are connected to Masters on PCs other than the C200H/...

  • マニュアル

    ... of the C200H-AD001 Analog Input Unit and the C200H-DA001 Analog Output Unit and includes the sections described below. The C200H-AD001 Analog Input Unit and the C200H-DA001 Analog Output Unit are analog-digital and digital-analog converters designed to work with the C200H or ...

  • マニュアル

    ...-CE001 F Adapter Cover --- C1000H-COV01 Communications C bl Cable Coaxial cables Auxiliary Power Supply Unit For use with the C200H-SLK11 C200H-APS03 Must be mounted to leftmost 2 slots on Rack with C200H-CPU11-E ...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Reducing Response Time (C200H, C200HS, C200HX/HG/HE(-Z)) . . . . . . . . . . . . . . . . Programming Examples . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 7 Error Processing . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7-1 7-2 7-3 SR Area Flags . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Error Examples . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Error Tables . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 8 Inspection and Maintenance . . . . . . . . . . . . . . . . . . . . . . . Appendix A Standard Models . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . B Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Glossary . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . vii About this Manual: A PC Link System enables use of the LR (Link Relay) data area as a common data area shared by all PCs in the PC Link System, thus simplifying programming, settings, and data exchange between PCs and permitting effective use of inputs and outputs. This manual has been written to provide the ...

  • マニュアル

    ...3G2A5-RPT01-(P)E required for more than 32 Units. Note If a Unit with the blown-fuse detection function and alarm detection circuit (C200H-OD411/213/214/OA221) is used on a C200H Slave Rack that is connected to a PC other than a C200H/...

  • マニュアル

    ...Data area 0 DM 1 IR 2 LR 3 HR 4 AR Note Use only the following words in the DM and IR areas: DM 0000 to DM 1999 and IR 000 to IR 235. Although the C200HS provides larger areas, if any words not within the specified ranges are used, an error will occur and an error code of 34 will be output. Number of Transfers Word n+3, bits 15 through 08 Set to between 1 and 3. When changing range parameters, data for up to three ranges can be transferred at the same time. When transferring the ...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Communications Protocol (C200HS/HX/HG/HE only) . . . . . . . . . . . . . . . . . . . . . . . . . . Frame Checksum (FCS) Calculation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 4 Commands and Responses . . . . . . . . . . . . . . . . . . . . . . . . 4-1 4-2 4-3 4-4 4-5 4-6 4-7 4-8 4-9 4-10 4-11 4-12 4-13 4-14 4-15 4-16 4-17 4-18 4-19 4-20 TEST . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . STATUS READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ERROR READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . IR AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . HR AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . AR AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . LR AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . TC STATUS READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . DM AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . FM INDEX READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . FM DATA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . PV READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SV READ 1 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SV READ 2 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SV READ 3 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . STATUS WRITE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . IR ...

  • マニュアル

    ... Section: ASCII Unit Refresh timing Words n to n+2 OUT refresh Word n+3 IN refresh 4 words are used (n: 100 + 10 + unit no.) Transferred to each Unit every time the I/O data is refreshed. SYSMAC C200H, ...

  • マニュアル

    ... addresses that are not listed in the table cannot be specified. 2. When specifying words in the DM area that are allocated to Special I/O Units (DM20000 to DM20999), you must specify word addresses used for the Special I/O Unit area in C200HX/HG/HE, ...

  • マニュアル

    ... Node Bypass (optical systems only) functions prevent the network from failing when one Unit fails. The Internode Echo Test function aids in communications troubleshooting. Remote monitoring of the network’s operating status also aids in troubleshooting and quick correction of communications problems. Improvements on the ...

  • マニュアル

    ... words of data is returned in each frame. A total of 30 words of data is returned in each frame. Applicable models C-series Host Link Units Built-in RS-232C ports or peripheral ports on SRM1, CPM1, CPM1A, CQM1, ...

  • マニュアル

    ... by a single C200H CPU and up to 4 Special I/O Units can be mounted on a Slave Rack. C500-SU981-E Fuzzy Support Software IBM PC/AT or compatible C200H-FZ001 Fuzzy Logic Unit Mouse SYSMAC C200H C200HS C200HX C200HG C200HE C200H-AD001 Analog Input Unit C200H-DA001 Analog Output Unit RS-232C connecting cable (9 pin to 9 pin or 9 pin to 25 pin) Note Do not mount the C200H-FZ001 in the 2 slots next to the CPU on the CPU Rack. 2 Section 1-3 Fuzzy Logic Theory 1-3 Fuzzy Logic Theory...

  • マニュアル

    ...] C200H-CPU21-E/CPU23-E/CPU31-E Programmable Controllers Installation Guide C200H Programmable Controllers Installation Guide (For CPU21-E/23-E/31-E) Revised April 2000 3232 Notification of and Request Related to Circuit Specification Changes to I/O Units for SYSMAC C200H, ...