全 126 件が検索されました。(21 - 40件を表示)

  • マニュアル

    ...c-o 0.0 50.0 sp-0 Alarm Value 4 *2 0 Monitor (Unit: A) *5 Heater Burnout Detection 1 (Unit: A) *5 sp-3 8.0 i 233 8.0 c-i SP 1 233 c-d SP 2 PV input Slope Coefficient 40 c-db SP 3 Proportional Band 0 oapt 0 M icpt 1 wtpt off M pfpt off Operation / Adjustment Protect Restricts displaying and modifying menu items in Operation, Adjustment, and Manual Control Levels. Initial Setting / Communication Protect Restricts movement to the Initial Setting, Communications Setting, and Advanced Function Setting Levels. 0.0 sprt off...

  • マニュアル

    ...率极限 0.0 M spmd 在U 程序SP模式下1秒钟以上 0 分段编号 orl 40%AT执行at-1 M 操作菜单的 PV/SP(1)(2) 25 M v-m 转至高级功能设定菜单 M 0 ON OFF 31 M cmwt 0 to 7时 M pid 25 X D 程序编号 0 X end Eend时 0 ∗电压输出(用于驱动SSR):2 − V 程序No.监控/ 分段...

  • マニュアル

    ...算启用 (限于已经设定了模拟输入) 0 X X 13 14 15 RS-485 A(-) 14 15 16 M cmwt 操作菜单的 PV/SP(1)(2) 25 M 分段编号 M c-o 在使用本产品时,请务必外接说明书上推荐的保险丝。 符合EN/IEC标准 13 020 通信、4个事件输入、2个 CT和转换输出 B(+) 0 ·默认的报警类...

  • マニュアル

    ... according to the error code, referring the table below. s.err (S. Err) e333 (E333) e111 (E111) Action Meaning Input error *2 A/D converter error *2 Memory error 20 21 M M SP 1 17 18 19 M M SP 0 13 14 15 16 M M HS Alarm 2 (Unit: A) *7 17 18 19 M SP 6 M Leakage Current 2 Value Monitor (Unit: A) *7 16 M SP 5 M Heater Burnout Detection 2 (Unit: A) *7 0 sp-2 hys *6 M 0 ...

  • マニュアル

    ...分时间 c-i (冷却) c-db 停止时的MV 0.0 M ∗6 ∗6 等待区间 off M SP 2 保温时间 1 M M SP 1 滞后 (加热) 1.0 soak 保护菜单平方根的运算启用(限于已经设定了模拟输入) 20 21 当发生一个错误时,第一显示将显示错误代码。 参考下表,根据错误代码采取适...

  • マニュアル

    ...经过输入偏移后过程值按照198.8°C处理。 限制可以显示或改变的设定类型以及通过按键操作进行的更改。 ON OFF SP 1 M M 转至高级功能设定菜单 0 M M M SP 0 M MV监控(冷却) 40 M soak 0 M sp-3 0.0 HS报警1 (单位:A)∗5 M M c-o 漏电流1值监控 (...

  • マニュアル

    .... Event input contact Control status ON (closed) RUN OFF (open) STOP 4-5-3 Using the Multi-SP The multi-SP function is used to switch between two SPs. Different SPs are set in advance for SP 0 and SP 1...

  • マニュアル

    ...143 144 145 Data name Alarm lower limit value 1 Alarm value 2 Alarm upper limit value 2 Alarm lower limit value 2 Alarm value 3 Manual manipulated variable Heater burnout detection SP 0 SP 1 Temperature input offset value Upper limit temperature input offset value Lower limit temperature input offset value Proportional band Integral time Derivative time Cooling coefficient Dead band Manual reset value Heating hysteresis Cooling hysteresis Section 4-3 Temperature Controllers that support setting Pulse Analog output output type type Temperature Controller variable area address ch1 ch2 Variable Address Variable Address type type Yes Yes C1 0006...

  • マニュアル

    ... lower limit values .......................4-6 terminal arrangement.......................................................... 2-5 shift method ......................................................................3-17 E5CS-U .......................................................................... 2-5 shifting input values..........................................................3-16 E5CSV ........................................................................... 2-5 shifting inputs ...................................................................3-16 tuning ................................................................................ 5-10 short-circuit........................................................................ A-7 ...

  • マニュアル

    ... changed automatically, even if the input type or SP Limiter is changed. Use an event input or operation command to switch between the remote SP and local SP. When using an event input for switching, set the Event Input Assignment to Local SP (0)/Remote ...

  • マニュアル

    ...Selection 2. The current bank number will be displayed. Press the O Key to move the bank setting level. 0 3. Press the U or D Key to set 3. d.bnk 3 C 3.lsp Bank 3 SP 1 4. Select the Bank 3 SP parameter by pressing the M Key. 3.lsp Bank 3 ...

  • マニュアル

    ... relationships between the ON/OFF status of multi-SP number switching bits 0 to 2 and the set point. Selected set point Multi-SP No. switching bits Bit 0 Bit 1 Bit 2 SP 0 OFF OFF OFF SP 1 ON OFF OFF SP 2 OFF ON OFF SP 3 ON ON OFF SP 4 OFF OFF ON SP 5 ON OFF ON SP 6 OFF ON ON SP 7 ON ON ON Note: Any bits that are not assigned to event inputs are treated as being OFF.  Using Key Operations You can select any of the set ...

  • マニュアル

    ... Lower Limit 1 Alarm Value 2 Alarm Value Upper Limit 2 Alarm Value Lower Limit 2 Alarm Value 3 Alarm Value Upper Limit 3 Alarm Value Lower Limit 3 Heater Burnout Detection 1 SP 0 SP 1 SP 2 SP 3 Process Value Input Shift PV Input Slope Coefficient Proportional Band Setting (monitor) value Level Protect H'00000000 (0): No restrictions in operation and adjustment levels H'00000001 (1): Move to adjustment level is prohibited. H'00000002 (2): Display and change of only "PV" and "PV/SP" parameters is allowed. H'00000003 (3): Display of only "PV" and "PV/...

  • マニュアル

    ...PV/SP/Program No. Monitor and Segment No. Monitor PV/SP/MV (Heating) (Valve Opening for Position-proportional Models) PV/SP/MV (Cooling) 4 PV/SP/Remaining Segment Time 5 Program Number 2 Can be set. (SP)*1...

  • マニュアル

    ... a section reference for a setting item, refer to that reference for details. Variable type C0 (80) 0000 PV C0 (80) 0001 Status *1*2 C0 (80) 0002 C0 (80) 0003 C0 (80) 0004 Present SP *1 Heater Current 1 Value Monitor MV Monitor (Heating) C0 (80) 0005 C0 (80) 0006 C0 (80) 0007 C0 (80) 0008 C0 (80) 000A C0 (80) C0 (80) 000D 000E Address Parameter name Setting (monitor) value Level Temperature: Use the specified range for each sensor. Operation Analog: Scaling lower limit −5% FS to Scaling upper limit +5% FS Refer to 3-2 Status ...

  • マニュアル

    ...SP 63% of the SP change width PV Standby time = Integral time (I) Thermac Simulator Operation Manual (H190) Temp. rise time 6 times the temperature rise time 4-1 Phase Changes during Log Data Collection Settling width: ...

  • マニュアル

    ... by operating the keys on the front panel or by using external input signals (event inputs). 5  Using Event Inputs Multi-SP No. switching bits Bit 0 Bit 1 Bit 2 SP 0 OFF OFF OFF SP 1 ON OFF OFF SP 2 OFF ON OFF SP 3 ON ON OFF SP 4 OFF OFF ON SP 5 ON OFF ON SP 6 OFF ON ON SP 7 ON ON ON Note: Any bits that are not assigned to event inputs are treated as being OFF. E5@D Digital Temperature Controllers User’s Manual (H224) 5 - 33 5-...

  • マニュアル

    ... Lower Limit 1 Alarm Value 2 Alarm Value Upper Limit 2 Alarm Value Lower Limit 2 Alarm Value 3 Alarm Value Upper Limit 3 Alarm Value Lower Limit 3 Heater Burnout Detection 1 SP 0 SP 1 SP 2 SP 3 Process Value Input Shift PV Input Slope Coefficient Proportional Band Setting (monitor) value Level Protect H'00000000 (0): No restrictions in operation and adjustment levels H'00000001 (1): Move to adjustment level is prohibited. H'00000002 (2): Display and change of only "PV" and "PV/SP" parameters is allowed. H'00000003 (3): Display of only "PV" and "PV/...

  • マニュアル

    ... settings. For setting (monitor) ranges, refer to the applicable parameter. 0 Setting*2 Set value *1 *2 5 - 78 Remarks Monitor/Setting Display 0 1 Disabled PV/SP/Bank No. Can be set. (SP)*1 ----- 2 PV/SP/MV (Heating) Can be set. (...

  • マニュアル

    ...指定します。 • 小数点形式 小数点形式の場合(C=&0) - 1.23456 文字列(ASCIIコード) に変換 2D 20 20 31 2E 32 33 34 35 36 (−) (SP) (SP) (1) (.) (2) (3) (4) (5) (6) 注:(SP)は半角スペースを意味します 例:-1.23456 S 浮動小数点データ S+1 87 数部桁数(文字数)を指定します。 D 以降への格納...