全 3026 件が検索されました。(2961 - 2980件を表示)
- マニュアル
... the front Panel may cause errors. Setting distance L (mm) Model Dimensions Installation distance The following graphs show the relationship between detection range and setting distance for each model of Sensor Head. Values differ according to each model of Sensor Head, ...
- マニュアル
... CISPR11 class A . The intended use of this product is in an industrial environment only. 9.8 The following graphs show the relationship between detection range and setting distance for each model of Sensor Head. Values differ according to each model of Sensor Head, ...
- マニュアル
... front Panel may cause errors. 17.90 32 Smart Sensor For Model ZFX-C□□ Sensor head unit 0.80 4.5 ZFX-SC50S ・ Do not peel off or probe the ventilation film with a sharp-pointed object. If you so, the specifications of the protective structure may no longer be satisfied. ・ Do not block the ventilation film. Doing ...
- マニュアル
...The product is considered to be classified as Risk Group 1 by IEC62471. 2-M4 depth 6 The following graphs show the relationship between detection range and setting distance for each model of Sensor Head. Values differ according to each model of Sensor Head, ...
- マニュアル
...INSTRUCTION SHEET 17.9 32 Smart Sensor For Model ZFX-C□□ Sensor head unit The following graphs show the relationship between detection range and setting distance for each model of Sensor Head. Values differ according to each model of Sensor Head, ...
- マニュアル
... the power supply separately from other devices. Wiring them together or placing them in the same duct may cause induction, resulting in malfunction or damage. 4. Cleaning ・ Do not use paint thinner, benzene, acetone or kerosene to clean the Sensor Controller. Doing ...
- マニュアル
... exclusive power supply to the ionizer. 3. Applicable standards ・EN61326-1 ・Electromagnetic environment : Industrial electromagnetic environment (EN/IEC 61326-1 Table 2) 4. Other ・Do not bring your fingers or metal objects into close contact with the discharge needles. Doing ...
- マニュアル
... short-circuited. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing them in the same duct may cause induction, resulting in malfunction or damage. • Avoid connecting or disconnecting connectors while the product is powered on. Doing ...
- マニュアル
... air by corona discharge and blowing ions on the charged object by a fan. • To neutralize electricity, proprietary mixing variable DC mechanism is used to materialize quick neutralization and excellent ion balance. • Its Auto Ion Control function maintains the best ion balance. • Indicators are equipped ...
- マニュアル
... air by corona discharge and blowing ions on the charged object by a fan. To neutralize electricity, proprietary mixing variable DC mechanism is used to materialize quick neutralization and excellent ion balance. Its Auto Ion Control function maintains the best ion balance. Indicators are equipped ...
- マニュアル
... short-circuited. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing them in the same duct may cause induction, resulting in malfunction or damage. • Avoid connecting or disconnecting connectors while the product is powered on. Doing ...
- マニュアル
... warning Indication WARNING Indicates a potential hazardous situation that improper handling may cause death or serious injury. WARNING Be sure to configure the circuits for safety protection such as emergency stop circuits, interlock circuits, and/or limit circuits to the external control circuits ...
- マニュアル
... must be within the rated range. 5. Use the power supply within the rated load. 6. Dispose of this product as industrial waste. 4. Cleaning ・Do not use paint thinner, benzene, acetone or kerosene to clean the Data Storage Unit. Doing ...
- マニュアル
... moderate injury or in property damage. ●Alert Statements in This Sheet WARNING This product is not designed or rated for ensuring safety of persons either directly or indirectly. Do not use it for such purposes. Do not disassemble the product. Doing ...
- マニュアル
... moderate injury or in property damage. ●Alert Statements in This Sheet WARNING This product is not designed or rated for ensuring safety of persons either directly or indirectly. Do not use it for such purposes. Do not disassemble the product. Doing ...
- マニュアル
... to PRECAUTIONS FOR SAFE USE on the Instruction Sheet of the dedicated Controller (ZW-CE1□□/ZW-C1□□□). • Tighten the mounting screw to the torque specified in this instruction sheet. • Always turn off the power of the main unit before taking the following actions. Not doing ...
- マニュアル
..., refer to PRECAUTIONS FOR SAFE USE on the Instruction Sheet of the dedicated Sensor Controller (ZW-5000□). • Tighten the mounting screw to the torque specified in this instruction sheet. • Always turn off the power of the main unit before taking the following actions. Not doing ...
- マニュアル
..., refer to PRECAUTIONS FOR SAFE USE on the Instruction Sheet of the dedicated Sensor Controller (ZW-5000□). • Tighten the mounting screw to the torque specified in this instruction sheet. • Always turn off the power of the main unit before taking the following actions. Not doing ...
- マニュアル
... to PRECAUTIONS FOR SAFE USE on the Instruction Sheet of the dedicated Controller (ZW-CE1□□/ZW-C1□□□). • Tighten the mounting screw to the torque specified in this instruction sheet. • Always turn off the power of the main unit before taking the following actions. Not doing ...
- マニュアル
...Do not touch the end face of the fiber cable. It may result in deterioration in performance. If it is touched or contaminated, wipe out contamination with a commercial fiber connector cleaner or soft cloth. Do not use a cloth containing alcohol. Doing ...