全 3026 件が検索されました。(2941 - 2960件を表示)

  • マニュアル

    ... go undetected, resulting in serious injury. Make sure to install the F3SG-R at the safety distance from the hazardous part of the machine. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...

  • マニュアル

    ... stop before a person reaches the hazardous part, resulting in serious injury. iv SCC-1224A Safety Mat / Edge Controller User Manual Introduction Serious injury may occur due to loss of required safety functions. Wire the SCC-1224A Safety Mat/ Edge Controller properly ...

  • マニュアル

    ... protection Install the latest commercial-quality antivirus software on the computer connected to the control system and maintain to keep the software up-to-date. Security measures to prevent unauthorized access Take the following measures to prevent unauthorized access to our products. • Install physical controls ...

  • マニュアル

    ... using the FH/FZ5, be sure to observe the following: • The FH/FZ5 must be operated by personnel knowledgeable in electrical engineering. • To ensure correct use, please read this manual thoroughly to deepen your understanding of the product. • Please keep this manual in a safe place ...

  • マニュアル

    ... using the FH/FZ5, be sure to observe the following: • The FH/FZ5 must be operated by personnel knowledgeable in electrical engineering. • To ensure correct use, please read this manual thoroughly to deepen your understanding of the product. • Please keep this manual in a safe place ...

  • マニュアル

    ... Units together and locking the sliders by moving them toward the back of the Units. The End Cover is connected in the same way to the Unit on the far right side of the Controller. A step in a procedure 1 Join the Units ...

  • マニュアル

    ... using the FH/FZ5, be sure to observe the following: • The FH/FZ5 must be operated by personnel knowledgeable in electrical engineering. • To ensure correct use, please read this manual thoroughly to deepen your understanding of the product. • Please keep this manual in a safe place ...

  • マニュアル

    ... possibly occur due to breakdown of safety outputs or test outputs. Do not connect loads beyond the rated value to the safety outputs and test outputs. Serious injury may possibly occur due to loss of required safety functions. Wire the NE1A-series Controller properly ...

  • マニュアル

    ... then consult a physician. Personal injury may occasionally occur. Stop using the Product immediately if leaked fluid or an unusual odor from the Battery Pack or clock battery is detected. • If there are flames nearby, move the Product away from the flames. Failure to do ...

  • マニュアル

    ...Serious injury may possibly occur due to breakdown of safety outputs or test outputs. Do not connect loads beyond the rated values to the safety outputs and test outputs. Serious injury may possibly occur due to loss of required safety functions. Wire the G9SPseries Controller properly ...

  • マニュアル

    ... safe use of this products. [ Circuit Design ] I5 Load Precautions for Safe Use I4 Load Fire may occasionally occur. Tighten the terminal block screws to the specified torque 5∼5.3in-lb.(0.565 to 0.6 N•m) ...

  • マニュアル

    ...For Model ZFV-CA□□ Sensor head unit Setting distance L (mm) 32 ZFV-SC10□ The following graphs show the relationship between detection range and setting distance for each model of Sensor Head. Values differ according to each model of Sensor Head, ...

  • マニュアル

    ...販売拠点は、Webページでご案内しています。 A v 2 0 1 4 年 7月 (4) Ventilation Film ・ Do not peel off or probe the ventilation film with a sharp-pointed object. If you so, the specifications of the protective structure may no longer be satisfied. ・ Do not block the ventilation film. Doing ...

  • マニュアル

    ... thoroughly to acquire sufficient knowledge of the product. For your convenience, keep the sheet at your disposal. The following graphs show the relationship between detection range and setting distance for each model of Sensor Head. Values differ according to each model of Sensor Head, ...

  • マニュアル

    ... interference. 100 30 10 (6) Maintenance and Inspection (2) Receiver part © OMRON Corporation 2008-2015 All Rights Reserved. 300 30.10 ZFV-SC50S ・ Do not peel off or probe the ventilation film with a sharp-pointed object. If you ...

  • マニュアル

    ... the front Panel may cause errors. © OMRON Corporation 2006-2015 All Rights Reserved. ●Meanings of Signal Words The following graphs show the relationship between detection range and setting distance for each model of Sensor Head. Values differ according to each model of Sensor Head, ...

  • マニュアル

    ... at a detection range of 25 mm required for the location of the sensing object, the setting distance of Sensor Head becomes 95mm. 30.10 Model ・ Do not peel off or probe the ventilation film with a sharp-pointed object. If you ...

  • マニュアル

    .... Do not exert unnecessary force to turn the control at the upper or lower limit positions as this might damage the control. Item Mounting fixture can be attached on each side. Workpiece Focus can be verified by the green guide light. Adjust ...

  • マニュアル

    ...(3) RS-232C PULL OPEN 4 DIN track (sold separately) PFP-100N (1 m) PFP-50N (0.5 m) PFP-100N2 (1 m) (2) 4 SET 1 Exhaust Unit 4.2 Vertilation ・ Install the Controller so that the distance between the Controller and other devices is at least the dimensions shown in the figure below to improve the ventilation. When installing Controller only: 3 (1) (3) ESC Right Wrong 2 (9) PFP-M 2 RUN AUTO ・Attach the Exhaust Unit (supplied) to the Controller when installing other devices adjacently on the same DIN track as the End Plate (sold ...

  • マニュアル

    ...CARD MENU ADJ RUN AUTO ESC SET 1 2 3 4 DIN track (sold separately) PFP-100N (1 m) PFP-50N (0.5 m) PFP-100N2 (1 m) 5.2 Ventilation ・ Install the Controller so that the distance between the Controller and other devices is at least the dimensions shown in the figure below to improve the ventilation. When installing Controller only: Min. 15 mm Min.50 mm TRIG signal Mode Input voltage ON current *1 ON voltage *1 OFF current *2 OFF voltage *2 ON delay OFF delay Internal circuit diagram NPN 12 to 24 VDC ±10% 5mA min....