全 279 件が検索されました。(261 - 279件を表示)
- マニュアル
...Select “L. Load image.” All the image data in the memory card will be displayed. Freeze T. Unfreeze/Freeze : Unfreeze Freeze I. Input image L. Load image S. Save image E. End Loading Image Data STD_CAP.IMG BOTTLE CAP Scn02 Fram0 Raw Frz 151896 80–01–01 W0123 01234567 CAL CA OFF CARD OK 4. Select the filename of the file that is to be loaded. A message will be displayed asking for confirmation. 85 Displays Section 4-2 5. Select “X. Execute.” After the loading has been completed, a message will be displayed asking for confirmation. Freeze T....
- マニュアル
..., and V690-L01 • Do not use any organic thinners. Resin materials and the case paint are dissolved by thinner. Laws and Standards 1. Japan The V690 is covered under the Specified Low-Power Wireless Station - Wireless Equipment for Mobile Object Identification (ARIB RCR ...
- マニュアル
... indicator The RUN indicator turns ON in the RUN mode. (3) Control keys The Control Keys are for setting measurement conditions and other information. Displays and Key Operations (4) p.47 Menu selector switch This switch selects the setup menu. ...
- マニュアル
... (1997) EN 60065 2. FCC Rules (Federal Communications Commission) FCC Part 15 Subpart C 3. Japan Radio Law Equipment using high frequencies: Inductive Reading/Writing Communications Equipment, Identification No. EC-04023 Conforming standards: Inductive Reading/Writing Communications Equipment; Standard: ARIB ...
- マニュアル
...) Sensor Head connector (1) OUTPUT indicator (2) RUN indicator (3) ERR indicator (4) READY indicator OUTPUT RUN ERR READY (8) LCD monitor A B C D TEACH /VIEW (7) Control keys ADJ STD EXP MENU RUN (5) Menu selector switch ESC SET (6) Mode selector switch (10) Coupler (13) RS-232C connector (12) USB port (11) I/O cable No. Name Description (1) OUTPUT indicator The Output indicator lits when the OUTPUT signal turns ON. (2) RUN indicator The RUN indicator turns ON in the RUN mode. (3) ERROR indicator The ERROR indicator turns ON when an error is ...
- マニュアル
... conditions. ADJ : Select this mode when adjusting the judgment threshold value. RUN : Select this mode when performing measurement. Measurement results and judgment results are output only when the RUN mode is currently selected. (3) Menu switch This switch selects the setup menu. ...
- マニュアル
...To check the details of values further, tap [Details of data]. 8. Adjust the processing item by referring to the displayed content. In the following example, Correlation values are clearly lower on some screens. Based on the revealed cause of false judgement, use the [Set up(...
- マニュアル
...FGS 2.1.1 Display Unit The status indicator colors combined with the indicator status show the air flow status and errors. Status Indicator Definition The air flow rate exceeds the upper threshold. Orange Blink Factory default setting: 1000 L/min (...
- マニュアル
...folder Analyzing inspection and measurement results (NG analyzer) 163 8 Adjust the processing item by referring to the displayed content. In the following example, Correlation values are clearly lower on some images. Based on the revealed cause of incorrect judgement, use the [Set up(...
- マニュアル
...かけて取付けてください。 入出力コード側のフックをレールにかけて取付けると取付け強度が低下します。 ADJ STD EXP MENU RUN (4)メニュー切替えスイッチ (3) OUTPUT※ ■入出力段回路図 1. コネクタ側のツメを DIN レールに引っかけます。 2. 入出力コード...
- マニュアル
...)操作キー計測条件など設定するための操作キーです。 (6) メニュー切替えスイッチ設定メニューを切替えます。 STD…標準メニュー。 計測で必要な最低限の項目を設定するときに選択します。 EXP…エキスパートメニュー。 より詳細な設定をす...
- マニュアル
...)操作キー計測条件など設定するための操作キーです。 (6) メニュー切替えスイッチ設定メニューを切替えます。 STD…標準メニュー。 計測で必要な最低限の項目を設定するときに選択します。 EXP…エキスパートメニュー。 より詳細な設定をす...
- マニュアル
...択します。 RUN:通常計測するときに選択します。 52.5 60 (6) メニュー切替スイッチ設定メニューを切替えます。 STD:標準メニュー。 計測で必要な最低限の項目を設定するときに選択します。 EXP:エキスパートメニュー。 より詳細な設定をするとき...
- 商品情報
...を利用する「小エリア無線」であり、免許申請が必要である。 WM51 は ARIB の標準規格「小エリア無線通信システムの無線設備(STD-44)」(1994 年に規格化)に適合しており、 機器毎に「自局のシリアル No」として「機器固有の値」を、不揮発性メモリに保持している。...
- 商品情報
...と判定し、安全停止検知出力をONします。■標準設定の場合:モータの逆起電力が10mV以下になったとき 設定方法:背面SWを「STD」にしてください。前面の「SET」ランプは消灯します。 ■ユーザ設定の場合:停止検知入力電圧が100mV以下の状態で、停止判定時...
- 商品情報
...合、電源ON時自動転送用プログラムファイルを作成することは可能ですが電源ON時自動転送用パラメータファイル(.STD)を作成することはできません。STDファイルの作成には、PLCが必要です。 商品情報 FA統合ツールパッケージ CX-One CXONE-AL□□C-...
- 商品情報
...プションメニューから[AUTOEXECファイルで転送]をチェックしてCPUユニット→メモリカード転送の操作を実施パラメータAUTOEXEC.STD◆オンライン作成(パソコン+PLC)CX-ProgrammerのPLCメモリカードのオプションメニューから[AUTOEXECファイルで転送]をチェックして...
- 商品情報
...ータ付き転送の場合「データファイル」: AUTOEXEC.IOM , ATEXECDM.IOM , ATEXECE□.IOM ※1 または AUTOEM□□.IOM ※2「プログラムファイル」: AUTOEXEC.OBJ「パラメータファイル」: AUTOEXEC.STD上記の場合、「パラメータファイル」と「プログラムファイル」は必須です。また、パラメータが実際の構成と矛盾している...
- 商品情報
...る場合に必要なファイルを教えてください。からご参照ください。AUTOEXEC名のプログラムファイル(.OBJ)、パラメータファイル(.STD)付きで作成する場合は、実際のPLC構成が必要となります。パラメータファイル(.STD...