全 2904 件が検索されました。(2721 - 2740件を表示)
- マニュアル
.... Center of Gravity and Axis Angle → p. 67, 147 The binary axis angle can be used to calculate the orientation (i.e., the binary axis) of the measurement object, in addition to the center of gravity and area. Binary axis searches increase processing time, ...
- マニュアル
... recognition is required, use a UL class II power supply. 11 Section 2-4 Camera 2-4 Camera The camera is designed for the V530-R150. Mounting the Camera The specified camera distance is only an approximation. Mount the Camera ...
- マニュアル
... recognition is required, use a UL class II power supply. 11 Section 2-4 Camera 2-4 Camera The camera is designed for the V530-R150. Mounting the Camera The specified camera distance is only an approximation. Mount the Camera ...
- マニュアル
...Camera 1 Connected to Camera 0 Push up pin 1 on the DIP switch. Connected to Camera 1 Shift pin 1 to the right. Camera Only The same Camera is also available without a lens and light source so that standard CCTV lenses and lights can be used. Use C-mount lenses. Camera Camera Model F150-S1A !Caution The F150-S1A Camera must be used with the F150. Using other Cameras can damage the F150 or the Camera. 17 Z141-E1-03.book Page 18 Monday, July 24, 2006 5:16 PM Section 2-5 Cameras with Light Sources Distance ...
- マニュアル
...measurement region Average density within measurement region: 200 Relative Search Use this method to obtain the positions of markings, holes, and other features, and to judge whether these features are within the acceptable range. This method is based on relative position, ...
- マニュアル
... 1 TOR + 24VD -1.2A C Cooling vents Before the F160 is shipped, a protective label is attached to the top of the F160 to cover the cooling vents. This label prevents wire strands from falling into the F160 during wiring, ...
- マニュアル
... that the inspection object is displayed on the monitor screen. 0.Scn 0 MON ---- ---ms For a new scene, press ENT at MON and then select SET from the menu. If it is not displayed, adjust the position of the inspection object ...
- マニュアル
... external device's delay time. The default setting is 1.0 ms. 3 Section 1-2 I/O Format Item Settings Set the length of time that the GATE signal remains ON. Set a value between 1.0 and 1,000 ms so that the external device can read the measurement result. The default setting is 5.0 ms. Gate ON time (Effective only when handshaking is OFF.) A timeout error will occur if there is no response from the external device within the timeout time. Set a value between 0.5 and 120.0 s. The default setting ...
- マニュアル
...area and center of gravity, use a gravity and area measurement. 7 Section 1-2 Types and Features of Measurement Methods OCR for 1 Character Use an OCR for 1 character measurement to recognize alphanumeric characters and special symbols. The F160 provides a dictionary, ...
- マニュアル
... subject to splashing water, oil, or chemical substances. ♦ Installation • This device uses the frequency band 13.56 MHz to communicate with a tag. This frequency band 13.56 MHz is used also as the ISM band (one of frequencies assigned to medical or industrial heater; ). ...
- マニュアル
... min. (See note.) Note: The parallel installation distances of 4.5 and 6 m minimum given above assume that there is no radio wave reflection. Any metal in the surrounding area will affect the installation distance. It may be necessary to program the system ...
- マニュアル
...cables. • Do not remove the core connected to the Scanner Cable (V530W001). • Do not lay cables with power cables to reduce the possibility of noise affecting operation. • Install cables well away from motors, arc welders, electromagnetic switches, and other possible sources of noise. • Lay cables ...
- マニュアル
... to take a Fiber Amplifier Sensor Communication Unit apart, to repair a Fiber Amplifier Sensor Communication Unit, or to modify a Fiber Amplifier Sensor Communication Unit in any way. • Never attempt to wire a Fiber Amplifier Sensor Communication Unit while power is being supplied. Doing ...
- マニュアル
... 182 Enlarge 5 Section 1-2 Functions Store Images Up to 24 images can be stored in memory. The images can be used to check what kind of errors have occurred. The stored images will be cleared when the power goes OFF, ...
- マニュアル
... laser beam path is terminated during use. If a mirror or shiny surface is positioned in the laser beam path, ensure that the reflected beam path is also terminated. If the Unit must be used without terminating the laser beam path, position the laser beam path ...
- マニュアル
...path is terminated during use. If a mirror or shiny surface is positioned in the laser beam path, ensure that the reflected beam path is also terminated. If the Unit must be used without terminating the laser beam path, position the laser beam path ...
- マニュアル
...Define Compensate the Measured Height and Position To compensate for the error, perform the measurement twice. Applicable measurement items: Height, Edge position, Edge center, Peak/bottom Example 1: When selecting Height Workpiece height: 10 mm Use the method shown below to calibrate workpieces ...
- マニュアル
... the laser beam path is terminated during use. If a mirror or shiny surface is positioned in the laser beam path, ensure that the reflected beam path is also terminated. If the Unit must be used without terminating the laser beam path, position the laser beam path ...
- マニュアル
... for monitoring the measurement status for each output. Refer to page 104. 15 Section 1-1 Menu Operation Trend Monitor Mostly used for setting and checking the hold function, and checking the waveform during operation. Measurement values are displayed in chronological order and ...
- マニュアル
... SECTION 5 SECTION 6 SECTION 7 SECTION 8 SECTION 9 SECTION10 Observe the following precautions to ensure safe use of the product. p.44 V530-R160 Operation Manual 7 INTRODUCTION INTRODUCTION Connectors Do not remove the connector cover. Doing ...