全 2904 件が検索されました。(2701 - 2720件を表示)

  • マニュアル

    ...9 10 11 12 13 14 15 0 0 0 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0 0 1 0 1 0 1 2 DLE SPACE ! DC1 ” DC2 DC3 # $ DC4 NAK % & SYN , ETB ( CAN ) EM SUB * + ESC , FS – GS ⋅ RS / US 0 1 1 1 0 0 1 0 1 1 1 0 1 1 1 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 4 @ A B C D E F G H I J K L M N O 5 P Q R S T...

  • マニュアル

    ...9 A B C D E F 0 0 0 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0 0 1 0 1 0 1 2 SPACE DLE DC1 ! DC2 ” DC3 # DC4 $ NAK % SYN & ETB , CAN ( EM ) SUB * ESC + FS , GS – ⋅ RS US / 0 1 1 1 0 0 1 0 1 1 1 0 1 1 1 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 4 @ A B C D E F G H I J K L M N O 5 P Q R S T...

  • マニュアル

    .../O The ID Controller is equipped with two user outputs that can be turned ON/OFF by a command from the host controller, and also two user inputs whose ON/OFF status can be read. These I/Os can be manipulated independently of each other, ...

  • マニュアル

    ... 1-1 Features V630 ID System offers powerful support to the automation of large-scale distributed control systems and multi-model small-scale production systems by means of contactless (infrared light) data communications. Good Transmission Range High Reliability • Data is transmitted with infrared light, ...

  • マニュアル

    ...11 12 1 Section 1-1 Using this Manual 1-1 Using this Manual Terminology Scenes A scene is a program area for saving contents and methods of measurement. The F300 has 16 scenes (numbered from 00 to 15), ...

  • マニュアル

    ... elements = 11 x 51 = 561 DIM TTA$(2, 5, 3) 3-dimensional array, number of elements = 3 x 6 x 4 = 72 . . . 4-dimensional array . . . 5-dimensional array . . . 6-dimensional array Subscripts start from zero, ...

  • マニュアル

    ...the Pt100 at a temperature of 100°C is 138.50 Ω. 1, 2, 3... 1. To use Fahrenheit, set function selector 4 to ON, which is usually set to OFF. 2. Insert the internal mechanism into the case. 3. Turn on the E5jJ ...

  • マニュアル

    ... provides powerful support to the automation of visual inspection processes. It greatly facilitates visual inspection and positioning in a wide range of industrial applications, such as, for example, labelling containers, distinguishing between different items, checking the directional orientation of components, positioning items for assembly, and ...

  • マニュアル

    ... Application Software Operation Manual: Included with the F350-UjjjE Application Software. • F350 OVL Reference Manual: Included with F350-L1jE OVL Unit. Procedure Software Application Programs F350-series catalog OVL program System design Consider the lighting environment, I/O devices, and ...

  • マニュアル

    ... Application Software Operation Manual: Included with the F350-UjjjE Application Software. • F350 OVL Reference Manual: Included with F350-L12E OVL Unit. Procedure Software Application Menus F350-series catalog OVL program System design Consider the lighting environment, I/O devices, and ...

  • マニュアル

    ... controlled with a 16-point Input Unit. It also has a parity-check for outputs, which can find disconnected cables or faulty connections. Compatible with Other OMRON FA ID Systems The Intelligent Flag and Intelligent Flag II are compatible with V600-series Data Carriers, ...

  • マニュアル

    ...: 0 to 9, A Note: Setting A is 10. Start address No. setting No. of bytes of data read from the Data Carrier is to be set in hexadecimal. The number of characters that can be read at one time is 256, so...

  • マニュアル

    ... and easy to mount. Cameras with Light Source Field of vision 12 Model 20 mm F150-SL20 50 mm F150-SL50 Section 2-5 Cameras Camera The same Camera is also available without a lens and light so that other CCTV lenses and lights can be used. Use C-mount lenses. Camera F150 Camera Model F150-S1 ! Caution The F150 Cameras listed above must be used. Using other Cameras can damage F150 components or the Camera. Distance from Measurement Object Note The Camera’s field of vision is fixed, and the Camera must be mounted at a distance from ...

  • マニュアル

    ... R/W Head and DC. This feature also helps to ensure superior transmission reliability even in environments where noise tends to occur. Superior Durability and High Reliability The R/W Head and DC offer superior resistance to environmental factors such as vibration, oil, water, and ...

  • マニュアル

    ... 40_C. (The write capacity is 100,000 times between the lower and upper limits of the operating temperature range.) Superior Durability and High Reliability The R/W Head and DC offer superior resistance to environmental factors such as vibration, oil, water, and ...

  • マニュアル

    ...power supply. Wiring mistakes may cause the equipment to explode or burn. Operating Environment Do not use the equipment in locations subject to corrosive, explosive or flammable gases, or dust (especially metallic dust). Construction Do not remove the product’s outer case. Doing ...

  • マニュアル

    .... Keep the power supply cable as short as possible. 8 Section CCTV Lens 2-4 2-5 Camera The Camera is designed for the F400. Mounting the Camera The specified camera distance is only an approximation. Mount the Camera ...

  • マニュアル

    ... and F150-SL50A are F150-S1A Cameras that are shipped with a lens and light attached. Field of vision Model 20 mm F150-SL20A 50 mm F150-SL50A Camera Only The same Camera is also available without a lens and light ...

  • マニュアル

    ... in accordance with the speed of movement for the measurement object (shutter speed). • Edges can be enhanced and the influence of noise can be reduced (filtering). • Background patterns can be cut (background suppression). 2 Images of acceptable (OK) and unacceptable (NG) products are registered ...

  • マニュアル

    ...measurement object from the measurement process. BGS changes image areas with densities below the lower limit to 0, and image areas with densities above the upper limit to 255. Image areas with densities between the lower and upper limits are graded from 0 to 255 ...