全 2904 件が検索されました。(2421 - 2440件を表示)
- マニュアル
... changing the setting of the sensor, a start-up check must be conducted. Normal operation can only be allowed after safety is confirmed. In order prevent access to a dangerous area, fixed barrier guards must be placed in fixed blanked areas. Failure to do ...
- マニュアル
... be stopped by electrical control in case of an emergency, such as a pressing machine with full-rotation clutch system. Serious injury may result if the machine does not stop before someone reaches the hazardous part. (Chapter 2-1) Install protective structures around the machine ...
- マニュアル
... be stopped by electrical control in case of an emergency, such as a pressing machine with full-rotation clutch system. Serious injury may result if the machine does not stop before someone reaches the hazardous part. (Chapter 2-1) Install protective structures around the machine ...
- マニュアル
...R HEAD 1 HEAD WRITE WRITE HEAD 2 RESET JOB ERR ERRO R TEST STOP DEC INC RESET ADR S DATA SE1 V600 IN 24 CA1A SO VDC 10mAURSE 10 OUT 0to24 24VD 0VAC C 10 50/60 Hz 35 0mA VA JAPAN OUTP UT ERRO R NC NC NC • 表示部:モニタ(MONITTOR)モードにおいて各種 NC データを表示します。 ラン(RUN)モードでは、「RUN」のみが表示されます。 ID • モード切換...
- マニュアル
...1 2 3 ADRS DATA SET 操作キー JAPAN TEST 7 6 0 DEC 1 RES 2 ET INC 3 ADR S V600 IN 24 CAIA SO VDC UR 10mA SE 10 OUT 0 to 240V 24VD AC 50 C 10 /60Hz 0mA 25VA JAPA N B JOB RESET ERR 5 MONIT OR RUN F WRITE 2 A 5 WRITE 2 B JOB 4 R STO P E WRITE 1 9 F REA D 9 8 HEAD 2 ERRO MONITOR RUN C 1 D READ DATA モード切換スイッチ SET JAPAN OUT...
- マニュアル
...R S T U V W X Y Z [ / ] ^ NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI DLE DC1 DC2 DC3 DC4 NAK SYN ETB CAN EM SUB ESC FS GS RS US FNC 3 FNC 2 SHIFT CODE C CODE B FNC 4 FNC 1 、 a b c d e f g h i j k l m n o p q r s t u v w x y z { | } ∼ DEL FNC 3 FNC 2 SHIFT CODE C CODE B FNC 4 FNC 1 103 104 105 START (CODE A)...
- マニュアル
...Connection with S3D2 Sensor Controller (Connection Example of Control Outputs) Discriminating whether the sensing object is within the desired range. Switch selection Control output Control output Output Operations Distance and Axis Adjustment The Sensor incorporates a laser beam delaying circuit, ...
- マニュアル
...から選択できます。 またメニューシートにより任意の1バイトを設定可能です。 (ただしホストから設定する場合、SO卜LST×、ESCの何れかの組み合わせになります。 ) ・フッタlETX、CR、CRLFなどから選択できます。 またメニューシートにより任意の1ま...
- マニュアル
... audible or visible warning when laser is switched on or if capacitor bank of pulsed laser is being charged Attenuator Not required Give means beside ON/ OFF switch to temporarily block beam Location controls Not required Controls located ...
- マニュアル
... 1 AEL’s as applicable Scan failure shall not cause product to exceed its classification Class label Required wording Not required Aperture label Service entry label Override interlock label User information Purchasing and service information Controls ...
- マニュアル
...容は 上へスクロールします。 端子台(常時 2 行表示) :2 進数で表示します。 (0:OFF,1:ON) NG 67ms シーン0▼確認▼ B [SO] ER [S I ] M [SO] 259, 810, 281, 222 [D I ] 01000100 [DO] 1001100001110010 RS-232Cの最新入出力内容 C ピックアップフリーズ 端子台入出力内容 [D I ]:入力 [DO]:出力 RS-232C入出力内...
- マニュアル
...示されます。 表示内容は計測すると上へスクロールし、最大 4行まで表示されます。 (4行目が最新) [S I ]:入力 [SO]:出力 [S I ] M [SO] ER [S I ] M [SO] 259, 810, 281, 222 [D I ] 01000100 [DO] 1001100001110010 C フリーズ 端子台の入出力内容が2進数で表示されます。 (0:OFF、1:ON)常に2行で...
- マニュアル
...sheet. (4) If the Sensor or cable has lock mechanisms, be sure to lock the mechanisms securely before use. (5) Never disassemble, repair nor tamper with the product. (6) Dispose of the product as industrial waste. (7) Do not short-circuit the load. Doing ...
- マニュアル
...れます 5. シリアルパラレル [シリアル]を選びます I/O モニタ画面が表示されます シリアルI/Oモニタ [SO]TEST STRING [S I ]RECEIVE TEST [SO]RECEIVE TEST 第4章 外部との入出力状態を確認する TRIG:テスト送信 S+ENT:詳細設定 画面の表示内容についてはたらき 表示...
- マニュアル
...れます 5. シリアルパラレル [シリアル]を選びます I/O モニタ画面が表示されます シリアルI/Oモニタ [SO]TEST STRING [S I ]RECEIVE TEST [SO]RECEIVE TEST TRIG:テスト送信 S+ENT:詳細設定 画面の表示内容についてはたらき 表示 6. ESC ...
- マニュアル
... you for your purchase of this F250-C50/C55 Vision Sensor (hereinafter referred to as the Controller). This manual explains how to use the Controller. Please observe the following points when using the Controller. • Please read and understand this manual thoroughly before using the Controller ...
- マニュアル
... you for your purchase of this F270-C10/C15 Vision Sensor (hereinafter referred to as the Controller). This manual explains how to use the Controller. Please observe the following points when using the Controller. • Please read and understand this manual thoroughly before using the Controller ...
- マニュアル
...INTRODUCTION Thank you for your purchase of this F210-C10/C15 (hereinafter referred to as the Controller). This manual explains how to use the Controller.Please observe the following points when using the Controller. - Please read and understand this manual thoroughly before using the Controller ...
- マニュアル
...れます 5. シリアルパラレル [シリアル]を選びます I/O モニタ画面が表示されます シリアルI/Oモニタ [SO]TEST STRING [S I ]RECEIVE TEST [SO]RECEIVE TEST 第4章 外部との入出力状態を確認する TRIG:テスト送信 S+ENT:詳細設定 画面の表示内容についてはたらき 表示...
- マニュアル
...れます 5. シリアルパラレル [シリアル]を選びます I/O モニタ画面が表示されます シリアルI/Oモニタ [SO]TEST STRING [S I ]RECEIVE TEST [SO]RECEIVE TEST TRIG:テスト送信 S+ENT:詳細設定 画面の表示内容についてはたらき 表示 6. ESC ...