全 2904 件が検索されました。(2361 - 2380件を表示)
- マニュアル
... using the FZ3 Series, be sure to observe the following: • The FZ3 Series must be operated by personnel knowledgeable in electrical engineering. • To ensure correct use, please read this manual thoroughly to deepen your understanding of the product. • Please keep this manual in a safe place ...
- マニュアル
... do not remember the entire mnemonic. (1) When you type “+”, suggested instructions are displayed. When you press the + , a list of instructions starting with “+” is displayed. (2) Press the “↓” key to select the instruction to be input in the list. Instruction names are displayed, ...
- マニュアル
... (L) ② AC (N) AC (L) NC AC (N) MOLEX 5194T 5194TL AMP 1-175196-5 1-175218-5 Fig. 1 Nomenclature / Bezeichnungen / Nomenclature EN NOTICE Fig.2 ■ Mounting • Install the power supply so that heat is effectively dissipated to improve and maintain the reliability of the power supply over a long period of time. • The screws must not protrude more than S82J010 □□□ , 025 □□□ , 050 □□□:4 mm, S82J-100 □□□ ,15024 □:6 mm inside the power supply when screw holes provided on the chassis are used. Mounting screw tightening torque (recommended value) S82J-010 □□□ , 025 □□□ , 050 □□□ : 0.54N•m S82J-100 □□□ ,...
- マニュアル
... Netzteil Lösungnen, fremden Substanzen ober Korrosiven Gasen ausgesetzt ist. 5. Es sind Standorte zu vermeiden, an denen es zu Stößen oder Vibrationen kommen kann. 6. Wenn die Stromversorgung in einem Gebiet mit starker elektronischer Rauschentwicklung verwendet wird, achten Sie darauf, die Stromversorgung ...
- マニュアル
.... ADJ adjuster/Adjusts the output voltage. ⑥ NC terminal/Vacant terminal. ④ ⑤ ④ Karasuma Nanajo, Shimogyo-ku, Kyoto 600, Japan OMRON Corporation 0667799-6D CSA Level 1 ② ■ When using provided mounting Precautions bracket ■ Mounting ・Install the power supply ...
- マニュアル
...due to non-recharging. 【Installation and Environment】 ・Do not use the battery in a tight area or near an object that generates sparks such as contactors, relays, or static charge that generates sparks. The battery may generate flammable gases when it is charged, ...
- マニュアル
... or vibration. 8. If the Power Supply is used in an area with excessive electronic noise, be sure to separate the Power Supply as far as possible from the noise sources. (2) Installation/Wiring 1. Ground the product (PE) completely. Failure to do ...
- マニュアル
...shortened or backup operation becomes impossible due to nonrecharging. 【Installation and Environment】 ・Do not use the battery in a tight area or near an object that generates sparks, such as contactors, relays, or static charge. The battery may generate flammable gases when it is charged, ...
- マニュアル
...shortened or backup operation becomes impossible due to nonrecharging. 【Installation and Environment】 ・Do not use the battery in a tight area or near an object that generates sparks, such as contactors, relays, or static charge. The battery may generate flammable gases when it is charged, ...
- マニュアル
... vous pourriez vous électrocuter. • N’enlevez pas les protections des connecteurs à moins d’utiliser les connecteurs de ligne de bus. Vous pourriez vous électrocuter. (1) Installationsumgebung Nicht an Orte die starke Vibratioen ausgestzt sind montieren. Achten Sie besonders darauf, dass das Netzteil ...
- マニュアル
... (Cross-sectional Area 2.081 to 3.309mm2) connected units (3) Handling of Bus Line Connector Do not give too strong shock to the Bus line connector such as dropping off. (4) Do not adjust the voltage after multi-connecting the unit. Failure to do ...
- マニュアル
... of the power supply. 7. If the Power Supply is used in an area with excessive electronic noise, be sure to separate the Power Supply as far as possible from the noise sources. (2) Wiring 1. Ground the product completely. Failure to do ...
- マニュアル
... radiation could cause the deterioration or breakage of the 䈧н㾱൘䗷䖭ᡆ䗃ࠪ⭥⎼⎚ח⍱仁㑱ਁ⭏Ⲵᛵߥл֯⭘䈕ӗ૱DŽ⭥Ⓚ䜘ݳಘԦᙗ㜭ਟ inner component. 㜭ᚦॆᡆᦏൿDŽ Ŗ/QWPVKPI5RCEG Install the power supply unit so that the air flow takes place around the power supply 䗷⭥؍ᣔ unit as the power supply is designed to radiate heat by means of natural air flow. 䈕⭥Ⓚ㜭ཏ㠚ࣘ؍ᣔ㠚䓛৺䍏䖭ݽਇ䗷⭥ⲴᦏᇣDŽྲ᷌䗃ࠪ⭥䎵...
- マニュアル
...ྲᦹ㩭ㅹᕪ⛸ⲴߢࠫDŽ (4)ཊਠ䘎᧕ਾˈ䈧н㾱䈳ᮤ䗃ࠪ⭥DŽࡉ䗃ࠪ⭥ ਟ㜭нっᇊDŽ (4) Do not adjust the voltage after multi-connecting the unit. Failure to do so could cause the instability to the output voltage. (5) See product catalogue for details. (5)䈖㓶ᇩ䈧৲㘳୶૱ⴞᖅDŽ Key to Warning Symbols 䆖ḷ䇶Ⲵਜ਼ѹ Indicates a potentially hazardous situation which, if not 㤕нᖃⲴ䈍ᴹਟ㜭ਁ⭏䖫ѝᓖՔᇣᡆ...
- マニュアル
.... Vermeiden Sie bitte direkte Sonnenneinstrahlung auf das Netzteil. 5. Vermeiden Sie bitte Orte, an denen das Netzteil Chemische Lösungnen, fremden Substanzen ober Korrosiven Gasen ausgesetzt ist. 6. Nicht an Orte die starke Vibratioen ausgestzt sind montieren. Achten Sie besonders darauf, dass das Netzteil ...
- マニュアル
....5 bis 6mm2 2.5 bis 4mm2 Fig. 3 OMRON CANADA INC. Phone: 1-416-286-6465 Phone: 1-866-986-6766 Fax : 1-416-286-6648 IT Nomenclature Fig.2 • Montagesitz Fig.3 Die Leistungseinheit muß so montiert werden, dass genügend Kühlung durch Luftstrom um die Leistungseinheit herum gewährleistet ist. Die Leistungseinheit gibt die Hitze durch den natürlich kühlenden Luftstrom ab. *1 Durchflußrichtung Luftstrom *2 75 (mm) oder mehr *3 75 (mm) oder mehr *4 20 (mm) oder mehr Versorgungsspannung Nennspannung: 100 bis 240 V Wechselstrom Ausgangsspannung-Einstellung Vorgabe-Einstellung: Auf Nennspannung einstellen Einstellbereich: Einstellbar mit “V.ADJ” ⑤ ...
- マニュアル
...-286-6648 2 IT S8VK-G015□□,S8VK-G030□□, Borne de mise S8VK-G060□□ à la terre S8VK-G12024,S8VK-G240□□, S8VK-G480□□ Toutes les S8VK-G□□□□□ bornes Nomenclature Fig.2 • Montagesitz Fig.3 Die Leistungseinheit muß ...
- マニュアル
.... Vermeiden Sie bitte direkte Sonnenneinstrahlung auf das Netzteil. 7. Vermeiden Sie bitte Orte, an denen das Netzteil chemischen Lösungnen, fremden Substanzen ober korrosiven Gasen ausgesetzt ist. 8. Nicht an Orten, die starken Vibrationen ausgesetzt sind, montieren. Achten Sie besonders darauf, dass das Netzteil ...
- マニュアル
...#28 à AWG#22 avec isolant dia ø1.0 à ø1.5 mm. Crimping tool is as below. UL1007 AWG26 Anmerkungen: 1. Die Crimphöhe an der Drahtcrimphülse muss entsprechend der festgelegten Höhe eingestellt werden. 2. Stellen Sie die Crimphöhe an der Isolierhülse ...
- マニュアル
...20 39.2 to 45.1 30 68.6 to 74.5 40 92.1 to 96.0 Anmerkungen: 1. Die Crimphöhe an der Drahtcrimphülse muss entsprechend der festgelegten Höhe eingestellt werden. 2. Stellen Sie die Crimphöhe an der Isolierhülse ...