全 2741 件が検索されました。(2001 - 2020件を表示)

  • マニュアル

    ... to 20mA to 9999, –199.9 to 999.9, –19.99 to 99.99, 2 1 to 5V –1.999 to 9.999 3 Voltage input 0 to 5V 4 0 to 10V • The default is “0”. 5 SD EV2 The setting data for the E5AN-□3HT/L is shown here as an example. *5 in-t 2 RS-485 RS-232C 11 Control output 1 Operation indicators • OUT2: Control output 2 indicator • ALM1: Alarm 1 indicator Lit when control output 2 is ON and Lit when alarm 1 is ON. not lit when it's OFF. • ALM2: Alarm ...

  • マニュアル

    ...POWER ON 0.2 off 12 A heater burnout alarm, heater short alarm, heater overcurrent alarm, or input alarm is output to the output to which the alarm 1 function is assigned. Communications RS-232C RS-485 11 ...

  • マニュアル

    ...BedienungsanleitungEi5AR/ER(Englisch)Nummer=Cat,No.Zl82-Et・-Ot 2.MitderUnterstUtzungssoftware(optional)istesmOglichdieParametermiteinemComputerzu konfigurierenundzuarldern.UnterstUtzungssoftware:ModellESTT-YB177-MVIS"ThermoTools V土0"oderh6her 42 ---------------------[End of Page 7090]--------------------- αeiche旧etrlebwlebeim」.UberschreltenderoberenGζenze, 一、 へ │ー』..♂ 、 ∫ Pr6cauti頒...

  • マニュアル

    ... 2 Communications (RS-232C) and CT 11 RD 12 12 SG 13 13 14 12VDC,21 DC,21 mA mA 15 15 - Control output 2 and transfer output RS-232C SD 14 + Transfer output 15 11 11 Controlol output p 2 12VDC,21 DC,21 mA m 12 DO NOT 13 USE + 14 CT1 Event inputs and transfer output 15 - EV1 EV2 + 4-20 mADC Transfer (Load: 600 Ω max.) output - 12 13 14 15 4-20 mADC (Load: 600 Ω max.) • A heater burnout alarm, heater short alarm, heater overcurrent alarm, or input alarm is output to the ...

  • マニュアル

    ...21 SDB 21 + L 4-20mA − Event input1/2 16 15 14 13 − 12 11 + 23 ● OPTION1 22 − Transfer output E5EK-T□B□ E5EK-T□F□ SD 20 RDA 19 RD 19 RDB 20 SG 18 SG 18 RS-232C RS-422 E5EK-T□01□ E5EK-T□02□ A B A B 22 21 19 20 RS-485 E5EK-T□03□ W C + V − − mA TC • Do not wire the terminals which are not used. Pt + M CABLE CONNECTIONS • RS-232C interface: E5EK-TM01M Host computer E5EK-T RS-232C:25P No. No. 1 FG 2 ...

  • マニュアル

    ...RS-422 No. Shielded cable RS-232C E5EK(No.30) RS-422 RS-422 RS-232C:25P No. A No. Terminator×2 (240Ω 1/2W) 1 FG No. RDA 22 SDA 2 SD 20 SD RDB 21 SDB 21 SDB (part pointed with an arrow in the above drawing) and turn a screwdriver to loosen the screw on the 3 RD 19 RD SDA 19 RDA 19 RDA 4 RS 18 SG SDB 20 RDB 20 RDB 5 CS SG 18 18 6 DR FG E5EK Watertight packing lower part of the front panel. Setting is not required on the E5EK-...

  • マニュアル

    ... to 20mA to 9999, –199.9 to 999.9, –19.99 to 99.99, 2 1 to 5V –1.999 to 9.999 3 Voltage input 0 to 5V 4 0 to 10V • The default is “0”. 5 SD EV2 The setting data for the E5EN-□3HT/L is shown here as an example. *5 in-t 2 RS-485 RS-232C 11 Operation indicators • OUT2: Control output 2 indicator • ALM1: Alarm 1 indicator Lit when control output 2 is ON and Lit when alarm 1 is ON. not lit when it's OFF. • ALM2: Alarm 2 indicator • STOP: ...

  • マニュアル

    ...ambient temperature does not exceed the specified limit. 1 A heater burnout alarm, heater short alarm, heater overcurrent alarm, or input alarm is output to the output to which the alarm 1 function is assigned. Communications RS-232C RS-485 ...

  • マニュアル

    ... value + 11 Event Inputs 1 A heater burnout alarm, heater short alarm, heater overcurrent alarm, or input alarm is output to the output to which the alarm 1 function is assigned. Communications RS-232C RS-485 11 ...

  • マニュアル

    ...) sl-h 1300 Alarms Alarm type d-u Setting range • The default is “0”. Setting dp RD CT CT input POWER ON Scaling Upper Limit when setting analog 100 (only input) *6 SD RS-232C communications • CMW: communications writing enable/ disable indicator Lit when communications writing is “enabled” and is out when it is “disabled”. 5 Input Type *3 in-h /0 to 3200 (°F) /0 to 2300 (°F) Setting 0 Use the following ranges for scaling: 1 −1999 to 9999, −199.9 to 999.9, −19.99 to 2 99.99, −1.999 to 9.999 3 4 • ...

  • マニュアル

    ...示灯如果指定给辅助输出1的功能为ON,就亮。 • 第二显示设定值,设定数据读出值或改变的输入值 操作菜单 不用 SD RS-232C通讯 • 将加热器烧毁报警、HS报警、加热器过流报警或输入报警输出到指定了报警1功能的输出。 • 因为电压输出(控制输出)在内...

  • マニュアル

    ... 0% output. • SUB2: Auxiliary output 2 indicator • STOP: control stop indicator Lit when the function assigned to Lit when event input or “Run/Stop ”is stopped auxiliary output 2 is ON. during operation. Initial Setting Level Input DO NOT USE ...

  • マニュアル

    ... the E5ZN until the hooks lock into place. Pull down on the hooks with a flat-blade screwdriver and lift up on the E5ZN. 130 130 SLGR @NQ @NQ @NQ POWER POWER POWER ERROR ERROR SD/RD SD/RD OUT1 OUT1 OUT2 OUT2 SUB1 SUB1 SUB1 SUB2 SUB2 SUB2 @NQ hooks into the SLGR SLGR SLGR ࡱ ② Insert the upper POWER ࡱ ERROR ...

  • マニュアル

    ...ネル内に内蔵) ・LAN コネクタ用防塵カバー(LAN コネクタに装着) ・OPTION コネクタ用防塵カバー(OPTION コネクタに装着) ・防塵用 SD ダミーカード(SD カードスロットに挿入) ・メモリバックアップ用電池についての注意書き・中国版 RoHS に関わる、製品中の化学...

  • マニュアル

    ...ネル内に内蔵) ・LAN コネクタ用防塵カバー(LAN コネクタに装着) ・OPTION コネクタ用防塵カバー(OPTION コネクタに装着) ・防塵用 SD ダミーカード(SD カードスロットに挿入) ・メモリバックアップ用電池についての注意書き・中国版 RoHS に関わる、製品中の化学...

  • マニュアル

    ...Lamp and Bluetooth® Communication Unit for F3SG Series EN Instruction Sheet Thank you for purchasing Bluetooth® Communication Unit for F3SG Safety Light Curtain. Read this document and user's manuals of the Safety Light Curtain (F3SG-RA or F3SG-RR) and Configuration Tool (...

  • マニュアル

    ... (日/英語) Model F39-GIF-1 Interface Unit for F3SG-RR Safety Light Curtain EN Instruction Sheet Thank you for purchasing Interface Unit for F3SG-RR Safety Light Curtain. Read this document and user's manuals of F3SG-RR and Configuration Tool (...

  • マニュアル

    ... the Dedicated Cables 1 and 2 and Interface Unit as shown below. 3. Insert the connected cables to the USB port of the PC and the Communication Port of the F3SG receiver. 4. Turn on the power of the F3SG. 5. Run the ...

  • マニュアル

    ... result in electric shock. Extension of the cable must be within a specified length. If it isn't, safety function may not work properly, resulting in danger. Settings WARNING Some settings of functions or the Setting Recovery function configurable with the configuration software, ...

  • マニュアル

    ..., CFG, LOCKOUT, STB and ON/OFF indicators on the receiver of the F3SG-RA blink when the F3SG-RA is in Setting mode. The blinking patterns are Blinking Once or Blinking Twice, depending on the access level. Refer to Safety Light Curtain Configuration Tool for Model F3SG (...