全 50426 件が検索されました。(2001 - 2020件を表示)

  • マニュアル

    ... on "dlun". WRITE (dlun) $in.string The following example returns any error generated during the write operation example above to the "error" variable. error = IOSTAT(dlun) Reading from a Disk The following example reads from the open file on "dlun" up to the first ...

  • マニュアル

    ...wide. /In Format values as decimal integers in fields n spaces wide. /On Format values as octal integers in fields n spaces wide. The following specifiers can be used to insert special characters in the string. /Cn Include the characters carriage return (...

  • マニュアル

    ... on "dlun". WRITE (dlun) $in.string The following example returns any error generated during the write operation example above to the "error" variable. error = IOSTAT(dlun) Reading from a Disk The following example reads from the open file on "dlun" up to the first ...

  • マニュアル

    ...CAGBSR CAGES, CAGEB CAKFB CAKFBR CAGDSR CAGDB CAGDBR *2 Encoder cable R88AStandard Flexible CRKAC *3 CRKACR *3 CRKCN *3 CRKCNR *3 CRKCN *3 CRKCNR *3 CRKCN *3 CRKCNR *3 CRKCN *3 CRKCNR *3 CAGES, *2 CAGEB *1. □ represents an optional specification for the motor.  represents a 3-digit cable length (005 for 5 m). *2. We have no plan ...

  • マニュアル

    ...CAGBSR CAGES, CAGEB CAKFB CAKFBR CAGDSR CAGDB CAGDBR *4 Encoder cable R88AStandard Flexible CRKAC *3 CRKACR *3 CRKCN *3 CRKCNR *3 CRKCN *3 CRKCNR *3 CRKCN *3 CRKCNR *3 CRKCN *3 CRKCNR *3 CAGES, *4 CAGEB *1. □ represents an optional specification for the motor.  represents a 3-digit cable length (005 for 5 m). *2. The G5 series with ...

  • マニュアル

    ...)日々{V1+V・)1 3一 −V3 V3-C2▼▼ G・1佗((㌔・∼旬・頂くV・・V・}・1/2V・1 4 ぬ V4-・C3 C・魂((迫・V・)・118(VIW2)・1!4V、.惚V4… a Vn VバーCrト1 1」2キ1(V1÷V∼)+1/2卜2V3ゴ計1!2Vn. . ↓叩utwaveforrp OM ON TIMtNGinρut OFF 篇mpleofP輌sAv・・ag・V・lueC・mp・ris・・wh・n・er・Cti・gS・mpli,g Numberofmeasurhgoperations 一.・-lnputva佃e OiSplayedvalue COmparedwithpresentvalUe 1 4.0 4,0-4.0=0 4.0 じ 3.0 13,・-...

  • マニュアル

    ...え回数オーバーか否かの判定を行います。 ●コマンドフォーマット M D S l X X X X X X * CR 減算回数をHEX(16進数)で指定します。 (00H、01H、02H、・・・、FBH) エリア先頭アドレス指定範囲 (□□□0H∼□□□5Hまたは□□□8H∼□□□DH) ●レスポンスフォーマット M D 7 5 * ...

  • マニュアル

    ...内蔵データキャリアを水中で加熱浸漬(100 ℃、16 時間)し、抽出されるイオンを分析するものです。 ・抽出イオン(含有量) Cr-…0.5p.p.m.、Na+…10p.p.m.、 NH4+…11p.p.m.、K+…1.0p.p.m. ● ICP 発光分光分析結果これは、データキャリア(形 V600-D23P66SP)を薬液に入れ、PFA を通して析出...

  • マニュアル

    ...第 5 章 リーダライタの機能 5-1 通信手順 5-1-1 通信フォーマット通信フレームはデータ部と、ターミネータ[CR] (ASCIIコード:0Dh) で構成されます。 データ部:272文字以内データ1 データ2 データ 文字数 データ部 1∼272 ターミネータ 1 データn ・・・...

  • マニュアル

    ...horizontal axis. • The monitoring results can be saved as CSV files on the computer. 116 Section 8-4 Wireless Channel Monitor 90 bytes, when there are 10 wireless slave stations Clear Clear Clear Cler WNODE ch ch ...

  • マニュアル

    ...8 9 A B C D E F 0 0 0 0 NUL SOH STX ETX EOT ENQ ACK BEL BS HT LF VT FF CR SO SI 0 0 1 0 1 0 1 2 SPACE DLE DC1 ! DC2 ” DC3 # DC4 $ NAK % SYN & ETB , CAN ( EM ) SUB * + ESC FS , GS – ⋅ RS US / 0 1 1 1 0 0 1 0 1 1 1 0 1 1 1 3 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 4 @ A B C D E F G H I J K L M N O 5 P Q R S...

  • マニュアル

    .... Countermeasure Examples When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC DC Yes C Power R supply xx Inductive load ...

  • マニュアル

    ...Countermeasure Examples When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC DC Yes C Power supply xviii R Inductive load ...

  • マニュアル

    .... Countermeasure Examples When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC DC Yes C Power R supply xxvi Inductive load ...

  • マニュアル

    ...Countermeasure Examples When switching an inductive load, connect a surge protector, diodes, etc., in parallel with the load or contact as shown below. Circuit Current AC DC Yes C Power supply xxiv R Inductive load ...

  • マニュアル

    ... Serial PLC Link (master) Serial PLC Link (master) NT Link (1:1) NT Link (1:N) Link words LR00 to LR15 - No setting (fixed value) Start code Disable/Enable Start code Disable/Set End code Received bytes / ...

  • マニュアル

    ... bits (Default) 7 bits (Default) Stop bits 2 bits (Default) 2 bits (Default) Parity Even (Default) Even (Default) Baud rate 57,600 bps 57,600 bps (Default) Protocol macro Transmission mode Full-duplex - Terminator - [...

  • マニュアル

    ...) Stop bit 2 bits (Default) 2 bits (Default) Parity Even (Default) Even (Default) Baud rate 57,600 bps 57,600 bps (Default) No-protocol Start Code Yes 1 (SOH) SOH (Fixed) No-protocol End Code Yes (CR+LF) ...

  • マニュアル

    ...192.168.250.1 192.168.250.2 Subnet mask 255.255.255.0 255.255.255.0 (Default) Gateway ---.---.---.--- 192.168.0.1 (Default) Port number Automatic allocation 9600 (Default) (Set by the program.) Terminator - [...

  • マニュアル

    ...1 bit (Default) Parity None None (Default) Baud rate 38,400 bps 38,400 bps (Default) CTS control None OFF (Default) No-protocol start code None (Default) - No-protocol end code Yes (16#0D) [CR] (Default) (connection) port Serial communications mode Terminator Precautions for Correct Use This document describes the procedure for setting the CJ1W-SCU42 Serial Communications Unit when the unit number 0, communications port 2 and device name J01 are used. To connect devices under different conditions, refer to 9. Program and create a program by changing the variable names and setting values. 8 6. Serial Communications Settings...