全 2436 件が検索されました。(1461 - 1480件を表示)
- マニュアル
...Immediate 0 B #59 Pn830 JOG Unit Selection 0, 1 − Immediate 0 B #60 Pn831 JOG Speed 1 to 240,000 × 1,000 steps/min Immediate 24,000 B #61 Pn832 JOG Acceleration Time 1 to 10,000 ms Immediate 100 B #62 Pn833 JOG Deceleration Time 1 to 10,000 ms Immediate 100 C #63 Pn834 JOG Switch Speed 1 to 240,000 × 1,000 steps/min Immediate 12,000 C #64 Pn835 JOG Second Acceleration/Deceleration Time 1 to 10,000 ms Immediate 200 C #65 Pn836 JOG Acceleration/ Deceleration Type 0 to 3 − Immediate 0...
- マニュアル
.... Note: If a new error occurs while the error log is being displayed, the error will not be displayed on the Error History Tab Page in real time. Click the Update Button to display the most recent error log. Clears the error log. 7-...
- マニュアル
...78 60 90 70 62 1/15 R88M-W40030@-@G15CJ 124.5 164 100 50 78 60 90 70 62 1/25 R88M-W40030@-@G25CJ 124.5 164 104 61 98 60 115 90 75 1/5 R88M-W75030@-@G05CJ 145 189.5 93.5 50 78 80 90 70 62 1/9 R88M-W75030@-@G09CJ 145 189.5 97.5 ...
- マニュアル
... table are used for the fundamental frequency input current and converted for a received voltage of 6.6 kV. Applicable motor [kW] Fundamental frequency input current [A] 200 V 400 V Value converted for 6.6 kV [mA] 0.4 1....
- マニュアル
...Preventing Motor Stalling During Operation ................................................................. 6-54 Changing Stall Prevention Level during Operation Using an Analog Input .................. 6-55 Using Frequency Detection .......................................................................................... 6-55 Detecting Motor Torque ................................................................................................ 6-58 Changing Overtorque and Undertorque Detection Levels Using an Analog Input ....... 6-...
- マニュアル
...50 78 60 70 90 70 62 17 3 8 19 30 M5 M6 M4 20 22 6 6 3.5 2.1 1/25 R7G-VRSFPB25D400 104 61 98 60 70 115 90 75 18 5 8 24 40 M5 M8 M4 20 30 8 7 4 3.2 1/5 R7G-VRSFPB05C750 93.5 50 78 80 90 90 70 62 17 3 10 19 30 M6 M6 M4 20 22 6 6 3.5 2.1 1/9 R7G-VRSFPB09D750 97.5 ...
- マニュアル
...50 78 60 70 90 70 62 17 3 8 19 30 M5 M6 M4 20 22 6 6 3.5 1/25 R7G-VRSFPB25D400 104 61 98 60 70 115 90 75 18 5 8 24 40 M5 M8 M4 20 30 8 7 4 1/5 R7G-VRSFPB05C750 93.5 50 78 80 90 90 70 62 17 3 10 19 30 M6 M6 M4 20 22 6 6 3.5 1/9 R7G-VRSFPB09D750 97.5 ...
- マニュアル
... command status prior to the input. •If you switch on/off this function during operation, the RUN command is reset to stop the Inverter. Before resuming operation, stop the RUN command from each command source to avoid possible danger and then input it again. 4-...
- マニュアル
... (network error) 09: LOG(logic operation output) 00: Output frequency 01: Output current Default setting Changes during operation Unit Page No ⎯ 4-53 No ⎯ 4-31 4-63 No ⎯ 4-61 00 01 05 00 00 00: NO contact at MA; NC contact at MB 01: NC contact at MA; NO contact at MB 00 01 0.0: Does not operate 0.1 × Rated current to 2.0 × Rated current Rated current 4-29 4-55 No A C241 *2nd overload warning level Rated current C042 Arrival frequency during acceleration 0.0 to 400.0 0.0...
- マニュアル
...When the FW signal is ON, the motor runs forward. When it is OFF, the motor decelerates and stops. S1 S2 S3 S4 S5 S6 S7 S8 Multi-function input Select 8 functions from among the 61 functions and allocate them to terminals S1 to S8. Note: Only terminals S1 and S3 can be used for the emergency shutoff function. For details, refer to "Emergency Shutoff Function" (page 2-10). Status / Factor Input impedance between each input terminal and the PSC terminal: 4.7 kΩ Allowable max. voltage: Voltage between each input terminal and the PSC terminal: 27 V DC...
- マニュアル
...78 70 90 70 3 8 19 30 1/5 R88G-VRXF05C750CJ 93.5 50 80 78 90 90 70 3 10 19 30 1/9 R88G-VRXF09D750CJ 97.5 61 80 98 90 115 90 5 10 24 40 1/15 R88G-VRXF15D750CJ 110.0 61 80 98 90 115 90 5 10 24 40 1/25 R88G-VRXF25D750CJ 110.0 ...
- マニュアル
...90 70 3 8 19 30 1/5 R88G-VRXF05C750CJ 93.5 50 80 78 90 90 70 3 10 19 30 1/9 R88G-VRXF09D750CJ 97.5 61 80 98 90 115 90 5 10 24 40 1/15 R88G-VRXF15D750CJ 110.0 61 80 98 90 115 90 5 10 24 40 1/25 R88G-VRXF25D750CJ 110.0 ...
- マニュアル
...no yes Hz A069 Acceleration 0.00 to 99.99 Stop Frequency 100.0 to 400.0 (1000.) 0.00 no yes Hz A070 Acceleration Stop Time 0.0 5-60 4 5-61 0.0 to 60.0 SYSDRIVE MX2 Series USER'S MANUAL (3G3MX2-A@@@@) Parameter List Others Limit/jump Parameter No. Function name Data can Data can be Default be set Set data changed Unit Page setting during during RUN RUN 5-62 no yes s 4-10 4-2 Function Mode PID control Parameter No. Function name Parameter List 4 A071 PID Selection 00: Disabled 01: ...
- マニュアル
...-2 Communications Response Time ..........................................................................................A-5 A-3 Object List ................................................................................................................................A-6 A-3-1 Object List................................................................................................................................... A-6 A-4 MX2 Series Parameter List ...................................................................................................A-10 A-5 RX-V1 Series Parameter List ................................................................................................A-34 A-6 Sysmac Error Status Codes .................................................................................................A-...
- マニュアル
...Belt Encoder 1 Connector 05624-000 Rev. K n/a Standard Option X 09443000 Cobra 350 User's Guide X X X X HDB26 Female DB15 Female M12 Female, 8-pin 61 5.3 Optional Cables Item Description Part # Standard Option Usersupplied Notes H Belt Encoder 2 Connector I SmartController EX (optional) 19300000 X J SmartController EX Belt 09550Encoder Y Adapter Cable Con- 000 nector X K Belt Branch Connector, Encoder 1 and 2 DB15 Male L Belt Branch Connector, Encoder 3 and 4 DB15 Male C PIN 8 PIN 15 PIN 15 PIN 7 PIN 14 PIN 6 PIN ...
- マニュアル
...4-18-2 4-18-3 Creating Backup Files ...............................................................................................................4-38 Restoring the AMR ....................................................................................................................4-40 SetNetGo Recovery Mode ........................................................................................................4-45 4-19 Safety Laser Scanner Zones...............................................................................................4-49 4-19-1 Safety Zones .............................................................................................................................4-49 4-20 Motion Limits........................................................................................................................4-...
- マニュアル
... Number (Key 1 - Key 4) l WEP Keys WPA/WPA2-PSK l PSK l PSK-Type (Passphrase or Raw Hex) Click Apply for your changes to take effect. 14766-000 Rev E LD Platform Cart Transporter User's Guide 61 4.2 Mapping Wireless Coverage The AIV must have wireless coverage for multi-AIV installations, or in areas where you wish to send new commands to or receive status updates from the AIV. Ensure that, in such cases, you have adequate wireless coverage. Because of the variation possible in different environments, we don't specify what components or techniques ...
- マニュアル
...Boot the call/door box, Enable its web interface Status Tab Network Tab WLAN Profiles Tab Resetting a Call/Door Box (WiFi or Wired) 5.4 Mounting the Hardware 55 57 57 58 59 59 60 61 61 65 67 67 Call/Door Box 67 5.5 MobilePlanner Configuration Host Software Overview of Tasks Configuring Call/Door Boxes Identifying an Installed Call/Door Box Setting the Arrival Beep Duration Enabling the Queuing Manager for Single-AMR Adding Door Areas to Your Map Configuring External I/O 5.6 Operation 70 70 70 70 73 73 74 74 76 77 Call/...
- マニュアル
...), file save, and undo/redo functions. Some of these items are also available from the File and Edit menus. For details, see Opens a submenu, which lets you select and open a file located on a particular robot or the Enterprise Manager (EM). on page ...
- マニュアル
...58 58 58 58 5.6 applicationFaultSet Command Syntax Usage Considerations Parameters Responses Details Examples Related Commands 59 59 59 59 59 59 59 60 5.7 arclSendText Command 61 Syntax Usage Considerations ARAM Settings Parameters 4 55 ...