全 270 件が検索されました。(81 - 100件を表示)

  • マニュアル

    ... conductive tape to shield gaps between the cutout and the PT before securing the PT in place. • To suppress noise terminal voltage, perform installation under the following conditions. It is recommended to use the following product for the DC power supply. Recommended Power Supply model: ...

  • マニュアル

    ...-3 (タイコエレクトロニクスアンプ㈱製) ・推奨コネクタピン: 形175217-3 (タイコエレクトロニクスアンプ㈱製) ・推奨24V電源: 形S82K-03024(オムロン㈱製) (上記推奨コネクタ・コネクタピンはV640−A90 (別売)に同梱しています。 ) コネクタピンを圧着する専用工具とし...

  • マニュアル

    ...-3 (タイコエレクトロニクスアンプ㈱製) ・推奨コネクタピン: 形175217-3 (タイコエレクトロニクスアンプ㈱製) ・推奨24V電源: 形S82K-03024(オムロン㈱製) (上記推奨コネクタ・コネクタピンはV640−A90 (別売)に同梱しています。 ) コネクタピンを圧着する専用工具とし...

  • マニュアル

    ...溶剤はねじ締め付け部に塗布しないでください。 ケースにクラックが発生する可能性があります。 ・推奨24V電源:形S82K-03024 (オムロン) 正しい使い方配線後は間違いがないか十分確認してください。 誤配線は故障の原因となります。 ・推奨ケーブ...

  • マニュアル

    ... to tables. Pages 28 and 65: Added information on power supply. Page 37: Changed resistance values from “60 Ω” to “70 Ω” and from “200 to 300 Ω” to “300 Ω or higher.” Page 55: Changed “S82H-series and S82Jseries” to “S82J-series and ...

  • マニュアル

    ... connector to connect to the power terminal block is provided. Note 1. Repeater Units do not use a node address. 2. See Connection Procedure for an explanation of how Repeater Units are used. 3. The following Power Supply Unit is recommended: OMRON ...

  • マニュアル

    ...22 Round terminal 6.0 mm max. Section Wiring and Connections 3-4 3-4-2 Power Supply Wiring Applicable Power Supply Use a power supply that conforms to specifications of at least 24 VDC and 3.5 W. OMRON’s ...

  • マニュアル

    ...14 Section 2-2 Preparations 2-1-2 System Configuration Example The following diagram shows the operating procedure using a system configuration example. The system configuration shown here uses Thin Cables. C200H-OD215 Output Unit C200HW-DRM21-V1 Master Unit ...

  • マニュアル

    ... supplied voltage becomes lower, the current consumption will increase. Select a device for the power supply that will allow a degree of variation. When selecting a power supply, take inrush current into consideration. The following OMRON products are recommended for the 24-VDC power supply: ...

  • マニュアル

    ... and voltage at the Unit’s connector. Backup Power Supply Specifications The following table shows the input specifications required for backup power supply to SYSMAC LINK Units. Be sure that the backup power supply being used meets these specifications. (We recommend the OMRON ...

  • マニュアル

    .... 4. The Controller Link Units conform to the Emission Standard (EN61000-62) for EMS but, depending on the backup power supply used, they may not conform to the standard for immunity to surges (IEC61000-4-5). In order to ensure conformance, either use an OMRON ...

  • マニュアル

    ...-DRT AC Power Supply Unit (Optional) AC Power Supply Unit Name AC Power Supply Unit Ratings 100 to 240 VAC input 24 VDC, 600 mA output Model CPM2C-PA201 Note General-purpose power supplies such as the S82J-series and ...

  • マニュアル

    ...devices conform. 3. For the Controller Link Support Boards, the backup power supply that is used may affect compliance for surge immunity (IEC61000-4-5) even though common immunity (EN61000-6-2) standards for EMS are met. Either use the recommended OMRON Power Supply (...

  • マニュアル

    ... power supply voltage fluctuation range Consumption current 20.4 to 26.4 VDC (24 VDC, –15 to +10%) Inrush current 2.5 A max. (when 24-VDC rising time is 5 ms) 24 VDC, 400 mA max. (per node) An OMRON S82K...

  • マニュアル

    ... Cables. The following diagram is simplified, so it does not include the separate I/O power supply that must be provided to the Output Unit (or Expansion Output Unit). 22 Section 2-2 Preparations CS1W-DRM21-V1 Master Unit (Node 63) ...

  • マニュアル

    ...3.5 mm Use a SELV power supply with overcurrent protection. A SELV power supply has redundant or increased insulation between the I/O, an output voltage of 30 Vr.m.s and a 42.4-V peak or maximum of 60 VDC. Recommended power supply: ...

  • マニュアル

    ...Phoenix Contact Use a SELV power supply with overcurrent protection. A SELV power supply has redundant or increased insulation between the I/O, an output voltage of 30 Vr.m.s and a 42.4-V peak or maximum of 60 VDC. Recommended power supply: ...

  • マニュアル

    ...Use an SELV power supply with overcurrent protection. An SELV power supply has redundant or reinforced insulation between the I/ O, an output voltage of 30 Vr.m.s and a 42.4-V peak or maximum of 60 VDC. We recommend these Power Supplies. • ...

  • マニュアル

    ...-2 CJ-series Analog I/O Units Operation Manual for NJ-series CPU Unit(W490) 4 CJ-series Analog Output Unit (CJ1W-DA021/041/08V/08C) *2 Select a 24-VDC power supply based on the surge current. The following OMRON power supplies are recommended. ...

  • マニュアル

    .... • Power supply Use a power supply unit that satisfies the following conditions. Condition Power supply voltage 24 VDC +10%, -15% Output current 500 mA DC min. Safety standard UL Class 2 Recommended model Manufacturer OMRON Model ...