全 307 件が検索されました。(61 - 80件を表示)

  • カタログ

    ....5: 2.5mm2 4.0: 4.0mm2 Grounding Terminal Blocks (1) (2) (3) (2) Wiring 1.1: 1:1 1.2: 1:2 (3) Number of Tiers 1: 1 tier 2: 2 tiers (4) Color Blank: Dark gray BL: Blue 2.2: 2:2 1 XW5T Part Names and Configuration DIN Track Terminal Block (Top Surface) Basic Configuration Short Bar Nameplate or Labels Terminal (insertion) hole Release hole (to release wire) Short Bar insertion holes • You can attach a Short Bar to either of the two holes. • Insert the tester pins here to perform a continuity check. Label attachment ...

  • カタログ

    ...Stranded Wire 1.5: 1.5 mm2 2.5: 2.5 mm2 (2) Number of Pins 8: 8 pins 12: 12 pins 16: 16 pins 20: 20 pins 40: 40 pins (3) Color of Short Bars RD: Red BL: Blue YL: Yellow Part Names and Configuration Terminal Block Basic Configuration Terminal (insertion) hole Release hole (to release wire) Indicator (Wire insertion state indication part) Nameplate End Cover Order separately Indicator (Wire insertion state indication part) Label attachment section Insertion hole for Short Bars • Insert the tester pins here to perform a continuity check. Note: Do not insert more than one ...

  • 技術解説/使用上の注意事項

    ...報は タブ端子の小型ローコストタイプ形G3PH AC240/480V 75A、150A 8台 4台 入力の定格電圧 DC5∼24V 共通事項 形G3PE-BLタイプは2台です。 形G3PE-BLタイプは1台です。 形G3PA-BLタイプは2台です。 形G3PA-BLタイプは1台です。 形G3NAの-UTUタイプは2台です。 形G3NAの-UTU...

  • マニュアル

    ...〔酬州lApnclFICPTELM PhOae:1-800-55-OMR〔削 Fax:1-847-s43-7祀「 Phone=1-416-286-{シHis Fax:1-416-2Bl}-6EtB P卜hDne:1-514-{i36-6676『renchi Fax=1-514・-fi36-2959 Phcme=31-23-5G-Bl-300 Fa}《:31-23-{i6-81-3田 Phnne:82-2「3218-5700 Ptmge:8elO-5B69-3〔}30 Pbぬne=852-23了5「3舵7 PhEme:田6-2」2715-3331 Phone:6H芒9878噸3π Phone=65-683i3911 ■取1揃旺寸法蜘Mountinghcks迦:㎜●D4NS-SK30 __2...

  • マニュアル

    ...13 3 4 5 *1: “-AU” Models 12 (−) Function setting mode 8 3 9 10 2 1 11 Total reset 0V (-) Sensor (+) 12 VDC Function setting mode bl-h otst kypt Models other than “- W(U) ----When it is ON, the count will shift from 0 to 999999. Disable the H7AN compatible function when replacing from the H7CX, or H7CX-N. -- 1,000 The monitored value is only displayed. It cannot be set.  1,000 Unit: year The Total run time monitor value is only displayed. It cannot be set. The software version is only displayed. It ...

  • マニュアル

    ...-2 Check Mode Chapter 4 Application H Monitor Details Display Monitored item r Motor speed A’ A C’ C E’ E P’ P F’ F cF cc L bL Present value (leftmost digits) Present value (rightmost digits) Reference value (leftmost digits) Reference value (rightmost digits) Position deviation (leftmost digits) Position deviation (rightmost digits) (Not used.) (Not used.) Mechanical speed (leftmost digits) Mechanical speed (rightmost digits) (Not used.) (Not used.) Motor current Effective load factor Unit r/min Mechanical axis movement o e e t Explanation Displays the actual rotation speed of the motor shaft. Calculates and displays the present ...

  • マニュアル

    ...-9-10 UPS Communication Cable Communication cable details are provided below. OMRON is not responsible for the operation or performance of any other brand of communication cable. Model Appearance S8BW-C02 Cable length 2m Specifications Signals for • Signal output (...

  • マニュアル

    ...MPL.VelocityRatio :=100; MPL.RotationVelocityRatio :=100; MPL.Velocity :=0; MPL.AccelerationRatio :=50; MPL.DecelerationRatio :=50; MPL.NullingTolerance :=_eRC_NULLING_TOLERANCE#_rcFineTolerance; MPL.SingleTurn :=_eRC_SINGLE_TURN#_rcMultipleTurn; //Reserved : [4(16#0)]); //BufferMode; BM_Bu :=_rcBuffered; BM_...

  • マニュアル

    ...) DVB(53) FUN69 FUN89 ASFT(017) XFERC(565) MOVBC(568) DISTC(566) COLLC(567) CMPL(060) MCMP(019) LINE(063) COLM(064) SEC(065) HMS(066) ++B(594) --B(596) +B(404) +BL(405) -B(414) -BL(415) *B(424) *BL(425) /B(434) /...

  • マニュアル

    ...) DVB(53) FUN69 FUN89 ASFT(017) XFERC(565) MOVBC(568) DISTC(566) COLLC(567) CMPL(060) MCMP(019) LINE(063) COLM(064) SEC(065) HMS(066) ++B(594) --B(596) +B(404) +BL(405) -B(414) -BL(415) *B(424) *BL(425) /B(434) /...

  • マニュアル

    ...(51) MLB(52) DVB(53) ADDL(54) SUBL(55) MULL(56) DIVL(57) MPRF(61) LINE(63) Not supported Not supported +C(402) -C(412) *U(422) /U(432) +BCL(407) -BCL(417) *BL(425) /BL(435) Not supported LINE(063) COLM(64) COLM(064) 18 Operand Number of operands When #0 is set to the operand, JMP is converted to #0: Changed from 1 to 0 JMP0 and the operand is deleted. <> #0: Same If a value other than #0 is set, the operand is the same. When #0 is set to the operand, JME is converted to #...

  • マニュアル

    ...(86) DVBL(87) INC(90) DEC(91) INCB(92) DECB(93) INCL(94) DECL(95) INBL(96) DCBL(97) BCNT(114) +BC(406) -BC(416) *B(424) /B(434) +BCL(407) -BCL(417) *BL(425) /BL(435) +C(402) -C(412) *U(422) /U(432) +CL(403) -CL(413) *UL(423) /UL(433) ++B(452) --B(454) ++(448) --(450) ++...

  • マニュアル

    ... BCD DIVIDE EXCLUSIVE NOR ADDL SUBL MULL DIVL XNRW ++B --B +BC -BC *B /B +C -C None SIGNED BINARY MULTIPLY: * None SIGNED BINARY DIVIDE: / +BCL -BCL *BL /BL None (XORW+COM) Subroutine instruction MACRO MCRO None Interrupt control instructions INTERVAL TIMER STIM MSKS INTERRUPT CONTROL INT MSKS MESSAGE DISPLAY MSG None Calculation instructions Special instruction Result of instruction conversion and measure Displayed as error. As CP1E does not have alternative instruction, we recommend you to use CPIL/CP1H. Converted Converted Converted Converted Converted Converted Converted Converted Displayed as error. Use SIGNED BINARY MULTIPLY instead. Displayed as error Use ...

  • マニュアル

    ...DVB DOUBLE BCD ADD DOUBLE BCD SUBTRACT DOUBLE BCD MULTIPLY DOUBLE BCD DIVIDE HOURS-TO-SECONDS SECONDS-TO-HOURS ADDL SUBL MULL DIVL SEC HMS None SIGNED BINARY DIVIDE: / +BCL -BCL *BL /BL None None Special math instructions SUM DATA SEARCH FIND MAXIMUM FIND MINIMUM SUM SRCH MAX MIN None None None None Logic instruction EXCLUSIVE NOR XNRW None (XORW+COM) Subroutine instruction MACRO MCRO None Interrupt control instructions INTERVAL TIMER STIM MSKS Displayed as error. Use MSKS instruction instead. INTERRUPT CONTROL INT MSKS SYNCHRONIZED PULSE CONTROL SYNC None Displayed as error. Use MSKS instruction instead. Displayed as error. CP1E ...

  • マニュアル

    ...581 583 ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ✓ ●Increment/Decrement Instructions Mnemonic ++ ++L ---L ++B ++BL --B --BL INCREMENT BINARY DOUBLE INCREMENT BINARY DECREMENT BINARY DOUBLE DECREMENT BINARY INCREMENT BCD DOUBLE INCREMENT BCD DECREMENT BCD DOUBLE DECREMENT BCD ●Symbol Math Instructions Mnemonic + +L +C +CL +B +...

  • マニュアル

    ...モード 3分 10 秒 通常運転 自己診断テスト 通常運転バックアップ運転スタンバイモード BU 信号(OUT)※2 BL 信号(OUT)※2 BS 信号(IN)※2 通常運転 ON 4 OFF ON OFF ON OFF ※1 工場出荷時設定は「ブザー無効」 です。 「ブザー無効」設定時も起動時のブザーは鳴りま...

  • マニュアル

    ...に起動します。 ON 入力電源 OFF High バッテリ充電容量 Low ON UPS出力 OFF UPS動作モード BU信号(OUT)*1 BL 信号(OUT)*1 BS 信号(IN)*1 *1. 詳細は 4-6 通常運転バックアップ運転 ON スタンバイモード 通常運転 OFF ON OFF ON OFF 「7-1 入出力信号の詳細 (P.7-2)」をご参...

  • マニュアル

    ...) FUN69 FUN89 STEP(08) ASFT(017) XFERC(565) MOVBC(568) DISTC(566) COLLC(567) CMPL(060) MCMP(019) LINE(063) COLM(064) SEC(065) HMS(066) ++B(594) --B(596) +B(404) +BL(405) -B(414) -BL(415) *B(424) *BL(425) /B(434) /...

  • マニュアル

    ...) FUN69 FUN89 STEP(08) ASFT(017) XFERC(565) MOVBC(568) DISTC(566) COLLC(567) CMPL(060) MCMP(019) LINE(063) COLM(064) SEC(065) HMS(066) ++B(594) --B(596) +B(404) +BL(405) -B(414) -BL(415) *B(424) *BL(425) /B(434) /...

  • マニュアル

    ...し ADB(50) SBB(51) MLB(52) DVB(53) ADDL(54) SUBL(55) MULL(56) DIVL(57) MPRF(61) LINE(63) +C(402) -C(412) *U(422) /U(432) +BCL(407) -BCL(417) *BL(425) /BL(435) なし LINE(63) COLM(64) COLM(64) オペランドが#0 の場合は、JMP0 に変換されオペランドはなくなります。 #0 以外の場合は、同じです。 オペランドが#0 の場合は、JME0 に変換...