全 98 件が検索されました。(61 - 80件を表示)
- マニュアル
...紅㎝τぴultユst辿c㎝asσ0.± 夏)a識1:`!1 ∋`62 …CMP2・-1 Compans鵬2Wh翻arg畿men(h缶≧th加泣別mo蝋2,1)A2=亘aロぷh¢卿¢斑10nr¢SUltIS【ak帥鎚目}WhenargUln綱11暴く山都a㎎u鵬nt2、DA加o蜘thぱopcτ釦㎝毘sultlst疏naso・o・ 63 CMP3 ・・一・一ーー一一ーーーーー一・一・・一一・一.一ーーー一一.一....
- マニュアル
... 6 5 1st digit ● Change from RUN Mode to Function Setting Mode. Internal circuit Function setting mode Count Function setting mode Set value up, down --- outm Output mode n, f, c, r, k-1, p, q, aK*1 --- otim Output time 0.01 to 0.50 to 99.99 cnts iflt dp Counting speed 30hz, 5khzK*1 Reset input signal width 20ms, 1msK*1 Decimal point position ------, -----.-, ----.--, ---.--- *1 Prescale value 0.001 to 1.000 to 99.999 Set value upper limit 1 to 999999 Key protect level kp-1, kp-2, kp-3, kp-4, kp-5, kp-...
- マニュアル
...ラメータ名 特記事項 設定値 機 能 設 定モード cntm 入力モード up, down outm 出力モード n, f, c, r, k-1, p, q, aK*1 − otim 出力時間 0.01 ∼ 0.50 ∼ 99.99 cnts iflt dp 計数速度最小リセット時間小数点位置 pscl sl-h kypt プリスケール値設定リミット上限キープロテクト...
- マニュアル
..._』_■』 ■■__一__』糊_■_一■■■」 S◎rt − tedTorqLe] ↑ξ● ↓ Clear Edit − ・こミ♪:こき"§ぶS>こ・s'"XSN.〉「;";、・」■、'"二'・N>・ミ、Ntsい・■>〉ぺ黛×ミミベ:、〉、x's、、、1「"iこ準、、?×べS"〉 Alτ−Ak,EC,」It vwe>くτT『1「酬「1)願爪」 ,3.SelectingaFlleName 6D。 uble-click。 nafilenameinthe[L・adFileList】. 〔柔コSelect[LoadFileList]usingthe「「abKey.SelectthefilenameusingtheUpandDownCursor Keys.PresstheReturnKey. ParametersarereadtOthe旧MPC/ATorcompatible,LoadFilewindowcloses,andprogramreturnstotheUserParameterwindow. 5・12 ---------------------[End of Page 4696]--------------------- Operation ChaPter5 ◎ExistingParameterFiles Tospeed-upthesettingoperationusetheexistingOMRONPositionControiUnit-compatibleparameter filesintheComputerMonitorSoftware. Filename ServoDrivermode1 ApplicablePositionControlUnit UAINT R88D-UA口口H!L C500-NC222-E,...
- マニュアル
...3-11 3-4 Operation Procedure (Example: Factory Default) 3. The code of the basic function mode is displayed (as "F001"). fk0k0k1 Press 3 Press (4 times) (4 times) 4. The extended function mode is displayed (as "A---"). ...
- マニュアル
... basic function mode is displayed (as "F001"). Dfk0k0k1 3 Press . (4 times) Press . (4 times) Operation 4. The extended function mode is displayed (as "A---"). •Extended function mode Displays in order of A ⇔ b ⇔ C ⇔ H. ...
- マニュアル
... sure to press the Enter key. Function mode 3k0.0k1 fk0k0k1 3k0.0k0 (Data display) (Data display) *1 *2 *1 *2 or 2k9.9k9 fk0k0k4 ak0k0k1 Extended function mode A 3 2 ak-k-k- or ak1k5k3 or 1 bk0k0k1 Extended function mode B bk-k-k- or bk1k3k2 ck0k0k1 Extended function mode C ck-k-k- or ck1k5k9 hk0k0k1 Extended function mode H hk-k-k- or hk0k7k3 pk0k0k1 Extended function mode P pk-k-k- or uk-k-kor Key sequence and display system of extended function mode U (See the next page.) pk1k3k1 3-14 3-...
- マニュアル
...Return without saving the changes ak0k0k1 0k2 3G3MX2 Digital Operator ak0k0k1 Move the function group bk0k0k1 0k1 Return after saving the changes (Reference) Key Operation System When the Conventional Digital Operator Model (3G3AXOP01) is Connected to the Conventional Model ...
- マニュアル
...Version Information The information in this document describes features and functionality for the LD-60/90/90x AMR using the following hardware and software versions. • AMR Core Version: Rev. B • Software Version: FLOW Core v4.1.9 • Docking Station Hardware Version: Rev. ...
- マニュアル
... the documentation. Version Information The information in this document describes features and functionality for the LD-250 AMR using the following hardware and software versions. • AMR Core Version: Rev. C • Software Version: FLOW Core v4.1.9 • Docking Station Hardware Version: Rev. ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-14-1 ACK: AK . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-14-2 NACK: NK . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Other Command . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-15-1 Undefined Command Response . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Response Codes . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Connecting Commands . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Communications Programming Example . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 58 59 59 59 60 61 61 63 64 64 67 69 70 70 70 71 71 72 73 73 74 74 75 76 77 78 79 79 80 82 84 84 84 85 85 85 86 86 86 86 86 87 87 87 88 89 57 Section Commands and Responses 5-1 5-1 Commands and Responses In order to communicate with the ID Tag in the communications area of the Antenna, commands ...
- マニュアル
...手順(例:工場出荷状態の場合) ④拡張機能モードを表示(A--- を表示) ・拡張機能モード A ⇔ b ⇔ C ⇔ H の順番で表示します。 ak-k-k- ࠍߔ 㧔࿁㧕 ࠍߔ 㧔࿁㧕 ⑤モニタモードのコード表示(d001 を表示) 3 ・②の状態に戻ります。 dk0k0k1 運転・操作 機能の設定方法 ・運転指令...
- マニュアル
...手順(例:工場出荷状態の場合) ④拡張機能モードを表示(A--- を表示) ・拡張機能モード A ⇔ b ⇔ C ⇔ H の順番で表示します。 ak-k-k- を押す (4回) を押す (4回) ⑤モニタモードのコード表示(d001 を表示) 3 ・②の状態に戻ります。 dk0k0k1 運転・操作 機能の設定方法 ・運転指令...
- マニュアル
...さい。 3k0.0k1 3k0.0k0 (データ表示) fk0k0k4 または (データ表示) *1 *2 2k9.9k9 *1 *2 ak0k0k1 拡張機能モードA 3 2 ak-k-k- または ak1k5k3 または 1 bk0k0k1 拡張機能モードB bk-k-k- または bk1k3k2 ck0k0k1 拡張機能モードC ck-k-k- または ck1k5k9 hk0k0k1 拡張機能モードH hk-k-k- または hk0k7k3 pk0k0k1 拡張機...
- マニュアル
...bk0k0k1 0k1 変更を記憶して戻る (参考)従来機種に従来機種用オペレータ(形 3G3AX-OP01)を接続した場合のキー操作体系 ak-k-k- ak0k0k1 データ表示に移動変更せずに戻る 0k2 従来機種用 3G3AX-OP01 ak0k0k1 該当機能なし bk0k0k1 0k1 変更を記憶して戻る SYSDRIVE MX2 シリーズ ユーザー...
- マニュアル
...-411) 1 はじめに • ソフトウェアバージョン: FLOW Core v4.1.9 • ドッキングステーションハードウェアバージョン: Rev. AK • バッテリバージョン: AF 単位特に断りのない限り、単位はすべてメートル法です。 2 AMR(Autonomous Mobile Robot)LD プラットフォーム ユーザズマ...
- マニュアル
... バージョン: Rev. C • ソフトウェアバージョン: FLOW Core v4.1.9 • ドッキングステーションハードウェアバージョン: Rev. AK • バッテリバージョン: AF AMR (Autonomous Mobile Robot) LD-250 プラットフォーム ユーザズマニュアル (SBCE-477) 1 はじめに 単位特に断りのない限り、単...
- マニュアル
....8 8 . 8.8 .8 SV .8 8.8 B2 SU B1 SU NU MA P RS T RM AT OP ST T2 OU T1 OU AK E5 AM リアケースフロントパネルこのページ ■フロントパネル PV バーグラフ 8.8.8.8 第1表示 SV 8.8.8.8 動作表示LED OUT1 OUT2 SUB1 SUB2 MANU STOP RMT RSP AT A RMT RSP MANU SUB1 OUT1 OUT2 STOP AT 第2表示...
- マニュアル
...HO T RM T1 OU .8 8.8 1 B SU B2 SU T AI W AT NU MA T RS T2 OU AM 0 % AK E5 N RU RST リアケースフロントパネルこのページ ■フロントパネルプログラム状態表示LED バーグラフ 8.8.8.8 OUT1 OUT2 SUB1 SUB2 MANU RMT HOLD RST WAIT AT SV PTN PTN TIME 0 % パターンNo. 7 8.8.8.8 100 動...
- マニュアル
...1 2 3 4 5 6 時間(ms) 50 100 200 300 400 500 AH 2フ レーム AI _AI_ 3フ レーム AJ _AJ_ AK 4フ レーム メ ニ ュ ーシー ト / コ マ ン ド 一覧 _AH_ 4章 1 フ レーム コマン ド 第 メ ニ ュ ーシー ト _AK_ 5フ レーム AL _AL_ 6フ レーム(工場出荷時の設定) AM _AM_ 無限 AG _AG_ 形V400-R1CF/R1CS...