全 792 件が検索されました。(761 - 780件を表示)
- マニュアル
...ル 仕様 100BASE-TX / 10BASE-T 非シールドツイストペアケーブル (UTP) :カテゴリ 5、5e シールドツイストペアケーブル (STP) :カテゴリ 5、5e で 100Ω のもの 1 9 非シールドツイストペアケーブル (UTP) :カテゴリ 3、4、5、5e シールドツイストペアケーブル (...
- マニュアル
... used to connect to an EtherNet/IP network. The twisted-pair cable has a RJ45 Modular Connector at each end. This cable is used to connect the built-in EtherNet/IP port or EtherNet/IP Unit to a Ethernet switch. Use an ...
- マニュアル
... Point/Start from Top Left Corner Default Character Set: English, Japanese, Simplified Chinese, Traditional Chinese, Korean, Turkish, Russian, or Vietnamese Menu and Dialog Language: Japanese, English, Simplified Chinese, Traditional Chinese, or Korean Multi-Language Exchange: On/Off Initial Value Installation folder/...
- マニュアル
... as a run-away motor (NC). 16 CWLY Y-axis CW limit input Limit switch input for Y axis in CW direction (NC) Name 21 Faulty Wiring Diagnostic Function Section 2-3 Configuration of Input Circuit +24V 24V ...
- マニュアル
... also be used as 10Base-T.) (3) Hub Recommended Hubs This is twisted-pair cable for connecting 100Base-TX-type Ethernet Units to the hub, with an RJ45 Modular Connector at each end. Use a category 3, 4, 5, or 5e UTP (unshielded twistedpair) or ...
- マニュアル
... can also be used as 10Base-T.) (2) Twisted-pair cable This is twisted-pair cable for connecting 100Base-TX-type Ethernet Units to the hub, with an RJ45 Modular Connector at each end. Use a category 3, 4, 5, or 5e UTP (unshielded twistedpair) or ...
- マニュアル
...1.0 or later CSMA/CD Baseband Star form 100 Mbit/s (100Base-TX) 10 Mbit/s (10Base-TX) Unshielded twisted-pair (UDP) cable Unshielded twisted-pair (UDP) cable Categories: 5, 5e Categories: 3, 4, 5, 5e Shielded twisted-pair (...
- マニュアル
... used as 10Base-T) CSMA/CD Baseband Star form 100 Mbit/s (100Base-TX) 10 Mbit/s (10Base-T) Unshielded twisted-pair (UTP) cable Unshielded twisted-pair (UTP) cable Categories: 5, 5e Categories: 3, 4, 5, 5e Shielded twisted-pair (...
- マニュアル
...えるには、一度電源を切断してからSWの変更が必要となります。 LAN ケーブルについて ●シールド付きツイストペア(STP)ケーブルをご使用される場合 STPケーブルをご使用されると、耐ノイズ効果が増します。 ただし、ケーブルのシールドは本...
- マニュアル
...Frame length 1,514 bytes max. Media access method CSMA/CD Modulation Baseband Topology Star NY-series Industrial Panel PC Machine Controller Hardware User's Manual (W557) 4-21 4 Specifications Item Specifications Transmission media ...
- マニュアル
...BOOL FALSE TRUE when home is defined for axis 0. Pwr_Status BOOL FALSE This variable is assigned to the Status output variable from the PWR instance of the MC_Power instruction. It is TRUE when the Servo is ON. ...
- マニュアル
.../IP Unit (CS1W-EIP21) (2) Twisted-pair cable The twisted-pair cable has a RJ45 Modular Connector at each end. This cable is used to connect the built-in EtherNet/IP port or EtherNet/IP Unit to an Ethernet switch. Use an ...
- マニュアル
..., WB) • Remote ON/OFF input • UPS Stop Signal input (BS) NY-series IPC Programmable Multi Axis Controller Hardware User's Manual (W580) 2-23 2-10-9 UPS *1. 2 Hardware 2-10-11 Recommended EtherCAT Cables For EtherCAT, use Straight ...
- マニュアル
...:Back 1 Step Cursor Specify the starting line of the measurement region. Step 3. 2 The screen for specifying the region will be displayed. 3 Step 4 Step Sen0's measurement region Strt+0023.597mm Stp -0023.983mm Strt 0lines ...
- マニュアル
... key: Moves the cursor. (Press these keys together with the SHIFT Key to move the cursor quickly.) ENT Key: Selects the setting. The measurement region is registered. Proceed to Step 4. 36 Operation Manual Sen0's measurement region Strt+000.1836mm ...
- マニュアル
... the cursor. (Press these keys together with the SHIFT Key to move the cursor quickly.) ENT Key: Selects the setting. The measurement region is registered. Proceed to Step 4. 36 Z550 Operation Manual Sen0's measurement region Strt+000.1836mm ...
- マニュアル
... that the display at CAM is "a". This indicates that the setting is applied to all cams. PRG TST CAM Setting the number of steps 4-20 STEP Press the [+] or [−] key of the ANGLE keys to set "2". "stp" starts flashing when setting starts. PRG TST CAM End of setting STEP Complete setting by pressing the [WRITE] key. ("...
- マニュアル
...FQ-WN0@@ Connects the Sensors to external devices such as the Touch Finder, computers, and PLCs. Standard RJ45 Ethernet Cable*1 --- Connects the Switching Hub to the Touch Finder, computers, and PLCs. Use a connector that complies with the FCC RJ45 standard. (...
- マニュアル
.... FQ Ethernet Cable FQ-WN0@@ Connects the Sensor to the Touch Finder or computer. Standard RJ45 Ethernet Cable*1 --- Connects the switching hub to the Touch Finder or computer. Use a connector that complies with the FCC RJ45 standard. (...
- マニュアル
...@@@ The Special EtherCAT Cable connects the Sensor to another Sensor or to another EtherCAT device. General-purpose Ethernet cable*1 --- This cable connects the Switching Hub to the Touch Finder, computers, and PLCs. Use a connector that complies with the FCC RJ45 standard. (...