全 916 件が検索されました。(761 - 780件を表示)
- マニュアル
....Fitthehookofthefittinginthe squareholeinthebodyandtightenthescreWwithaPhil│ipsheadscrewdriver whilelightlypullingthefitting. 囁〒1⇒・ト 31 ---------------------[End of Page 6179]--------------------- InstatlationandConnection Section2"3 2・3・2 C◎nnectingtheNT612GtoaH◎stUnit ComecttheNT612Gtoahostunit(suchasaPCandacomputer)withacable. Differenthostl/Funitsrequiredifferentconnectionmethodsandcables.ThefolIowingfiguresshowconnectionofsomehostunitstotheNT612G.Forconnection,refertotheuser'smanualofeachhostl/Funit.' WhereaHostllFUnitisUsed SYSMACC・・seriesPC, CVMi/...
- マニュアル
...-LK201 type: NT600M-LK202 type: RS-232C RS-422 PC or communication unit with a host link function 11 Connection of NT610C and Host Units Section 1-6 NT Link Where a PC is that of the CQM1 or CVM1/CV series, the NT610C may be connected to the PC, using a host link method. In this case, a host link I/F unit must be installed in the NT610C and connected to the host unit through the RS-232C cable while a system ROM is used that is different from the ordinary ROM for the host link. The ...
- マニュアル
... 0005) 1-3-4 NT LINK The NT link is a communication method of the host link I/F units. The NT link uses the direct connection function and can execute high speed communications with a CPU (built-in host link) of the C and CVM1/...
- マニュアル
... cable(*) (for host link) (Max. 500 m) Printer Can print out screens being displayed at the NT620S/NT620C. OMRON’s PC Controls NT620S/620C as required while controlling machines and monitoring the production line. Host link: C series, CVM1/...
- マニュアル
... a PC. Refer to the manuals for individual devices for information on devices other than the NT30/30C in the system. OMRON PC Controls the NT30/30C as required while controlling machines and monitoring the production line. Host Link: C-series PC, CVM1/...
- マニュアル
... in advance. The “PLC Vendor” is set with the support tool. The applicable programmable controllers (PCs) depending on the “PLC Vendor” setting are as follows. PLC Vendor Applicable Programmable Controller (PLC) OMRON For connection to an OMRON CS1 series, C series, or CVM1/...
- マニュアル
...-3 NT Link NT link is a method for high--speed communications with a PC using the direct connection function. The PCs that can be connected to NTH25/NTH25C with the NT link are as follows: CPM1, CQM1, C200HS, C200HX/HG/HE(--Z)E, CVM1/...
- マニュアル
... comments are automatically saved in a file with an extension .SP1. 301 I/O Comment Table Section 7-7 SYSMAC CPT saves ladder program in SSS program (*.SP1) and use this file to import I/O comment. I/O comment of CVM1/...
- マニュアル
...1-3-1 Peripheral Devices That Can Be Connected The following peripheral devices can be connected to an NT31/NT31C. Host Controls the NT31/NT31C as required while controlling machines and monitoring the production line. Host Link: CS/CJ-series, C-series, and CVM1/...
- マニュアル
...1-3-1 Peripheral Devices That Can Be Connected The following peripheral devices can be connected to an NT631/NT631C. Host Controls the NT631/NT631C as required while controlling machines and monitoring the production line. Host Link: CS/CJ-series, C-series, and CVM1/...
- マニュアル
...-1 Peripheral Devices That Can Be Connected The following peripheral devices can be connected to the NT31/NT31C and NT631/NT631C. Host Controls the NT31/NT31C or NT631/NT631C as required while controlling machines and monitoring the production line. Host Link: C series, CVM1/...
- マニュアル
... Programmable Terminals. The DeviceNet (CompoBus/D) Interface Unit is used with NT31, NT31C, NT631, and NT631C PTs. “CS1 Series” refers to CS1H and CS1G PCs and related products. “C Series” refers to C200H, C1000H(F), C2000H, C200HS, CPM1, and CQM1 PCs and related products. “CVM1/...
- マニュアル
...1-3-1 Peripheral Devices That Can Be Connected NT21 The following peripheral devices can be connected to an NT21. Host Controls the NT21 as required while controlling machines and monitoring the production line. Host Link: CS/CJ-series PCs, C-series PCs, CVM1/...
- マニュアル
... is used in this manual. 8 PT In this manual, indicates an NS-series Programmable Terminal. NS Series Indicates products in the OMRON NS@ @ Series of Programmable Terminals. PLC Indicates a Programmable Controller in the OMRON SYSMAC CS/CJ, C, or CVM1/...
- マニュアル
... following terminology is used in this manual. PT In this manual, indicates an NS-series Programmable Terminal. NS Series Indicates products in the OMRON NS@ @ Series of Programmable Terminals. PLC Indicates a Programmable Controller in the OMRON SYSMAC CS/CJ, C, or CVM1/...
- マニュアル
... following terminology is used in this manual. PT In this manual, indicates an NS-series Programmable Terminal. NS Series Indicates products in the OMRON NS[ ] [ ] Series of Programmable Terminals. PLC Indicates a Programmable Controller in the OMRON SYSMAC CS/CJ, C, or CVM1/...
- マニュアル
... Support Software Operation Manual: CVM1 PLCs SYSMAC CPT User Manual and Quick Start Guide W249-E1-@ W332-E1-@ W333-E1-@ CX-Programmer Ver. 4 User Manual SYSMAC C Series Host Link Unit System Manual W425-E1-@ W143-E1-@ SYSMAC CVM1/...
- マニュアル
...Connection to another company’s PLC Connection to the Barcode Reader Transferring project data to the NS Series/NSRuntime 1-8 NS Series 1024 X 768 dots max. (When using NS15) Any of the following Series: C, ...
- マニュアル
... communications. The connection can be made either directly to the built-in serial port on the CPU Unit or to a Host Link Unit mounted to the PLC. C Series C200HS, C200HX/HG/HE(-Z), CQM1, CQM1H, CPM2A/CPM2C, CPM1/CPM1A, C500, C1000H, C2000H ...
- マニュアル
... Series PLC CPU Unit NV-Designer Host xii In this manual, indicates an NV-series Programmable Terminal. Indicates products in the OMRON NV Series of Programmable Terminals. Indicates a Programmable Controller in the OMRON SYSMAC CS/CJ/CP, C, or CVM1/...