全 916 件が検索されました。(841 - 860件を表示)
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . 308 309 Appendices A B PLC Comparison Charts: CJ-series, CS-series, C200HG/HE/HX, CQM1H, CVM1, and CV-series PLCs . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 317 Changes from Previous Host Link Systems . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 343 Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 347 Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 353 xxii About this Manual: This manual describes the programming of the CPU Units for CS/CJ-series Programmable Controllers (PLCs) and includes the sections described on the following page. The CS Series, CJ Series and NSJ Series are subdivided as shown in the following figure. NSJ Series CJ Series CS Series CS1-H CPU Units CJ2 CPU Units CJ2H-CPU@@-@@@ CS1H-CPU@@H CS1G-CPU@@...
- マニュアル
... through the Controller Link Support Board to a PLC with a Controller Link Unit mounted. Connecting through the Ethernet Board to a PLC with an Ethernet Unit mounted. (1) Host Link communications use FINS commands enclosed in a header and terminator data (i.e., SYSWAY-...
- マニュアル
...SPD ATN SPE: Serial-poll enable TA: Talker address STB: Status byte SPD: Serial-poll disable 1-4 1-4-1 Comparison with other OMRON Units’ GP-IB Functions Functional Comparison Model CS1W-GPI01 C500-GPI01 CVM1, ...
- マニュアル
... for Ethernet Unit in the Unit settings (CPU Bus Unit setups). Applicable models: CS1W-ETN21, CJ1W-ETN21 •Importing DM/EM Data Files from Previous Support Software Previous version (version 3.1) DM/EM data files created with the SYSMAC Support Software (SSS) or ...
- マニュアル
...Compatible PLCs, PTs and Programmable Relay...................................................... 13 Connection Configurations.......................................................................................... 14 General Specifications ................................................................................................ 15 Dimensions .............................................................................................. 16 D-sub Connector Cable .............................................................................................. 16 System Configuration............................................................................... 17 CS/CJ-series PLCs ..................................................................................................... 17 C-series PLCs ............................................................................................................. 19 CVM1 and ...
- マニュアル
...Version CS-series Ethernet Unit 100BASE-TX CS1W-ETN21 10BASE-5 10BASE-T CS1W-ETN01 CS1W-ETN11 CJ-series Ethernet Unit 100BASE-TX CJ1W-ETN21 10BASE-T 10BASE-5 CJ1W-ETN11 CV500-ETN01 CV/CVM1-series Ethernet Unit FinsGateway Version 4.xx or lower Version 2003 or higher Programmable Terminal Open Network Controller (ONC) 106 NS Series --- Supports automatic generation method (dynamic)? Yes No: Set by automatic generation method or combined method. Communications are not possible with personal computers with variable IP addresses. Yes No: Set by automatic generation method or combined method. Communications are not possible with personal computers ...
- マニュアル
... the parameter area. 6-3-3 Using Socket Services with CMND(490) Service request commands can be sent to the Ethernet Unit by executing the CMND(490) instruction in the ladder diagram. CS/CJ Ethernet Units support the same functionality as the CVM1/...
- マニュアル
... Support Software. The Controller Link Support Software enables manually set data links and other procedures for a Controller Link Network. Installation, setup, and operating procedures for the W309 Wired Controller Link Units. Controller Link Units are used to connect C200HX/HG/HE, ...
- マニュアル
... damages resulting from the use of the information contained in this publication. CX-Programmer_Page (ii) OMRON PART1: CX-Programmer About this Part This part describes the CX-Programmer application and its ability to create and maintain programs for use with OMRON SYSMAC CS, ...
- マニュアル
... to a PLC with a sGateway Version 2) Controller Link Unit mounted. ETN_UNIT Driver Connecting through the Ethernet Board to a PLC with an Ethernet Unit mounted. Host Link communications use FINS commands wrapped in header and terminator data (i.e., SYSWAY-...
- マニュアル
...Model/Series/ Version CS1D-ETN21D CS-series Ethernet Unit 100Base-TX 10BASE-5 CS1W-ETN21 CS1W-ETN01 10Base-T CS1W-ETN11 CJ-series Ethernet Unit 100Base-TX 10Base-T CJ1W-ETN21 CJ1W-ETN11 CV/CVM1-series Ethernet Unit 10BASE-5 CV500-ETN01 FinsGateway Version 4.xx or earlier Version 2003 or higher Programmable Terminal Open Network Controller (ONC) Supports combined method? Yes Yes No: Set by automatic generation method or combined method. Communications are not possible with personal computers with variable IP addresses. Yes No: Set by automatic generation method or combined method. Communications are not possible with personal computers ...
- マニュアル
... compatible 9-pin connector Built-in RS-232C port on CPU Unit or Serial Communications Board/Unit Peripheral port on CPU Unit CS1W-CN118 (0.1 m) CS1W-CN226 (2.0 m) CS1W-CN626 (6.0 m) XW2Z-200S-CV (2.0 m) XW2Z-500S-...
- マニュアル
...[W434-E1-01] CVM1-LK401 PC Link Unit Operation Manual Cat. No. W434-E1-01 This manual is PDF file only. SYSMAC CVM1/CV Series CVM1-LK401 PC Link Unit CVM1-LK401 PC Link Unit Operation Manual Produced July 2004 iv Notice: OMRON products are manufactured for use according to proper procedures by a qualified operator and only for the purposes described in this manual. The following conventions are used to indicate and classify precautions in this manual. Always heed the information provided with them. Failure to heed precautions can result in injury to people or damage to property. !...
- マニュアル
...CS1W-CN118 (See note.) PC-9801 BX PC-9801 BX NEC NEC CS1W-CN226 CS1W-CN626 Note 10-pin 9-pin female 9-pin female RS-232C port (9-pin female) XW2Z-200S-CV / 200S-V (2.0 m) XW2Z-500S-CV / 500S-V (5.0 m) XW2Z-200S-...
- マニュアル
... damages resulting from the use of the information contained in this publication. CX-Programmer_Page (ii) OMRON PART1: CX-Programmer About this Part This part describes the CX-Programmer application and its ability to create and maintain programs for use with OMRON SYSMAC CS, ...
- マニュアル
... side of the instance. The value of the input source (data contained in the specified parameter just before the instance was called) will be passed to the input variable. P_On 1.0 FB EN ENO D0 D100 PV ...
- マニュアル
...CS1W-CN118 (0.1 m) (See note 1.) CS1W-CN226 (2.0 m) CS1W-CN626 (6.0 m) CS1W-CN118 (See note 1.) CS1W-CN226 CS1W-CN626 9-pin 10-pin RS-232C port (9-pin female) XW2Z-200S-CV/200S-V (2.0 m) XW2Z-500S-CV/500S-V (5.0 m) XW2Z-200S-...
- マニュアル
...RUN CX-Designer Model: NSJ Protocol: USB USB Off-the-shelf USB cable USB port Connecting to an RS-232C Port (Serial Port A or B) Connect the Programming Device to serial port A or B using an XW2Z-200SCV/500S-...
- マニュアル
..., refer to the Product Guide in the package. For details on procedures for installing the CX-Drive from the CX-One FA Integrated Tool Package, refer to the CX-One Setup Manual (W463) provided with CX-One. Cat. No. W463 Model CXONE-@@@@...
- マニュアル
.../ALM INH PRPHL COMM CS/CJ-series PLC OPEN MCPWR L1 BUSY AC100-240V INPUT L2/N PERIPHERAL For Peripheral Port : CS1W-CN226 or CS1W-CN626 For RS-232C Port: XW2Z-200S-CV or XW2Z-500S-CV Or via network RUN OUTPUT AC240V DC24V PORT RS-422A/485 Modbus-RTU Inverter FREF FOUT IOUT MNTR F/R LO/RE PRGM RUN MIN MAX FREQUENCY STOP RESET SYSDRIVE DIGITAL OPERATOR PJVOP140 RUN ALARM *1. CS/CJ-series Serial Communications Board/Unit Ver. 1.2 or later. Required devices Model 3G3JV 3G3MV 3G3RV (-V1) Note Required Devices 3G3JV-PSI485J RS-422/...