全 44876 件が検索されました。(7141 - 7160件を表示)

  • マニュアル

    ... in USA, Canada and Europe Right side This manual must be consulted in all cases in order to find out the nature of the potential HAZARDS and any actions which have to be taken to avoid them. If the equipment is used in ...

  • マニュアル

    ... the NX series components in USA, Canada and Europe This manual must be consulted in all cases in order to find out the nature of the potential HAZARDS and any actions which have to be taken to avoid them.If the equipment is used in ...

  • マニュアル

    ... Code in the USA and the Canadian Electrical Code, Part I in Canada and may vary from information given in the product manuals or safety precautions. ● Surrounding Air Temperature The rated temperature for all Units is 55°C. Type NX-ID6142-5 is suitable for ...

  • マニュアル

    ..., the manuals for the CPU Unit and Communication Control Unit, and the manuals for all other Units in the Controller. Contact your OMRON representative and make sure that you use the most recent version of each manual. Keep this document and all relative manuals in ...

  • マニュアル

    ...。 ただし、次に掲げる用途であっても当社の意図した特別な商品用途の場合や特別の合意がある場合は除きます。 (a)高い安全性が必要とされる用途(例:原子力制御設備、燃焼設備、航空・宇宙設備、鉄道設備、昇降設備、娯楽設備、医用機器、安全...

  • マニュアル

    ...に設置してください。 ・DC 電源を供給するユニットに接続する DC 電源は、以下の項目を満たすようにしてください。 (a) 強化絶縁、または二重絶縁されたもの (b) 出力保持時間が 20ms 以上 (c) IEC/EN60950-1, EN50178 の要求を満足する SELV 電源・電源ケーブルの長...

  • マニュアル

    ...メモリカード 取扱説明書(日/英語) Precautions for Correct Use Start NX-series NX102 CPU Units NX-CSG Communication Control Unit Memory Cards for Updating Firmware Procedures to Update Firmware with ...

  • マニュアル

    ... which rated temperature is 80°C or above. SYSMAC NX102 series INSTRUCTION SHEET © OMRON Corporation 2019 All Rights Reserved. Precautions for Compliance with UL/ CSA Standards and EU Directives Cleaning Do not use paint thinner or similar chemical to clean with. Use ...

  • マニュアル

    ... NX1P2 and NX1W series in USA, Canada and Europe. This manual must be consulted in all cases in order to find out the nature of the potential HAZARDS and any actions which have to be taken to avoid them. If the equipment is used in ...

  • マニュアル

    ... Standards and CSA Standards Solenoid or Valve 3-Wire Sensor Notice to Users of NXR-@@@@@@-@@@ components in USA and Canada 4 IO-Link Master Unit NXR-ILM08C-EIT [Unit/Input Power Supply] 24 VDC (-15% to +10%), MAX. 4.0 ...

  • マニュアル

    ...[3102117-5C] NX series (NX-SL5[][][]/-CSG320) Instruction Sheet (Precaution for UL CSA Standards) Do not touch the NX bus connector Definition of Precautionary Information Left side Caution NG Indicates ...

  • マニュアル

    ... equipped with an over-current protection with current limitation. This manual must be consulted in all cases in order to find out the nature of the potential HAZARDS and any actions which have to be taken to avoid them. If the equipment is used in ...

  • マニュアル

    ... the safe usage of the Controller, read and understand this document and the manuals for all other Units in the Controller. Contact your OMRON representative and make sure that you use the most recent version of each manual. Keep this document and all relative manuals in ...

  • マニュアル

    ...and understand this document, the manuals for the CPU Unit and the manuals for all other Units in the Controller. Contact your OMRON representative and make sure that you use the most recent version of each manual. Keep this document and all relative manuals in ...

  • マニュアル

    ... ە‬Compliance with Class I Division 2 Hazardous Location: Input and output wiring must be in accordance with Class I Div.2 wiring methods and in accordance with the authority having jurisdiction. 1. This equipment is suitable for use in Class I, Div.2, Group ...

  • マニュアル

    ... Automation Controller Industrial PC Platform NJ/NY-series NC Integrated Controller User’s Manual NJ501-5300 NY532-5400 CPU Unit O030-E1-07 NOTE 1. All rights reserved. No part of this publication may be reproduced, stored in ...

  • マニュアル

    ... (G code) Machine Automation Controller Industrial PC Platform NJ/NY-series G code Instructions Reference Manual NJ501-5300 NY532-5400 O031-E1-03 NOTE 1. All rights reserved. No part of this publication may be reproduced, stored in ...

  • マニュアル

    ...[O032-E1-03] SYSMAC-RTNC[][][][][] CNC Operator Operation Manual Operation Software CNC Operator Operation Manual SYSMAC-RTNC O032-E1-03 NOTE All rights reserved. No part of this publication may be reproduced, stored in ...

  • マニュアル

    ...from excessive or corrosive moisture, abnormal ambient temperatures, and conductive materials. If Delta Tau Data Systems, Inc. products are directly exposed to hazardous or conductive materials and/or environments, we cannot guarantee their operation. Security Measures To prevent computer viruses, install antivirus software on ...

  • マニュアル

    ... CPU Unit User’s Manual NJ501-R520 NJ501-R500 NJ501-R420 NJ501-R400 NJ501-R320 NJ501-R300 CPU Unit O037-E1-08 NOTE 1. All rights reserved. No part of this publication may be reproduced, stored in a retrieval system, or transmitted, in any form, or by any means, mechanical, electronic, photocopying, recording, or otherwise, without the prior written permission of OMRON. 2. No patent liability is assumed with respect to the use of the information contained herein. Moreover, because OMRON is constantly striving to improve its high-quality products, the information contained in this manual is subject to ...