全 44873 件が検索されました。(6961 - 6980件を表示)
- マニュアル
...[2256876-5B] H3CR-AP ソリッドステート・タイマ 取扱説明書 (日/英/中語) C J UK/USA Nomenclature (A,B,B2,C,D,E,G,J) H3CR-AP Power indicator Output indicator Rated time selector Time unit selector Setting dial (setting time value) Operation mode selector POWER OUT 15 MODE 10 20 5 C 25 0 30 min J Note: If pointer is turned counterclockwise until overranged, instantaneous output will be issued. (zero point instantaneous operation) H3CR INSTRUCTION MANUAL UK/USA (sec,10s,min,10min,hrs,10h) (1....
- マニュアル
... den Zeitbereich hinausdreht, wird der Sofortkontakt gesetzt. Remarque: Si le pointeur est tourné dans le sens inverse des aiguilles d'une montre jusqu'à sortir de l'échelle graduée, une sortie instantanée sera créee. 66.6 45+ 0.6 0 □ φ37φ14 ...
- マニュアル
... conditions. Consider the actual application conditions and do not exceed the rated load or electrical life. If the output relay is used beyond its service life, the contacts may fuse or burning may occur. Also, never exceed the rated load current. When using ...
- マニュアル
...Front connection socket ᒻP2CF-08, P2CF-11 㧙㕙ធ⛯࠰ࠤ࠶࠻ ᒻP3G-08, P3GA-11 㧙ⵣ㕙ធ⛯࠰ࠤ࠶࠻ ޓ ޓޓޓ㧦H3CR-F8(N) ާ 㧦H3CR-F(N)ި ޓ ޓޓ ި Dimensions A 㧙 Panel cutout dimensions Applicable socket A 㧙ࡄࡀ࡞ࠞ࠶࠻ኸᴺ 㧔㨠―ࡄࡀ࡞ෘ㧕 ㆡ↪ធ⛯࠰ࠤ࠶࠻ޓ ශਭP3G-08, P3GA-11 䘔ᨈᓝ ȼ ԙ㺞φH3CR-F8(N) ާ ԙ㺞φH3CR-F(N) േ࠴ࡖ࠻ Model P3G-08, P3GA-11...
- マニュアル
...0.6 45+ 0 Avant d'utiliser ce produit, veuillez, s'il vous plait, lire attentivement ce manuel pour vous familiariser avec le produit. □ φ39 48 Karasuma Nanajo, Shimogyo-ku, Kyoto 600, Japan Dimensions Abmessungen D ...
- マニュアル
...] H3CR-G スター・デルタタイマ 取扱説明書 (日/英/伊/独/仏/西語) Safety Precautions UK/USA D Model H3CR-G UK/USA CAUTION STAR-DELTA TIMER Sicherheitsvorkehrungen Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury or in property damage. ●Sicherheitshinweise CAUTION D Bedienungsanleitung F Manuel d'instructions The life of the output relay largely depends on the switching current and other switch conditions. Consider the actual application conditions and do not exceed the rated load or electrical life. If the ...
- マニュアル
...п䀈ᐛ֒⽰⚥ Ԛ ᱕ᐛ֒ᰬ䰪䘿 ԛ - 䖢ᦘᰬ䰪䘿 Ԝ 䇴ᇐࡱᓜⴎ δ᱕ᐛ֒ᰬ䰪ε 15 6 78 0.7 㧗0.6 45ޓ 0 □ φ3 9 A 44.8 0.6 45 㧗 ޓ0 t㧩1㨪5 © All Rights Reserved ⚦ߥ↪ᣇᴺߪwww.fa.omron.co.jp߳ࠕࠢࠬࠍ߅㗿ߒ߹ߔޕ t1 3 5 ― 8㧔䗉࠰㧕 6 ― 8㧔䗉࠰㧕 ( ) *2 ( ) *3 C H3CR-G8EL ԝ Ԡ Ԟ ᄖᒻኸᴺ UK/USA Dimensions ...
- マニュアル
....6 sec D Bedienungsanleitung F Manuel d'instructions ➂ ➁ (0.6, 1.2, 6, 12) [mm] Bitte lesen Sie diese Betriebsanleitung sorgfältig durch, bevor Sie mit dem Gerät arbeiten. 15 +0.6 45 0 □ φ39 A 44.8 OMRON Corporation 0.6 45 + 0 t=1∼5 t t Rt (POWER) (Ry ON)*1 ●H3CR-H8RL(-HRL*2 ) *2 ― ― ― ― *2 ― ― *2 ― ― *2 ― ― t Rt (OUT) * ** P3G-08, P3GA-11 rückseitige Klemmen Zeitablauf F t :Einstellzeit *1 :(Relais EIN) Anzeige *2 :Pin No der- HRL t :Réglage du temps * 1 :(Ry ON) indicateur * 2 :Numéro de borne pour le type -HRL (...
- マニュアル
...[2245464-6B] H3CR-H 電源オフディレータイマ 取扱説明書 (日/英/伊/独/仏/西語) Safety Precautions UK/USA D Model H3CR-H UK/USA Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury or in property damage. CAUTION POWER OFF DELAY TIMER ●Sicherheitshinweise CAUTION D Bedienungsanleitung F Manuel d'instructions ACHTUNG The H3CR Series uses ...
- マニュアル
... 2256879-0A t C t Rt t Rt ― ― ― δགྷփε 㧖2 ― ― δ䗉࠰ε 㧖2 ― δ䗉࠰ε ― δ⭫Ⓠε 㧖2 ― ― Dimensions A 㧙ࡄࡀ࡞ࠞ࠶࠻ኸᴺ 㧔t = ࡄࡀ࡞ෘ㧕 A 㧙Panel cutout dimensions 䘸⭞Ⲻᨈᓝ ㆡ↪ធ⛯࠰ࠤ࠶࠻ Applicable socket ශਭP2CF-08, P2CF-11 ࢃ䘔ᨈᓝ ᒻ P2CF-08, P2CF-11 㧙 㕙ធ⛯࠰ࠤ࠶࠻ Model P2CF-08, P2CF-11 Front connection socket ශਭP3G-08, P3GA-11 䘔ᨈᓝ ᒻ P3G-08, P3GA-11 㧙 ⵣ㕙ធ⛯࠰...
- マニュアル
... wiring. Minor injury due to electric shock may occasionally occur. Do not disassemble, modify, or repair the Timer or touch internal components. Minor electric shock, fire, or malfunction may occasionally occur. Precautions for Safe Use 1) When mounting the Timer to ...
- マニュアル
...[3616492-6A] H5CC デジタルタイマ 取扱説明書(日/英語) Precautions for Safe Use 1) When mounting the Timer to a panel, tighten the two mounting screws alternately, a little at a time, so as to keep them at an equal tightness. If the panel screws are tightened unequally, water may enter the panel. indicator LEDs, LCD, and resin parts may deteriorate more quickly depending on the application environment, preventing normal indications. Periodic inspection and replacement are required. 21) The waterproof packing may deteriorate, shrink, or harden depending on the application...
- マニュアル
...に対し余裕を持った使い方や、万一故障があっても危険を最小にする安全回路などの安全対策を講じてください。 a) 屋外の用途、潜在的な化学的汚染あるいは電気的妨害を被る用途またはカタログ、取扱説明書等に記載のない条件や...
- マニュアル
...Do not touch any of the terminals while power is being supplied. Doing so may result in electric shock. Be sure to mount the terminal cover after wiring. Do not use the product where flammable or combustion gases are present. There may be ...
- マニュアル
...に対し余裕を持った使い方や、万一故障があっても危険を最小にする安全回路などの安全対策を講じてください。 a)屋外の用途、潜在的な化学的汚染あるいは電気的妨害を被る用途またはカタログ、取扱説明書等に記載のない条件や...
- マニュアル
... the product for the systems, machines, and equipment with which it will be used. Know and observe all prohibitions of use applicable to this product. NEVER USE THE PRODUCTS FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS ...
- マニュアル
...Key protection 16 Counter and Panel Cutout Dimensions 1 Relay output Definition of Precautionary Information IP54 (front section only) Note: Reduce the load current as shown in the diagram on the right according to the power supply voltage if ...
- マニュアル
...Key protection 16 Counter and Panel Cutout Dimensions 1 Relay output Definition of Precautionary Information IP54 (front section only) Note: Reduce the load current as shown in the diagram on the right according to the power supply voltage if ...
- マニュアル
...the product is installed in the USA or Canada. These conditions are required by NFPA 70, National Electrical Code in the USA and the Canadian Electrical Code, Part I in Canada and may vary from information given in the product manuals or safety precautions. • Installation in ...
- マニュアル
...ーブル選定・その他の条件については、該当するマニュアル、 もしくは取扱説明書を参照ください。 ・この商品は 「class A」 (工業環境商品) です。 住宅環境でご利用されると、 電波妨害の原因となる可能性があります。 その場合には電波妨害に対する...