全 53645 件が検索されました。(6661 - 6680件を表示)
- マニュアル
... VOC-1MS2 と組合せた場合 ) 逆電力:動作電力整定 0.2% 時± 10%、それ以外の動作整定時± 5% 零相電圧 5. システム構成 R S T フロントカバー CT 100-6ε% 以上 ※ ε=2.3%+( 定格値 / 動作電圧値 ) × 0.16% 復帰値 ※R 相監視時の例 専用 CT 電流入力 逆電力 動作値の 80% 以...
- マニュアル
...°C/-340.0 to +940.0°F Measurement resolution 0.1°C Indication accuracy (at ambient temperature: 23°C) Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’ ...
- マニュアル
...换器 注意 -UI P-RSUCER K3FTRANSD 1562°F mA - 20 8°F V/ 0(4) /-23 0°C 1 - 5 - 85 - 10V, 50°C A, 0 : -1 ) - 20m E G AN 0(4 S. R MEA: OUT OUT U,I 2 3 1 7+ R E DC POW 82 GND IN GND DA l No. a Seri tion ora Corp ANY RON ERM OM E IN G D MA Do not allow pieces of metal, wire clippings, or fine metallic shavings or filings to enter the product.Doing so may occasionally result in minor or moderate injury or ...
- マニュアル
... °F PLE 00° C/-238 10V U 2 O 1 C 0° 0 0°C - 135 - 5V, RMO -15 )1 THE : J 0°C , (0 GE -15 mA AN K ) - 20 0(4 S. R A ME P- K3F 5+ ,I OUT TU 6OU D1 GN 7+ ER W DC PO 24V 8D GN 2 3 IN 4 n tio N ora PA orp 0 JA N C 53 NY RO 00-8 MA OM to, 6 GER o Ky DE IN MA 0 有时可能会发生轻度感电,着火,机器...
- マニュアル
...説明書等に 記載のない条件や環境での使用 Suitability for use OMRON shall not be responsible for conformity with any standards, codes, or regulations that apply to the combination of the products in the customer'...
- マニュアル
... are initialized. Take this into consideration when setting up the control system. 10)Install an external switch or circuit breaker and label them clearly so that the operator can quickly turn OFF the power. 11)Ensure that the rated voltage is achieved no longer than 2 ...
- マニュアル
... of their respective companies. OMRON EUROPE B.V. (Importer in EU) Wegalaan 67-69, NL-2132 JD Hoofddorp The Netherlands Phone 31-2356-81-300 FAX 31-2356-81-388 OMRON ELECTRONICS LLC 2895 Greenspoint Parkway, Suite 200 Hoffman Estates, IL 60169 U....
- マニュアル
...Overvoltage category II, Measurement category II (CAT II, ZCT (IRT) input), Pollution Degree 2 (EN 61010-1) Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...売店やオムロン販売拠点は、Webページでご案内しています。 Specifications Precautions for Safe Use (1) Thank you for purchasing the K6PM-series. Be sure to read the K6PM User's Manual (Cat. No. H231) before using the product. 2871954-4A Safety Precautions zWarning Indications WARNING Indicates a potentially hazardous situation which, if not avoided, could result in death or serious injury. Additionally, there may be severe property damage. (2) (3) (4) (5) (6) Indicates a potentially hazardous situation which, if CAUTION not avoided, may ...
- マニュアル
...following items when using the Product. Before using the Product, thoroughly read and understand this manual to ensure correct use. This Product is designed for use by qualified personnel with a knowledge of electrical systems. Be sure to read the K7DD User'...
- マニュアル
...If the measurement value dropped below the alarm value, the xx.x (MΩ) alarm output indicator is lit red and ALM 2 (critical) will be output. One Alarm value 2 is provided in common for all channels. Motor Stop Waiting Time mtwt xxx (...
- マニュアル
...E E E E E E E (14) メインユニットとプローブユニットを確実に連結させてご使用くださ TN-C-S い。 L1 L2 (15) プローブユニット増設台数は仕様範囲内で行ってください。 (16)動力源と負荷の間には必ず電磁接触器などを設置し、本機はそ...
- マニュアル
...:AC24V 50/60Hz、DC24V -20 ∼ 65℃ (ただし、結露または氷結のないこと) 高度 2000m 以下 耐振動 振動数 10 ∼ 55Hz、片振幅 0.35mm、 加速度 50m/s²、 X/Y/Z 各方向 5min×10 掃引 耐衝撃 100m/s² 3 軸 6 方向 各 3 回 保護構造 IP20 端子台形状 プッシュイン Plus ケース外装色 黒(マンセル N1.5) 取り付...
- マニュアル
... accidents. Change the position of side SW while power is NOT being supplied. Safety Precautions A malfunction in the product may occasionally make control operations impossible or prevent alarm outputs, resulting in property damage to connected equipment and machinery. Periodically check the product'...
- マニュアル
...を改善。 - CSV出力の1分対応 R 2021 年 10 月 ・仕様追加に伴う改訂演算チャネルの入力を最大32チャネルに拡張 S 2024 年 6 月 ・セキュリティ対策を「使用上のご注意」に追加・システム内部ファイル、ユーザ指定ファイルの保存期間とタイミングに...
- マニュアル
...イス、 K3HB、NJ/NX1P ・動作環境(対応 OS)の変更・環境センサの通信タイムアウトの設定機能を追加対応機種:D6FZ-FGX21, ZN-CTX21, ZN-KMX21, ZN-DPX21-S, ZN-THX21-S, ZN-PD03-S, ZN-PD50-S ・接続先サーバの指定方法の改善・EQ サーバ管理に開始機能を追加・EQ-Andon の最大表示グラフ数の変...
- マニュアル
...ータ出力」) 設定項目追加(「5.11.5 設定」) ・無線ユニットでの K3GN/E5CC/E5EC をサポート。 (「9.5.1 計測デバイスの設定内容一覧」)s ・ K3GN 、KM1-EMU8A での ON/OFF 値 取 得 の 追 加 設 定 (「9.5.2 計測デバイスチャネル一覧」) ・データ種別に ON/OFF を追加(「9.5.3 データ種別一覧}) そ...
- マニュアル
...1.7. 機能一覧 ........................................................................................................... 1-15 1-1 第 1 章 形 KM-N1 の概要 1.1. 主な特長 (2) 高精度計測電流,電圧計測精度:±0.5%F....
- マニュアル
...配列は以下のとおりです。 電圧入力端子電圧入力端子 相線式 設置と配線 V1 V2 V3 VN 三相 4 線 R S T N 単相 2 線 L − − N 単相 3 線 R − T N 三相 3 線 R S T − 【参考】 • R/S/T/N は U/V/W/O や L1/L2/L3/N と表記されることがあります。 • R/N/T は U/O/W や ...
- マニュアル
...のとおりです。 計測電圧入力端子 相線式 設置と配線 計測電圧入力端子 V1 V2 V3 VN 三相 4 線 R S T N 単相 2 線 R − − N 単相 3 線 R − T N 三相 3 線 R S T − 【参考】 • R/S/T/N は U/V/W/O や L1/L2/L3/N と表記されることがあります。 • R/N/T は U/O/W や L1/...