全 61 件が検索されました。(41 - 60件を表示)
- マニュアル
.... The communications cycle time depends on whether remote I/O communications are being used. Message Communications Only (Remote I/O Communications Not Used) Message communications time = 2 (see note) + 0.11 × TB + 0.6 (ms) TB: Baud rate (500 kbps: ...
- マニュアル
... FINS command code. The communications cycle time depends on whether remote I/O communications are being used. Message Communications Only (Remote I/O Communications Not Used) Message communications time = 2 (see note) + 0.11 × TB + 0.6 (ms) TB: Baud rate (500 kbps: ...
- マニュアル
... different types of Slave are given below. Output Slaves with 8 or Less Bytes of Output TRT = 0.016 × TB × SOUT1 + 0.11 × TB + 0.07 SOUT1 : The number of Output Slave output words TB : The baud rate factor (500 kbps: ...
- マニュアル
... are given below. Output Slaves with 8 or Less Bytes of Output TRT = 0.016 × TB × SOUT1 + 0.11 × TB + 0.07 (ms) SOUT1: TB: The number of Output Slave output words The baud rate factor (500 kbps: TB = 2...
- マニュアル
... determined by the number of target values specified in TB. The table can be between 4 and 145 words long, as shown below. 87 15 TB Direction1 0 No. of values2 TB+1 Lower word of target value 1 TB+2 Upper word of target value 1 TB+3 Interrupt task number for target value 1 TB+142 Lower word of target value 48 TB+143 Upper word of target value 48 TB+144 Interrupt task number for target value 48 0000 0000 to FFFF FFFF hex 0000 0000 to FFFF FFFF hex Interrupt Task Number 15 14 12 ...
- マニュアル
... can be between 4 and 145 words long, as shown below. 531 Section 3-20 High-speed Counter/Pulse Output Instructions 87 15 Direction1 TB 0 No. of values2 TB+1 Lower word of target value 1 TB+2 Upper word of target value 1 TB+3 Interrupt task number for target value 1 TB+142 Lower word of target value 48 TB+143 Upper word of target value 48 TB+144 Interrupt task number for target value 48 0000 0000 to FFFF FFFF hex 0000 0000 to FFFF FFFF hex Interrupt Task Number 15 14 12 11 87...
- マニュアル
...IR, SR, DM, HR, TC, LR R: Result word IR, AR, DM, HR, TC, LR When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of TB, TB+1, ...
- マニュアル
..., SR, DM, HR, TC, LR R: Result word IR, AR, DM, HR, TC, LR Description When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of TB, TB+1, ...
- マニュアル
...155 Section 4 Programming Instructions Result Bits and Ranges The following table shows the bits that are turned ON then the comparison value equals a value in channels TB through TB plus 15. TB Channel R BIT 00 TB + 1 ...
- マニュアル
...IR, SR, DM, HR, TC, LR R: Result word IR, AR, DM, HR, TC, LR Description When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of TB, TB+1, ...
- マニュアル
... the first value in the table and the process is repeated. The following diagram shows the structure of a target value comparison table for use with high-speed counter 0, or high-speed counters 1 or 2 in linear mode. TB TB+1 ...
- マニュアル
..., HR, TC, LR Limitations TB and TB+15 must be in the same data area. Description When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of TB, TB+1, ...
- マニュアル
... comparisons will not begin, and the INI(––) instruction must be used to begin comparisons. 107 Using Interrupts Section 5-5 The following diagram shows the structure of a target value comparison table for use with the high-speed counter. TB TB+1 ...
- マニュアル
... time: 3.5 [ms] Only when Slaves with input, output, or mixed I/O of more than 8 bytes exist. Explicit messages processing time: 0.11 × TB + 0.6 [ms] Explicit message communications execution time TB: Baud rate factor (500 kbps: ...
- マニュアル
...CIO, G, A, T, C, DM, DR, IR R Variations j TCMP(023) Description When the execution condition is OFF, TCMP(023) is not executed. When the execution condition is ON, TCMP(023) compares S to the content of TB, TB+1, ...
- マニュアル
... network that use at least 8 bytes for input, output, or both. Explicit Message Communications Time: 0.11 × TB + 0.6 [ms] Only added as delay time resulting from explicit message communications (send or receive). TB =The baud rate factor (500 kbps: ...
- マニュアル
... n [ms] The explicit message communications time is added as a delay time when explicit communications (sending or receiving) are performed. n= Number of explicit messages (both sending and receiving) that occur in one cycle time The baud rate factor TB = (500 kbps: ...
- マニュアル
... Processing Time: (0.11 × TB) × n [ms] Only added when explicit communications (transmission or reception) are performed. n: Number of explicit messages that occur at the same time during one CPU Unit cycle (including transmission and reception). TB = Baud rate factor (...
- マニュアル
..., TIM/CNT, LR Limitations DM 6144 to DM 6655 cannot be used for R. Description When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of TB, TB+1, ...
- マニュアル
... table is determined by the number of target values specified in TB. The table can be between 4 and 145 words long, as shown below. 0 15 TB Number of target values TB+1 Lower word of target value 1 TB+2...