全 61 件が検索されました。(21 - 40件を表示)

  • マニュアル

    ..., TIM/CNT, LR Limitations DM 6144 to DM 6655 cannot be used for R. Description When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of TB, TB+1, ...

  • マニュアル

    ...Only when Slaves with input, output or mixed I/O of more than 8 bytes exist. Explicit message communications time: 0.11 × TB + 0.6 [ms] Added as delay time when explicit message communications (send or receive) are used. TB: Constant (500 kbps: ...

  • マニュアル

    ... I/O Slave in the network with more than 8 bytes of I/O data. • Explicit message communications time: 0.11 × TB + 0.6 [ms] Added as a delay time when explicit message communications (send or receive) are used. TB: Constant (500 kbps: ...

  • マニュアル

    ...). TB: First comparison table word TB is the first word of the comparison table. The structure of the comparison table depends on the type of comparison being performed. 0 Number of target values TB+1 Lower word of target value 1 ...

  • マニュアル

    ...CP1E/CP2E CPU Unit Instructions Reference Manual(W483) 2 Instructions TB: First comparison table word 15 0 0001 to 6 hex (1 to 6 target values) Number of target values TB TB+1 Lower word of target value 1 ...

  • マニュアル

    ... of target values in the table, the target-value comparison table requires a continuous block of 4 to 145 words. 0 15 TB 1 to 48 (0001 to 0030 hex) Number of target values TB+1 Target value 1 (lower word) ...

  • マニュアル

    ... communications time is added as a delay time when explicit communications (sending or receiving) are performed. n= Number of explicit messages (both sending and receiving) that occur simultaneously within one CPU Unit task period of CPU Unit TB = The baud rate factor (500 kbit/s: ...

  • マニュアル

    ...NX-TBB122 12 None 10 A NX-TBB162 16 None 10 A NX-TBC082 8 Provided 10 A NX-TBC162 16 Provided 10 A Note When you purchase a terminal block, purchase an NX-TB£££2. A-100 NX-series EtherCAT Coupler Unit User’s Manual (W519) Appendices A-10 Functional Restrictions by Model The functions supported by EtherCAT Coupler Units depend the model number of the EtherCAT Coupler Unit. There are also functional restrictions depending on the unit version. Functional restrictions and support are given for each model in the following table. Function NX-ECC201 Supported. Cyclic I/O ...

  • マニュアル

    ... Unit are given. Refer to 4-1-2 Attaching Markers on page 4-5 for details on the marker attachment locations and 3-2 Indicators on page 3-13 for details on the indicators. Terminal Blocks There are two models of screwless clamping terminal blocks: NX-...

  • マニュアル

    ... on page 3-6 for details on indicators. 3-2 NX-series Analog I/O Units User’s Manual for Analog Input Units and Analog Output Units (W522) 3 Part Names and Functions Terminal Blocks There are two models of screwless clamping terminal blocks: NX-...

  • マニュアル

    ... details on the marker attachment locations and 3-1-2 Indicators on page 3-6 for details on the indicators. 3-2 NX-series System Units User's Manual (W523) 3 Part Names and Functions There are two models of screwless clamping terminal blocks: NX-...

  • マニュアル

    ... Position Interface Units User’s Manual (W524) 3-7 3 Part Names and Functions Before change 3-8 After change NX-series Position Interface Units User’s Manual (W524) 3 Part Names and Functions 3-3 Terminal Blocks • NX-...

  • マニュアル

    ...NX-TBA162 16 NX-TBB082 8 NX-TBB122 12 NX-TBB162 16 NX-TBC082 8 NX-TBC162 16 Not provided 4A 10 A Provided Note When you purchase a Terminal Block, purchase an NX-TB£££2. NX-series Data Reference Manual (W525) A-4 List of Screwless Clamping Terminal Block Models A-4 List of Screwless Clamping Terminal Block Models A-15 Appendices A-4-3 Applicable Screwless Clamping Terminal Blocks for Each Unit Model The following indicates the Screwless Clamping Terminal Blocks that are applicable to each Unit. Terminal Block Unit model number Model Number of terminals Ground terminal...

  • マニュアル

    ... Number of terminals Ground terminal mark Terminal current capacity NX-TBB162 16 None 10 A NX-TBC082 8 Provided 10 A NX-TBC162 16 Provided 10 A Note When you purchase a terminal block, purchase an NX-TB£££2...

  • マニュアル

    ... 4-22 for the calibration control number. 3-4 NX-series Analog I/O Units User’s Manual for Temperature Input Units and Heater Burnout Detection Units (W566) 3 Part Names and Functions Terminal Blocks There are two models of screwless clamping terminal blocks: NX-...

  • マニュアル

    .... NX-TBA161 Number of terminals 16 Ground terminal mark Not provided Terminal current capacity 4A NX-TBB161 NX-TBA162 10 A NX-TBB162 NX-TBC162 Provided Note When you purchase a terminal block, purchase an NX-...

  • マニュアル

    ... the terminal capacity of the NX-TBC082 is 10 A. Appendices Terminal block model NX-TBC162 Number of terminals 16 Ground terminal indication Provided Current capacity of terminals 10 A Note When you purchase a terminal block, purchase an NX-...

  • マニュアル

    ...). TB: First comparison table word TB is the first word of the comparison table. The structure of the comparison table depends on the type of comparison being performed. 0 Number of target values TB+1 Lower word of target value 1 ...

  • マニュアル

    ... the terminal capacity of the NX-TBC082 is 10 A. Appendices Terminal block model NX-TBC162 Number of terminals 16 Ground terminal indication Provided Current capacity of terminals 10 A Note When you purchase a terminal block, purchase an NX-...

  • マニュアル

    ...-2 Part Names and Functions Part Names and Functions 2-2 Safety Input Unit Possible in the upright installation orientation. • Connected to a Communications Coupler Unit 2-23 2 Specifications Terminal Blocks There are two models of screwless clamping terminal blocks: NX-...