全 80 件が検索されました。(41 - 60件を表示)

  • カタログ

    ...% FS ±1 digit max. Platinum resistance thermometer input: (±0.1% of PV or ±0.5°C, whichever is greater) ±1 digit max. Position-proportional potentiometer input: ±5% FS ±1 digit max. Control mode Standard control (heating or cooling control), heating/cooling control, standard control with remote ...

  • カタログ

    ...% FS ±1 digit max. Platinum resistance thermometer input: (±0.1% of PV or ±0.5°C, whichever is greater) ±1 digit max. Position-proportional potentiometer input: ±5% FS ±1 digit max. Control mode Standard control (heating or cooling control), heating/cooling control, standard control with remote ...

  • カタログ

    ...c ** c * ** c * ** c ** c AT実行/中止 オートチューニング at off cmwt off sp-0 0 sp-1 0 sp-2 0 sp-3 0 ins 0.0 insh 0.0 insl 下限温度入力補正値 0.0 * c * ** 現在値 25 :許可 :禁止 通信書込 許可・禁止 目標値0 目標値1 マルチSP で使用する目標値 目標値2 目標値3 1点...

  • カタログ

    ... the Unit can then be used during operation to switch between the set values. For models with built-in communications, communications can be used to switch between the set values. SV (3) Cycle time 2. SV 0 to 3 (sp-0, sp-1, ...

  • マニュアル

    ...mv-e ml-h ml-l mrl inf oc-h alh1 alh2 alh3 insh insl AT実行/停止目標値0 A SV SV at sp-0 sp-1 sp-2 sp-3 al-1 al-2 al-3 p i d c-sc c-db db of-r hys chys cp c-cp ct hb 1秒以上 マニュアル動作 (PID制御時のみ有効) メニュー画面に移行 PV menu sub1 PV 1 秒以上 AT開始/停止...

  • マニュアル

    ... :SP lower limit +1 to upper limit of sensor setting range *2 Temperature :Lower limit of sensor setting range to SP upper limit - 1 *3 1/4 input :Standard (0) / heating or cooling (1) Standard (0) / heating or cooling (1) Standard with remote ...

  • マニュアル

    ... move to the communication setting level. Display Set value/monitor value m-sp ct1 ct2 lcr1 lcr2 cmwt ct1 ct2 lcr1 lcr2 hb1 hb2 hs1 hs2 sp-0 sp-1 sp-2 0 to 3 0.0 to 55.0 0.0 to 55.0 0.0 to 55.0 0.0 to 55.0 ON, OFF 0.0 to 55.0 0.0 to 55.0 0.0 to 55.0 0.0 to 55.0 0.0 to 50.0 0.0 to 50.0 0.0 to 50.0 0.0 to 50.0 Set point ...

  • マニュアル

    ...sp-0 Limite inferiore del valore di impostazione a limite superiore del valore di impostazione 0 Punto di impostazione 1 EU sp-1 Limite inferiore del valore di impostazione a limite superiore del valore di impostazione 0 Punto di impostazione 2 EU ...

  • マニュアル

    ...1A 䆒ᅮ⚍1ǂ 䆒ᅮ⚍ϟ䰤㟇䆒ᅮ⚍Ϟ䰤 sp-1 0 EU ᔧ⬉⌕ؐᇣѢ1AᯊˈẔ⌟ࡳ㛑ϡৃ䴴DŽ 䆒ᅮ⚍2ǂ 䆒ᅮ⚍ϟ䰤㟇䆒ᅮ⚍Ϟ䰤 0 sp-2 EU ࡴ⛁఼Ꮉ԰⬉⌕ㄝѢ៪㗙໻Ѣ10.0Aᯊ˖ℷᐌⱘࡴ⛁఼⬉⌕ؐˉࡴ⛁఼ᮁ㒓⬉⌕ؐ㻢2.5A 䆒ᅮ⚍3ǂ 䆒ᅮ⚍ϟ䰤㟇䆒ᅮ⚍Ϟ䰤 sp-3 EU 0 ᔧ⬉⌕ؐᇣѢ2.5AᯊˈẔ⌟ࡳ㛑ϡৃ䴴DŽ NA 0㟇2 Փ⫼໮䏃SPⱘϾ᭄ǂ ...

  • マニュアル

    ... alarm use HS alarm latch HS alarm hysteresis Heater Overcurrent Use Heater Overcurrent Latch Heater Overcurrent Hysteresis Display m-sp ct1 lcr1 cmwt ct1 hb1 oc1 lcr1 hs1 sp-0 sp-1 sp-2 sp-3 ev-m ev-1 ev-2 psel u-no bps len sbit prty sdwt mspu hbu hbl hbh hsu hsl hsh ocu ocl och Set value/monitor value 0 to 3 0.0 to 55.0 0.0 to 55.0 ON, OFF 0.0 to 55.0 0.0 to 50.0 0.0 to 55.0 0.0 to 55.0...

  • マニュアル

    ...加热器过流使用加热器过流闩锁加热器过流滞后 显示 m-sp ct1 lcr1 cmwt ct1 hb1 oc1 lcr1 hs1 sp-0 sp-1 sp-2 sp-3 ev-m ev-1 ev-2 psel u-no bps len sbit prty sdwt mspu hbu hbl hbh hsu hsl hsh ocu ocl och 设定值/监视值 0至3 0.0至55.0 0.0至55.0 ON、OFF 0.0至55.0 0.0至50.0 0.0至55....

  • マニュアル

    ... rise rate program, parameters are set to two steps as shown in the figure above. The following figure shows the relationship between the program and parameters. Target SP 1 Soak time 0 Soak time 1 Soak time 2 Target SP 0 Target ...

  • マニュアル

    ... rise rate program, parameters are set to two steps as shown in the figure above. The following figure shows the relationship between the program and parameters. Target SP 1 Soak time 0 Soak time 1 Soak time 2 Target SP 0 Target ...

  • マニュアル

    ... rate program, parameters are set to two steps as shown in the figure above. The following figure shows the relationship between the program and parameters. Target SP 1 Soak time 0 Soak time 1 Soak time 2 Target SP 0 Target ...

  • マニュアル

    ... input Event input Event input 1 Event input 2 Multi-SP assignment 1 assignment 2 function function Uses 0 NONE or STOP 1” NONE or RUN/STOP switching 1” NONE or 1 – (not disNONE or Multi–SP 2 set played) STOP points (set point 0/1 RUN/STOP switching switching) 2 – (not displayed) Multi–SP 4 set points (set point 0/1/2/3 switching) Note E5CN 11 12 EV1 EV2 13 4-5-2 “STOP (RUN/STOP) switching” can be set only on one of event input assignments 1 or 2. The event input on the side that ...

  • マニュアル

    ..." Comment Number of MultiĆSP Uses Setting Event input assignment 1 0 Event Input Function Event input assignment 2 Event input 1 function NONE or STOP 1" NONE or RUN/STOP switching 1" Multi-SP 2 set points 1 - (not displayed) NONE or STOP (set point 0/1 switchĆ ing) 2 NONE or RUN/STOP switching Multi-SP 4 set points - (not displayed) *1 Event input 2 function (set point 0/1/2/3 switching) STOP (RUN/STOP) switching" can be set only on one of event input assignments 1 or 2. The event input on the side that is ...

  • マニュアル

    ... 1 0 1 Event Input Function Event input assignment 2 NONE or STOP 1” – (not displayed) 2 Event input 1 function Event input 2 function NONE or RUN/STOP switching 1” NONE or STOP Multi–SP 2 set points NONE or (set point 0/1 switch- RUN/STOP switching) ing Multi–SP 4 set points (set point 0/1/2/3 switching) – (not displayed) *1 “STOP (RUN/STOP) switching” can be set only on one of event input assignments 1 or 2. The event input on the side that is set can be used. The setting on the other ...

  • マニュアル

    ... can be achieved by setting the “standby sequence,” “alarm hysteresis,” and “close in alarm/ open in alarm” parameters. Optimum PID constants can be set easily by autotuning. • The following functions can be achieved using the event input (one input per Temperature Controller): SP selection (multi-...

  • マニュアル

    ....) 1.) 1 (Not displayed.) 2 (Not displayed.) Note Event inputs Function of event Function of event input 1 input 2 None, or switching RUN/STOP, switching auto/manual, or starting/resetting program NONE, STOP, MANU, Multi-...

  • マニュアル

    ....) 1.) 1 (Not displayed.) 2 (Not displayed.) Note Event inputs Function of event Function of event input 1 input 2 None, or switching RUN/STOP, switching auto/manual, or starting/resetting program NONE, STOP, MANU, Multi-...