全 80 件が検索されました。(21 - 40件を表示)
- マニュアル
... can be achieved by setting the “standby sequence,” “alarm hysteresis,” and “close in alarm/ open in alarm” parameters. Optimum PID constants can be set easily by autotuning. • The following functions can be achieved using the event input (one input per Temperature Controller): SP selection (multi-...
- マニュアル
...Detection 2 Heater Overcurrent Detection 2 Leakage Current 1 Monitor HS Alarm 1 Leakage Current 2 Monitor HS Alarm 2 Heater Burnout Detection 1 Heater Burnout Detection 2 SP 0 SP 1 sp-1 SP 2 sp-2 SP 3 sp-3 at Display Default Unit off, at-2, at-1 OFF None cmwt OFF: AT Cancel AT-2: 100%AT Execute AT-1: 40%AT Execute (See note 3.) OFF, ON off, on OFF None irdr OFF, ON off, on OFF None spmd ct1 LSP, RSP 0.0 to 55.0 lsp, rsp LSP None A hb1 0.0 ...
- マニュアル
... number switching bits 0 to 2 and the set point. Selected set point Multi-SP No. switching bits Bit 0 Bit 1 Bit 2 SP 0 OFF OFF OFF SP 1 ON OFF OFF SP 2 OFF ON OFF SP 3 ON ON OFF SP 4 OFF OFF ON SP 5 ON OFF ON SP 6 OFF ON ON SP 7 ON ON ON Note: Any bits that are not assigned to event inputs are treated as being OFF. Using Key Operations You can select any of the set points 0 to 7 by changing the set value ...
- マニュアル
... 1 Alarm Value 2 Alarm Value Upper Limit 2 Alarm Value Lower Limit 2 Alarm Value 3 Alarm Value Upper Limit 3 Alarm Value Lower Limit 3 Heater Burnout Detection 1 SP 0 SP 1 SP 2 SP 3 Process Value Input Shift PV Input Slope Coefficient Proportional Band Setting (monitor) value Level Protect H'00000000 (0): No restrictions in operation and adjustment levels H'00000001 (1): Move to adjustment level is prohibited. H'00000002 (2): Display and change of only "PV" and "PV/SP" parameters is allowed. H'00000003 (3): Display of only "PV" and "PV/SP" parameters ...
- マニュアル
... to 7) H'00000001 to H'00000020 (32) 0002 Segments Used*1 Segment H'00000000 to H'0000001F (31) Level Program setting *1 Selection C4 (84) 0003 Segment Format*2 C4 (84) 0004 Segment SP*2 H'00000000 (0): Ramp H'00000001 (1): Soak H'00000002 (2): Step SP Lower Limit to SP Upper Limit C4 (84) 0005 Segment Slope*2 H'00000000 to H'0000270F (0 to 9999) C4 (84) 0006 Segment Time*2 C4 (84) 0007 PID Set No.*1 C4 (84) 0008 C4 (84) 0009 Alarm Value 1*1 Alarm Value Upper H'00000000 to H'...
- マニュアル
... by using external input signals (event inputs). 5 Using Event Inputs Multi-SP No. switching bits Bit 0 Bit 1 Bit 2 SP 0 OFF OFF OFF SP 1 ON OFF OFF SP 2 OFF ON OFF SP 3 ON ON OFF SP 4 OFF OFF ON SP 5 ON OFF ON SP 6 OFF ON ON SP 7 ON ON ON Note: Any bits that are not assigned to event inputs are treated as being OFF. E5@D Digital Temperature Controllers User’s Manual (H224) 5 - 33 5-8-1 Event Input Settings The following table shows ...
- マニュアル
... 1 Alarm Value 2 Alarm Value Upper Limit 2 Alarm Value Lower Limit 2 Alarm Value 3 Alarm Value Upper Limit 3 Alarm Value Lower Limit 3 Heater Burnout Detection 1 SP 0 SP 1 SP 2 SP 3 Process Value Input Shift PV Input Slope Coefficient Proportional Band Setting (monitor) value Level Protect H'00000000 (0): No restrictions in operation and adjustment levels H'00000001 (1): Move to adjustment level is prohibited. H'00000002 (2): Display and change of only "PV" and "PV/SP" parameters is allowed. H'00000003 (3): Display of only "PV" and "PV/SP" parameters ...
- マニュアル
...The PV on the No. 1 display in the PV, PV/SP, PV/Manual MV, or PV/SP Manual MV Display and the control or alarm status specified for the PV status display function are alternately displayed in 0.5-s cycles.*1 • PV • PV/...
- マニュアル
...を行ってください。 46 Sysmac Library ユーザーズマニュアル 温度制御ライブラリ編 (SBCA-429) TempUniformityFilter 変数入力変数 Enable RefPointIndex*1 SP*2 名称動作指令 データ型 BOOL 初期値 FALSE 有効範囲 FALSE/TRUE リファレンス UINT ポイント指定 0 0∼9 目標値 0 ARRAY[1..9] OF REAL 単位 ― ― -3200.00 ∼ +3200.00 ― PV*2 FilterGain*...
- マニュアル
...プンにします。 rSP2、3、6、7 ......伝送路選択ピン(ショートプラグ使用) BSD(バックSD) 対上流用 NRD (ノーマルRD) SP 6 SP 2 SP 7 SP 3 NSD(ノーマルSD) BRD (バックRD) 対下流用 2C 1 2-C間ショートで光ファイバ使用電源供給ピンの設定と合わせて行ってくだ...
- マニュアル
...i ソーク時間 1 6-28 M 1.000 力傾き補正係数 p 調節感度 1.0 (冷却) soak w1of M M M 0 sp-2 6-25 M M sp-1 PV 入力傾き 1.000 補正係数 Rrss 6-28 M M M sp-0 6-25 M M hs2 PV 入力補正値 0.0 inrt 調節感度 1.0 (加熱) chys 参照ページ M M M M lcr2 6-24 M M hs1 目...
- マニュアル
...水冷用比例帯 0.6 減少閾値 233 0 sp-4 M 8.0 M sp-3 水冷用比例帯 1.4 増大閾値 40 M sp-2 M d 目標値 1 水冷出力調整 off 機能 233 M sp-1 M i M PID 更新 off (適応制御) p M sp-0 a-ud w-dl M hs1 M w-il 6-18 入力デジタル 0.0 フィルタ w-ht 6-17 M...
- マニュアル
... use this library, implement safety measures, such as monitoring for excessive temperature rise and fall, outside of the function or function block. 46 Sysmac Library User’s Manual for Temperature Control Library (W551) TempUniformityFilter Variables Input Variables Meaning Enable RefPointIndex*1 ...
- カタログ
...ト下限値 -200 M al2l 警報下限値2 0 M prst プログラムスタート 0.0 マルチSPで使用 M する目標値 sp-2 目標値2 漏れ電流値1モニタ 0.0 1.0 0.0 ° c 0 M soak ソーク時間 M lcr2 漏れ電流値2モニタ ° c 0.0 M ヒステリシス設定 chys 調節感度(冷却)...
- カタログ
....0 M hs2 C M soak Soak Time Leakage Current 2 Monitor HS Alarm 2 1 M wt-b C off M sp-0 M mv-s SP 0 M sp-2 MV at Stop M Current 2 lcr2 Leakage Monitor MV at PV Error SP used by multi-SP SP 2 M sp-3 SP 3 C M sprt SP Ramp Set Value off M ol-h 0 105.0 M M ol-l MV Upper Limit MV Lower Limit M orl MV Change Rate Limit 0.0 M sqrp 0.0 M C Extraction of Square Root...
- カタログ
...0.0 M 132 M al2h 警報上限値2 0 M prst プログラムスタート 0.0 マルチSPで使用 M する目標値 sp-2 目標値2 漏れ電流値1モニタ 0.0 1.0 0.0 ° c 0 M soak ソーク時間 M lcr2 漏れ電流値2モニタ ° c 0.0 M ヒステリシス設定 chys 調節感度(冷却) 50....
- カタログ
...al-3 警報値3 M 0.0 ° c M s-hc 0.0 M mv-e 異常時操作量 マルチSPで使用 M する目標値 sp-2 目標値2 onof 0.0 M off ° c 0 0 ° c 50.0 M cntl PID・ON/OFF 0 1.0 0.0 ° c ° c M soak ソーク時間 M lcr2 漏れ電流値2モニタ ° c 目標値の制限 M sl-l 目標値リミッ...
- カタログ
...lcr1 ヒステリシス設定 mv-s ストップ時操作量 50.0 M C hys 調節感度(加熱) off M hs2 SSR故障検出2 sp-2 ct2 ヒータ電流値2モニタ al2h 警報上限値2 0 M 0.0 M 1 M 50.0 M 目標値2 C 0.0 M soak ソーク時間 0.0 M 0 M ct1 ヒータ電流値1モニタ sp-...
- カタログ
...% FS ±1 digit max. Platinum resistance thermometer input: (±0.1% of PV or ±0.5°C, whichever is greater) ±1 digit max. Position-proportional potentiometer input: ±5% FS ±1 digit max. Control mode Standard control (heating or cooling control), heating/cooling control, standard control with remote ...
- カタログ
...% FS ±1 digit max. Platinum resistance thermometer input: (±0.1% of PV or ±0.5°C, whichever is greater) ±1 digit max. Position-proportional potentiometer input: ±5% FS ±1 digit max. Control mode Standard control (heating or cooling control), heating/cooling control, standard control with remote ...