全 44 件が検索されました。(41 - 44件を表示)

  • マニュアル

    ... when the PLC is turned ON or the Thermocouple Input Unit is restarted. m + 34 m + 49 m + 64 m + 79 0 to 8 0000 to 0008 hex 3 (0003 hex) Sensor type 0: B, 1: E, 2: J, 3: K, 4: N, 5: R, 6: S, 7: T, 8: mV m + 35 m + 50 m + 65 m + 80 –32000 to 32000 8300 to FFFF hex, 0000 to 7D00 hex 4000 (0FA0 hex) Maximum input signal value (set value x 0.1°C/°F or mV) m + 36 m + 51 m + 66 m + 81 –32000 to 32000 8300 to ...

  • マニュアル

    ...2 s+2 : : s+3 OUT block 1 15 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable : k+4 00 Not usable 01 01 Not usable 01 02 k+5 l: First word of the allocation size setup table s: First word of OUT block 1 k: First word of IN block 1 Note 00 IN block 1 00 Not usable : 00 : 02 : 1. The numbers in the OUT 1 and IN 1 blocks represent node addresses. 2. Bytes are allocated in order in the blocks in word units in ...

  • マニュアル

    ... one of the cursor control keys, the system will display on the screen the name of the key you pressed and end execution of the program. 100 K=KEYIN 110 IF K=1 THEN GOTO 200 120 IF K=2 THEN GOTO 300 130 IF ...

  • マニュアル

    ... A<=HI THEN PRINT ”OK” ELSE PRINT ”NG” GOTO 10030 Example 2 10000 ’Display the criteria set with the menu. 10010 K$(0)=”Area” 10020 K$(1)=”X grav cent” 10030 K$(2)=”Y grav cent” 10040 K$(3)=”Axis angle” 10050 ...