全 44 件が検索されました。(21 - 40件を表示)

  • マニュアル

    ...0 Bit Screen No. (4-digit BCD or hexadecimal) k k+1 X coordinate (4-digit BCD or hexadecimal) k+2 Y coordinate (4-digit BCD or hexadecimal) k+3 Screen No. (4-digit BCD or hexadecimal) k+4 X coordinate (4-digit BCD or hexadecimal) k+5 Y coordinate (4-digit BCD or hexadecimal) k+6 Screen No. (4-digit BCD or hexadecimal) k+7 X coordinate (4-digit BCD or hexadecimal) k+8 Y coordinate (4-digit BCD or hexadecimal) Global window Local Window1 Local Window2 Reference: It is not necessary to allocate words in the host for ...

  • マニュアル

    ..., and k+6 can then be designated individually to set the counter value as required. PC Word Application Example 1: Transferring Range Parameters Contents k FF k+1 and k+2 Counter value 1 k+3 FF k+4 and k+5 Counter value 2 k+6 FF k+7 and k+8 Counter value 3 k+9 through k+11 Ignored The following example shows use of TRANSFER DATA to transfer the upper limit, lower limit, and output pattern for three ranges. The system configuration consists of a Counter Unit (unit #0) on a C200H PC and an ...

  • マニュアル

    ... when the PLC is turned ON or the Thermocouple Input Unit is restarted. m + 34 m + 49 m + 64 m + 79 0 to 8 0000 to 0008 hex 3 (0003 hex) Sensor type 0: B, 1: E, 2: J, 3: K, 4: N, 5: R, 6: S, 7: T, 8: mV m + 35 m + 50 m + 65 m + 80 –32000 to 32000 8300 to FFFF hex, 0000 to 7D00 hex 4000 (0FA0 hex) Maximum input signal value (set value x 0.1°C/°F or mV) m + 36 m + 51 m + 66 m + 81 –32000 to 32000 8300 to ...

  • マニュアル

    ...2 s+2 : : s+3 OUT block 1 15 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable : k+4 00 Not usable 01 01 Not usable 01 02 k+5 l: First word of the allocation size setup table s: First word of OUT block 1 k: First word of IN block 1 Note 00 IN block 1 00 Not usable : 00 : 02 : 1. The numbers in the OUT 1 and IN 1 blocks represent node addresses. 2. Bytes are allocated in order in the blocks in word units in ...

  • マニュアル

    ... CJ-series Unit Variable name Description aaaa[0] Range 0 k, k+1 00 to 15 aaaa[0].LowLmt Lower Limit Range 0 k+2, k+3 00 to 15 aaaa[0].UpLmt Upper Limit Range 0 k+4, k+5 00 to 15 aaaa[0].OutPat Output Pattern Range 0 k+6 to k+11 00 to 15 aaaa[1] Range 1 k+12 to k+17 00 to 15 aaaa[2] Range 2 k+18 to k+23 00 to 15 aaaa[3] Range 3 k+24 to k+29 00 to 15 aaaa[4] Range 4...

  • マニュアル

    ...IN block 1 15 00 00 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable Not usable : 00 : k+4 Not usable 01 01 Not usable 01 02 k+5 l: First word in allocation size setup table s: First word in OUT block 1 k: First word in IN block 1 00 : 02 : Note 1 The numbers in the OUT 1 and IN 1 blocks represent node addresses. 2 Bytes are allocated in the blocks in word units in the order of node addresses. If the allocated size is 1 ...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-5 K-4 Camera Settings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-6 K-5 White Balance Settings (QSXGA Color Only) . . . . . . . . . . . . . . . . . . . . . . . . K-7 K-6 Color Filter . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-8 K-7 Focus Setup . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-9 K-8 Illumination Brightness . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-10 K-9 Morphological Pre-Processing . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-12 K-10 Morphological Operation and Operator Size . . . . . . . . . . . . . . . . . . . . . . K-13 K-11 Damaged Symbol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-15 K-12 Linear Security Level . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-16 K-13 Advanced Decoding Parameters . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-16 MicroHAWK V320-F / V330-F / V420-F / V430-F Barcode Reader User Manual K-1 Appendices K-1 Camera and IP Setup Serial Commands Window of Interest...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-5 K-4 Camera Settings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-6 K-5 Illumination . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-7 K-6 Morphological Pre-Processing . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-8 K-7 Morphological Operation and Operator Size . . . . . . . . . . . . . . . . . . . . . . . . K-9 K-8 1D Damaged Symbol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-11 K-9 Linear Security Level . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-12 K-10 Fast Linear Mode . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K-13 V440-F C-Mount Code Reader User Manual K-1 Appendices K-1 Camera and IP Setup Serial Commands Window of Interest 1D Damaged Symbol ...

  • カタログ

    ...電機、 富士電機キーエンス 回路 回 路 パターン A 回 路 パターン B 標準価格 形式 I /O 点数 (¥) X W 2 K- 4 0 G - O 3 2 A 32 点 入出力兼 用 入出力兼 用 X W 2 K- 4 0 G - O 3 2 C 3,800 X W 2 K- 4 0 G - M 3 2 3,800 X W 2 ...

  • マニュアル

    ...: 0.1 Hz (less than 100 Hz) and 1 Hz (100 Hz or over) Analog commands: 0.06 Hz/60 Hz (equivalent to 1/1000) 0.01 Hz 150% of rated output current for 1 min Selectable with FREQ adjuster: 0 to 10 V DC (20 ...

  • マニュアル

    ....1 Hz (less than 100 Hz) and 1 Hz (100 Hz or over) Analog commands: 0.06 Hz/60 Hz (equivalent to 1/1000) 0.01 Hz 150% of rated output current for 1 min Selectable with FREQ adjuster: 0 to 10 V DC (20 kΩ), 4...

  • マニュアル

    ...置データアドレス 4 k+1 位置データ (上位) k+2 位置データ (下位) k+3 速度アドレス Mコード k+4 ドゥエルタイムアドレス 加減速パターン k+5 属性 位置データアドレス 4 k+6 位置データ (上位) k+7 位置データ (下位) k+8 位置決めパター...

  • マニュアル

    ...トから本ユニットに転送されるパラメータ ●センサ種類 m+34 m+49 m+64 m+79 0∼8 0000∼0008 Hex 3 0:B、1:E、2:J、3:K、4:N、5:R、 (0003 Hex) 6:S、7:T、8:mV ●測定値の入力レンジ設定 m+35 m+50 m+65 m+80 -32000∼ 8300∼FFFF Hex、 4000 入力信号最大値(設定値×0.1℃/°F または +32000 0000∼...

  • マニュアル

    ...15 INブロック1 00 k 00 00 01 01 k+1 00 00 01 01 k+2 (使用不可) 00 02 k+3 01 : k+4 (使用不可) 01 k+5 02 02 : : : l:割付サイズ設定テーブルの先頭チャネル番号 s:OUTブロック1先頭チャネル番号 k:INブロック1先頭チャネル番号 01 00 注:・OUT1/IN1 ブロッ...

  • マニュアル

    ... Each Mode Changes the measurement conditions, discrimination values, communication conditions and option when the code in the table is received. 【 e.g.1】 】 Header: STX, Footer: ETX (STX)(A)(2)(ETX) 【 e.g.2】 】 Header: none, Footer: CR Bar position measurement mode (...

  • マニュアル

    ...ードに設定する場合 :な し 、 フッタ :C R で 、 【 例 2 】ヘ ッ ダ 、丸棒位置測定モードに設定する場合ダ: 、フタ: 3 (K)(4)(CR) 章 各コード受信時、正常の設定変更ができた場合は、 「OK」を送信した直後から新しい設定条件が有効になります。 設定変更できなか...

  • マニュアル

    ...0 Bit Screen No. (4-digit BCD or hexadecimal) k k+1 X coordinate (4-digit BCD or hexadecimal) k+2 Y coordinate (4-digit BCD or hexadecimal) k+3 Screen No. (4-digit BCD or hexadecimal) k+4 X coordinate (4-digit BCD or hexadecimal) k+5 Y coordinate (4-digit BCD or hexadecimal) k+6 Screen No. (4-digit BCD or hexadecimal) k+7 X coordinate (4-digit BCD or hexadecimal) k+8 Y coordinate (4-digit BCD or hexadecimal) Global window Local Window1 Local Window2 Reference: It is not necessary to allocate word to window control area ...

  • マニュアル

    ...0 Bit Screen No. (4-digit BCD or hexadecimal) k k+1 X coordinate (4-digit BCD or hexadecimal) k+2 Y coordinate (4-digit BCD or hexadecimal) k+3 Screen No. (4-digit BCD or hexadecimal) k+4 X coordinate (4-digit BCD or hexadecimal) k+5 Y coordinate (4-digit BCD or hexadecimal) k+6 Screen No. (4-digit BCD or hexadecimal) k+7 X coordinate (4-digit BCD or hexadecimal) k+8 Y coordinate (4-digit BCD or hexadecimal) Global window Local Window1 Local Window2 Reference: It is not necessary to allocate words in the host for ...

  • マニュアル

    .... b15-b12 b11-b8 k 1 0 0 4 k+1 0 0 0 1 k+2 0 0 0 0 k+3 0 2 1 0 k+4 1 5 0 4 k+5 1 0 2 4 k+6 0 0 0 0 k+7 0 0 0 0 k+8 0 1 3 0 k+9 1 5 4 4 k+10 1 0 3 4 k+11 0 0 0 1 k+12 0 0 0 0 k+13 0 2 0 0 k+14 0 0 C 6 k+15 1 0 4 4...

  • マニュアル

    ..., and k+6 can then be designated individually to set the counter value as required. PC Word Application Example 1: Transferring Range Parameters Contents k FF k+1 and k+2 Counter value 1 k+3 FF k+4 and k+5 Counter value 2 k+6 FF k+7 and k+8 Counter value 3 k+9 through k+11 Ignored The following example shows use of TRANSFER DATA to transfer the upper limit, lower limit, and output pattern for three ranges. The system configuration consists of a Counter Unit (unit #0) on a C200H PC and an ...