全 113 件が検索されました。(41 - 60件を表示)
- 推奨代替品ガイド
...ソール 形E3X-MC11-SV2が使用できません。 4) 通信ユニット 形E3X-DRT21-S VER.3が使用できません。 形E3X-HD0のみ通信ユニット 形E3X-CRT、形E3X-ECTとの組み合わせで使用できます。 形E3NX-FA0は通信ユニット 形E3X-CRT...
- 商品情報
...ニット:形3G3AX-RX-CRT-Eに対応しました。 - :CX-Oneオートアップデート(V4向け_2012年2月) 新規機能 CompoNet用スレーブデバイス:E3X-CRTに対応しました。 - :CX-Oneオートアップデート(V4向け_2011年11月) 新規機能 MX2シリーズインバータ用 CompoNet通信ユニット:形3G3AX-MX2-CRT-...
- 推奨代替品ガイド
...-FAシリーズはモバイルコンソール 形E3X-MC11-SV2が使用できません。 10)形E3NX-FAシリーズは通信ユニット 形E3X-DRT21-S VER.3、形E3X-CRT、形E3X-ECTが使用できません。 形E3NX-CAシリーズに代替する場合、以下の点をご注意ください。 1)形E3X-DAB(青)、形E3X-DAG(緑)の単...
- 商品情報
...ージ先頭へ戻る CompoNet DTM の更新内容 - :CX-Oneオートアップデート(V3向け_2012年2月) 新規機能 CompoNet用スレーブデバイス:E3X-CRTに対応しました。 - :CX-Oneオートアップデート(V3向け_2011年11月) 新規機能 MX2シリーズインバータ用 CompoNet通信ユニット:形3G3AX-MX2-CRT-E...
- 推奨代替品ガイド
...機能を搭載しています。 3. モバイルコンソール形E3X-MC11-SV2は使用出来ません。 4. 通信ユニット形E3X-DRT21-S VER.3、形E3X-CRT、形E3X-ECT、形E3NWは使用できません。 5. 制御出力の負荷電流が異なります。 詳細は定格/性能をご確認ください。 6. 形E3NCシリーズお...
- 生産終了品/推奨代替品
...-G E3S-GS / VS E3S-LS E3S-LS3C1D / LS3RC4 E3S-LS5 E3S-X, E32-TA50 / DA50 E3S-X2 E3S-X3 E3SA E3S(旧タイプ) E3V E3V3 E3W E3W2 E3X-A / H / F / VG E3X-CRT E3X-DA-N E3X-DA-S E3X-DA-S / MDA E3X-DAC-S E3X-DRT21 / SRT21 / CIF11 E3X-DRT21-S VER.3 E3X-ECT E3X-NH E3X-NL E3X-NT / NM / NV / NVG E3X-SD E3XA E3XR E3XR-CGE4 E3XR-GM E3Y E3Z(イージーオーダータイプ) E4A-3K E4B E4C E4C-UDA E4DA E4E...
- 商品情報
...通信ユニット - 商品カテゴリ | オムロン制御機器 センサ通信ユニット センサをCompoNetにつなげる通信ゲートウェイ E3X-CRT センサ通信ユニット,ZS-CRT センサ通信ユニット Home > 商品情報 > 商品カテゴリ > FAシステム機器 > ネットワーク機器 > CompoNet > センサ通...
- 技術解説/使用上の注意事項
...、 形E3NW-ECT(EtherCAT)、形E3NW-CRT(CompoNet)、 形E3NW-CCL(CC-Link)とお使いいただけます。 形E3X-HDシリーズは形E3X-HD0をお使いいただきますと、 形E3X-CRT(CompoNet)もしくは形E3X-ECT(EtherCAT)とお使いいただけます。 *2 ファイバアンプ コントロー ル ねじ型や円柱型の取りつけ穴はどれぐら...
- 商品情報
... containing previous versions of Slice IO Coupler DTM cannot display the DTM views in CX-ConfiguratorFDT. ページ先頭へ戻る Change history of CompoNet DTM - :CX-One Version 3 Auto-update (February 2012) New functions Support the CompoNet Slave device of ...
- 生産終了品/推奨代替品
...-G E3S-GS / VS E3S-LS E3S-LS3C1D / LS3RC4 E3S-LS5 E3S-X, E32-TA50 / DA50 E3S-X2 E3S-X3 E3SA E3S(旧タイプ) E3V E3V3 E3W E3W2 E3X-A / H / F / VG E3X-CRT E3X-DA-N E3X-DA-S E3X-DA-S / MDA E3X-DAC-S E3X-DRT21 / SRT21 / CIF11 E3X-DRT21-S VER.3 E3X-ECT E3X-NH E3X-NL E3X-NT / NM / NV / NVG E3X-SD E3XA E3XR E3XR-CGE4 E3XR-GM E3Y E3Z(イージーオーダータイプ) E4A-3K E4B E4C E4C-UDA E4DA E4E...
- カタログ/マニュアル訂正
...D4NH 1627 E2K-L 778 E3S-LS3□ 358 D4NL 1568 E2K-X 768 E3T D4NS 1605 E2KQ-X 782 D4NS-SK 1605 E2MP D4NS-SK□ 1607 E2S 676 E3X-CRT D4SL-CN□ 1532 E2SS 798 E3X-DA-S D4SL-N 1528 E2V 642 E3X-DA-S/MDA D4SL-NK□ 1532 E32-□ 12 E3X-DA0-S 152、154 D4SL-NSK10-LK□ 1528 E32-A□ 36、42、52、56、60、62 E3X-DAC-S 136 1533、1555 E32-C□ 16、26、28、40 E3X-DAT□-S 160 16、28 E3X-DRT21-S 156 D4GL-SK10-LK□ D4SL-SK10H D5A 1241 D5B 1251...
- 商品情報
...きますと、 形E3NW-ECT(EtherCAT)、形E3NW-CRT(CompoNet)、 形E3NW-CCL(CC-Link)とお使いいただけます。 形E3X-HDシリーズは形E3X-HD0をお使いいただきますと、 形E3X-CRT(CompoNet)もしくは形E3X-ECT(EtherCAT)と お使いいただけます。*2 *1. 形E3X-DA-Sは2017年3月に受注終了しました。形E3X-MDAは2021年8月に...
...E2M*/E2NC-*/E2Q*/E2S*/E2V-* E32-* E39-* E3C-* E3AS-*/E3D-*/E3F*/E3G-*/ E3H*/E3J*/E3K-*/E3L-*/E3M*/E3N-* E3NC-LA*/LH*/-SA*/ -SH* E3NW-* E3NX-* E3R-*/E3RA-*/E3RB-*/E3S-*/ E3T-*/E3V*/E3X-A* E3X-CIF11 E3X-CN* ...
- カタログ
... doing so may cause malfunction. • It may take time until the measurement value become stable immediately after the power is turned on depending on use environment. • The Mobile Console E3X-MC11, E3X-MC11-SV2 and E3XMC11S cannot be connected. • The Communication Unit E3X-DRT21-S, ...
- カタログ
... receives excessive sensor light, the mutual interference prevention function may not work properly, resulting in malfunction of the unit. In such case, increase the threshold. (12) The E3NW-ECT Sensor Communications Unit can be used with the E3NX-FA0, but the E3X-DRT21-S, ...
- カタログ
... used. It may be damaged if connected. 13.If the unit receives excessive sensor light, the mutual interference prevention function may not work properly, resulting in malfunction of the unit. In such case, increase the threshold. 14.The Communication Unit E3X-DRT21-S, ...
- カタログ
.... 11.If the unit receives excessive sensor light, the mutual interference prevention function may not work properly, resulting in malfunction of the unit. In such case, increase the threshold. 12.Standard models (E3NC-@A21/51/7/9) The Sensor Communications Unit E3X-DRT21-S, ...
- カタログ
...-Link only.) 12.If the unit receives excessive sensor light, the mutual interference prevention function may not work properly, resulting in malfunction of the unit. In such case, increase the threshold. 13.Standard models and Advanced models The Sensor Communication Unit E3X-DRT21-S, ...
- カタログ
... not work when in combination with E3C/E2C/E3X. 12. Excessive incident light cannot be sufficiently handled by the mutual interference prevention function and may cause malfunction. To prevent this, set a higher threshold level. 13. The Communication Unit E3X-DRT21-S, ...
- カタログ
...OMRON NJ-series Unit) --- High-speed Mode (HS) 10 Units Standard Mode (Stnd) 10 Units Giga-power Mode (GIGA) 10 Units *1. The E3NW-ECT Sensor Communications Unit can be used, but the E3NW-CRT/CCL, E3X-DRT21-S, and ...