全 44 件が検索されました。(41 - 44件を表示)
- マニュアル
... ms max. (excluding the input ON/OFF delays). When a Communications Unit is used with the C200HS-CPU31-E/CPU33-E CPU, the interrupt response time is 10 ms max. Input Interrupts Up to 8 interrupt subroutines can be executed by inputs to a ...
- マニュアル
...bleeder resistor constant can be calculated as follows: R x (VCC – VR)/(IOUT (min.) – ION) Power W y (VCC – VR)2/R × 4 [allowable margin] Note The residual voltage in the PC is 4.0 V for the following Units: C200H-ID211/ID212/IM211/IM212, ...
- 商品情報
...互換モード、通信ユニット接続時) 1ms(C200HSモード、通信ユニットなし)最大10ms入力割り込み割り込み入力ユニット最大8点 C200HS-INT01(8点)入力割り込み機能なしベースユニットC200H-BC□□1-V2(割り込み入力ユニット対応)- 割り込み応答時間 最大1ms(通信...
- 商品情報
...末尾が「-V1」「-V2」の場合、それぞれ以下のユニットに対応しております。・C200H-BC□□1-V1:C200H-OC225、C200H-OD212、C200H-OD21A、C200H-B7AO1・C200H-BC□□1-V2:上記に加えて、C200HS-INT01(割込入力ユニット)*1形式末尾に「-V□」が付かないベースユニットは、 上記の出力ユニット、割込入力ユニットに対応...