全 1173 件が検索されました。(481 - 500件を表示)

  • マニュアル

    ...製品に同梱される取扱説明書やMSDSなどの紙面へ下記の表示を行うことが必要となります。 Perchlorate Material - special handing may apply, see https://dtsc.ca.gov/perchlorate/ 4. EU電池規則について本 製 品 に は、(EU) 2023/1542 Batteries and waste batteries regulation に 適 合 し た リチ ウ ム コ イ ン 電池 CR2032が組み込まれています。 5....

  • マニュアル

    ...製品に同梱される取扱説明書やMSDSなどの紙面へ下記の表示を行うことが必要となります。 Perchlorate Material - special handing may apply, see https://dtsc.ca.gov/perchlorate/ 4. EU電池規則について本 製 品 に は、(EU) 2023/1542 Batteries and waste batteries regulation に 適 合 し た リチ ウ ム コ イ ン 電池 CR2032が組み込まれています。 5....

  • マニュアル

    ...Specifications Capacity R a t ed input volta ge Input volta g e ra ng e Input maxi- for rated input voltage mum current for rated loads connected Input t ermina l Input prot ect ion Input prot ect ion ca...

  • マニュアル

    ...XM2A-0901 9-pin, made by OMRON, for PT side XM2S-2511 25-pin, made by OMRON, for personal computer side XM2S-0911 9-pin, made by OMRON, for PT side AWG28×5P IFVV-SB Multi-core shielded cable, made by Fujikura Ltd. ...

  • マニュアル

    ... by OMRON, for personal computer side 9-pin, made by OMRON, for PT side Connector hood XM2S-2511 XM2S-0911 25-pin, made by OMRON, for personal computer side 9-pin, made by OMRON, for PT side Cable AWG28×5P IFVV-SB ...

  • マニュアル

    ... to the input field at the top left of the screen ↑, ↓, ←, → Used to move to the required input field Confirms input without shifting to another input field Stops the buzzer , Shift between input fields MENU Used to display the System Menu ...

  • マニュアル

    ... ordinances as they apply. • The following precaution must be displayed on all products containing lithium primary batteries with a perchlorate content of 6 ppb or higher when exporting them to or shipping them through California, USA. Perchlorate Material - special handling may apply. See www.dtsc....

  • マニュアル

    ... ordinances as they apply. • The following precaution must be displayed on all products containing lithium primary batteries with a perchlorate content of 6 ppb or higher when exporting them to or shipping them through California, USA. Perchlorate Material - special handling may apply. See www.dtsc....

  • マニュアル

    ... local ordinances as they apply. • The following precaution must be displayed on all products containing lithium primary batteries with a perchlorate content of 6ppb or higher when exporting them to or shipping them through California, USA. Perchlorate Material - special handling may apply. See www.dtsc....

  • マニュアル

    ...ach Langua age The font se ettings for te ext strings off objects are e common across a all thee languages s. You canno ot therefore change c fontt size or colo or between languages. You ca can specify y these parameeters for each languagge. If the text othe er than default is not speciffied, the setting g is default displayeed. Commoon to all lang guages 15 5 2-3 Sw witching Among A Mu ultiple Lan nguages 2--3-1 Settting Up the e Startup L anguage You u can select the languag ge that is dissplayed at th...

  • マニュアル

    ... the PC (Programmable Controller). This data can be further manipulated and transferred to other I/O Units for extended system control. The C200H Temperature Sensor Unit is available in four models. The C200HTS001/002 are for use with thermocouples, and can be used with K (...

  • マニュアル

    ... details, refer to the PC or host computer manuals. C500-LK203 Noise Tolerance The RS-422 interface on the C500-LK203 Host Link Unit is insulated to improve its tolerance to electrical noise. Although the increased tolerance provides better performance under normal operating conditions, the operation ...

  • マニュアル

    ... approaches the Read/Write Head and then reads data from the internal memory of the Data Carrier as it comes within detection range of the Read/Write Head. Up to 1024 bytes (512 words) of data can be read at a time. Clear-all ...

  • マニュアル

    ...(reference) Classification by application and tolerance Constituent materials + conductor B R ----- BX-G --RX-G, SX-G --- General-purpose, standard class S --- RX-H, SX-H --- Heat-resistant, standard class K ...

  • マニュアル

    ...一一一 BX-G 一一一 G旬eraトpurp◎se,standardclass Copper C◎pper B R ●工■ RX-G,SX・G ●●一 AlbywRhcoppgromickglasmak)r◎◎nstRuθnt S ●●一 RX・H,SX・H ●●■ Heat-rgsistant,standardclass K CA KX-G WCA・G Gθ随raトpurpos9,standaζdclass Albywithnickθlorchromeasmajorconstituent Alloyw口hnickθlasmalorcons慌uent KX・GS WCA唱S KX・H WCA-H Heat-resistant,standardclass KX・HS WCA-HS Heat・resistant,precisionclass WX-G WCA{i General・purP◎se,standardclass lron A‖oywロhcoppgrornickθlasmajorcons世U白nt WX・H WCA・H Heat・resistant,standardclass VX・...

  • マニュアル

    ... Unit models and available temperature sensors. Only one kind of temperature sensor can be connected to the C200H-TS001 or C200H-TS002. Each Temperature Sensor Unit connects to a maximum of four temperature sensor inputs. Model Connectable temperature sensor C200H-TS001 K (...

  • マニュアル

    .../0 to 10 V (switchable); 2 outputs C200H-DA001 Programmed using the Fuzzy Support Software. Up to 8 inputs and 4 outputs. C200H-FZ001 Available on either 3.5” or 5.25” floppy disks. C500-SU981-E Thermocouple p K(...

  • マニュアル

    ...External signal is s line-driver ed e signal X/Z Axis Y/U Axis Y/U Axis Specification Response Time A15 A14 B15 B14 Conform to above input specifications spec ca o s N.O. contact: 0.1 ms 0 s max. a C contact: N.C. 1 ms max. A16 A14 B16 B14 Signal is a line-driver output corresponding ssignal g a co espo d g to o S Am26LS31 N.O. contact: 0.1 ms 0 s max. a C contact: N.C. 1 ms max. 19 Section Specifications Output Specifications Item 2-1 Specification Maximum ...

  • マニュアル

    ... at startup. Using FinsGateway Select FinsGateway as the communications driver. Using CX-Server Select CX-Server as the communications driver. 1-6-3 Using FinsGateway Regardless of the connection method, use FinsGateway as the communications driver. Communications network Serial co ...

  • マニュアル

    ....0 or later). To change the size of the I/O comment 168 Section 8-2 Programming Console Operations area, refer to the CX-Programmer (version 2.0 or later) Operation Manual (W414). RUN MONITOR OK OK CLR ...