全 513 件が検索されました。(421 - 440件を表示)

  • マニュアル

    ... 1999 # 0000 to 9999 or 0000 to FFFF 135 Appendix E Programming Instructions Name Mnemonic Symbol BIT COUNTER (@)BCNT(67) Function Operand Data Areas Counts the number of ON bits in one or more words (...

  • マニュアル

    ...HR 1214 HR 1215 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 16-TO-4 ENCODER – DMPX(77) Operand Data Areas SB: First source word Ladder Symbols IR, SR, AR, DM, HR, TC, LR DMPX(77) @DMPX(77) SB SB R R Di Di R: Result word Limitations IR, AR, DM, HR, LR Di: Digit designator IR, AR, DM, HR, TC, LR, # The rightmost two digits of Di must each be between 0 and 3. 155 Section 5-16 Data Conversion All source words must be in the same data area. Description...

  • マニュアル

    ...3・e3亀S◎ CSock..P研ses 1 鞠lsew}d詣 。 」si。 ・2・]… Flag 蜘{-63・-63・2 Gec}eracese.f・sdWkρutSe 慈㌶裟懇懇髭灘寒 `).■o.05s・bi・,・o.05s畦 ←α↓sB{Tan Geh合'ateso.2・scbckpvigs 懸灘懸鱗簗簗 』-a.te.-eiー一〇、15͡ 栖一一一〇.2s−一一階茸]戴〕1 Geiterates1.0$ciOckpuiSe 欝欝欝欝灘謹蘂 .;e-e.5s-*-o.5s-el Pt1.es→ 8it5302 Eachciockb'R'esONforthefirsthaifoftherateCtpuisetlme,thenOF肖orlhe latterhaif・治o齢rw。 rCts、eaChc}。...

  • マニュアル

    ...HR 1214 HR 1215 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 16-TO-4 ENCODER – DMPX(77) Operand Data Areas SB: First source word Ladder Symbols IR, SR, AR, DM, HR, TC, LR DMPX(77) @DMPX(77) SB SB R R Di Di R: Result word Limitations IR, AR, DM, HR, LR Di: Digit designator IR, AR, DM, HR, TC, LR, # The rightmost two digits of Di must each be between 0 and 3. All source words must be in the same data area. Description 152 When the execution condition is ...

  • マニュアル

    ...0 HR 1215 0 15 1 2 RB+1 : HR 11 6 0 3 4-8-6 Encoder - DMPX(78)<77> DMPX(78) determines the position of the highest ON bit in the specified beginning source channel (SB), encodes it into single-digit hexadecimal data according to the bit number, then transfers the result to the specified digit in the result channel (R). Up to four digits from four consecutive source channels starting with ...

  • マニュアル

    ...RT2」 VERMNG RTI_.1 RTI_2 LTEST.EX∈ RT1迫 SCAE2 SCAEl SCA7 SCA5 SCA4 SCA3 SCA2 SCAI SCAE7 SCAE6 SCAEs SCAE4 SCAE3 SBEI S8E2 SBEEI SBEE2 SB円 SBF2 SBF自 SCA6 SBFE2 DIAGMT32.DAT DGTESTM.EXE PCDSPMSM.C ROUTE.DAT DGSUB.BIN CONF32.EXE INST32M.EXE VER32,EXE PCDSPMSM.EXE DGSUB.OBJ RTREAD、EXE OPTCONF.EXE RTSET.EXE TBLCONF.EXE CUT32.EXE DIAGMT32、EXE ATDSP8AM.BAS CONFIG.SMP DGIOX.SYS 翼翼憂翼翼服認翼翼翼翼璽㎜蜘㌶潔86㎜ 司11 蕪繋…蕪議…繋…講講羅…講羅』 52㎝...

  • マニュアル

    ...HR 1214 HR 1215 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 16-TO-4 ENCODER – DMPX(77) Operand Data Areas SB: First source word Ladder Symbols IR, SR, AR, DM, HR, TC, LR DMPX(77) @DMPX(77) SB SB R R Di Di R: Result word Limitations IR, AR, DM, HR, LR Di: Digit designator IR, AR, DM, HR, TC, LR, # The rightmost two digits of Di must each be between 0 and 3. All source words must be in the same data area. Description 158 When the execution condition is ...

  • マニュアル

    ...f 18 24 CN CAN X X f f f f f 19 25 EM S1 X X f f f f f 1A 26 SB EOF X X f f f f f 1B 27 EC ESC X X f f f f f 1C 28 → S4 f f f f f f f 1D 29 ← S5 f f f f f f f 1E 30 ↑ S6 f f f f f f f 1F 31 ↓ S7 f f f f f f f 00 0 NUL X 01 1 SH SOM 02 03 2 SX EOA 3 EX...

  • マニュアル

    ...S襯S喘S鵬 ㎜脇∂㎜㎜㎜㎜展翅蜘蜘 ㎜18 ㎜ …… … … S砿◆h 創 for SNQI 脇1 Swteh for S櫛1 飽m1 S醜ol潮 forS鴇1 Sb比C紺 「orS嶋1 S縛Q1 →ト s賜1 】 1圃2書目闘■麺一蟹田窟圃7蟹園圃■8日間■曽S眉目翻劃一■C MnemonlcLadderPro9『amming Whenaprogramiscreatedinmnem◎nicform,itiSautomaticallywrittentothe workdisk.1/OnamescannormallybebetWeen2and81ettersinlength,butenly sIettersaredisplayedinthemnemonicprogram.1/OcommentscanbeuptO30 characterslong.AIIl10commentscreatediRthemnemonicdisplaymodecanbe 74・ ---------------------[End of Page 9104]--------------------- P?り即〃∂卿inカ...

  • マニュアル

    ...CTS 20 DTR 6 DSR The following cables are recommended for connecting the host computer and PC. Other cables can be used if desired as long as they meet the required specifications. Manufactured by Fujikura: UL2464 AWG28 x 5P IFS-RVV-...

  • マニュアル

    ...FG Frame ground --- Applicable Connector Plug: XM2A-0901 (OMRON) Hood: XM2S-0911 (OMRON) or equivalent One plug and one hood are supplied for each port. Connectors other than those on the left cannot be used. Recommended Cables AWG28 x 5P IFVV-...

  • マニュアル

    ...130 140 150 160 170 180 190 200 210 220 230 240 250 0k RUN MKI$( MKS$( 'testco㎜andnarne:MK工$/MKS$/MKD$ PARACTO DIMBUF$128 1A宅=100駕:SB=12345.6=DC#=12345.123456789# OPEN"DATA"AS#1 F工ELD#ユ,128ASBUF$ A$=MK工$(IA%) PR工NT"MK工$(":1A毯;")一一〉";A$ B$=MKS$(...

  • マニュアル

    ...A (F n) FD Label E Label F Label G FF FG SF SG FE FB Fuzzy output n Label D FC FA 0 0 SA SB SC SD SE FFF Output data If all of the fuzzy outputs are zero, the divisor in the equation above will also be zero, the division will not be performed and the Error Flag (bit 15) and No Corresponding Output Flag (bit 04) for that output will be turned ON. Refer to 3-3-2 Output Data for details on the output data format. Maximum Value Method 8 The maximum value method uses ...

  • マニュアル

    ...152 SUBROUTINERETURN ROL(↑) 062 ROTATELEFT ROLL(↑) 066 DOUBLEROTATELEFT ROOT(↑) 140 SQUAREiROOT ROR(↑) 063 ROTATERIGHT RORL(↑) 067 DOUBLEROTATERIGHT RSET側) 017 RSET SA(↑) 210 ACTIVA「「ESTEP SBB(↑) 081 BlNARYSUBTRACT ...

  • マニュアル

    ...HR 1215 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 5-17-8 16-TO-4 ENCODER – DMPX(77) Operand Data Areas SB: First source word Ladder Symbols IR, SR, AR, DM, HR, TC, LR DMPX(77) @DMPX(77) SB SB R R Di Di R: Result word Limitations IR, AR, DM, HR, LR Di: Digit designator IR, AR, DM, HR, TC, LR, # The rightmost two digits of Di must each be between 0 and 3. All source words must be in the same data area. Description 152 When the execution condition ...

  • マニュアル

    ...1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 5-19-6 16-TO-4 ENCODER – DMPX(77) Operand Data Areas Ladder Symbols SB: First source word IR, SR, AR, DM, HR, TC, LR DMPX(77) @DMPX(77) SB SB R R Di Di R: Result word Limitations IR, SR, AR, DM, HR, LR Di: Digit designator IR, SR, AR, DM, HR, TC, LR, # The rightmost two digits of Di must each be between 0 and 3. All source words must be in the same data area. DM 6144 to DM 6655 cannot ...

  • マニュアル

    ... remain in R (counting from the designated first digit), the remaining digits will be placed at digits starting back at the beginning of R. The final word to be converted (S plus the number of digits to be converted) must be in the same data area as ...

  • マニュアル

    ...LOSSOFPROF[TSORCOMMERCIALLOSSINANYWAYCONNECTEDWITHTHEPRODUCTS, WHETHERSUCHCLAIMISBASEDONCONTRACT,WARRANTY,NEG〕GENCE,ORSTRICT LIABILITY lnnoeventshalltheresponsibilityofOMRONforanyactexceedtheindividualpriceofthepreductonwhich liabilityisasserted. INNOEVENTSHALLOMRONBERESPONSIBLEFORWARRANTY,REPAIR,OROTHERCLAlMS REGARDINGTHEPRODUCTSUNLESSOMRON`SANALYSISCONFIRMSTHATTHEPRODUCTS WEREPROPERLYHANDLED,STORED,INSTALLED,ANDMAINTAINEDANDNOTSUBJECTTO CONTAMINATION,ABUSE,MISUSE,ORINAPPROPRIAτEMODIFICATIONORREPAIR, 1 ---------------------[End of Page 2986]--------------------- No.6†82 AρpIicationCoηs∫de]rations SL〃7フ...

  • マニュアル

    ...Output 9 Signal ground SG – Shell Safety ground FG – Plug: XM2A-0901 (OMRON) or equivalent Hood: XM2S-0911 (OMRON) or equivalent Note One plug and one hood are provided. Recommended Cable 12 AWG28 5P IFVV-...

  • マニュアル

    ...: 512 bytes Flow control RTS/CTS flow, Xon/Xoff flow control supported Connector type D-sub 9-pin for both ports Applicable connector (enclosed) Plug: XM2A-0901 or equivalent Connector hood: XM2S-0911 or equivalent Recommended cable UL2464 AWG28x5P IFS-RVV-...