全 64 件が検索されました。(21 - 40件を表示)

  • マニュアル

    ...ジが表示されますので、[OK]を押下してください。 MicroHAWK V320-F/V330-F/V420-F/V430-Fシリーズ ユーザーズマニュアル(84-9000401-02) S S-9 付録 16 WebLinkが起動します。 17 バージョンを確認します。 WebLink画面が表示されたら、画面右上の歯車マーク - [About WebLink...]を押下してくだ...

  • マニュアル

    ... CS 2 STA.ERRORS INF. 90-09-05 The date is displayed first. This date was previously registered by the user as the date from which errors were to be monitored. Year Month Day INC STA.ERRORS INF. S 9 1 COM.DC E Press the INC key to display the number of times an error has occurred, the error message, and the R/W Head word number. Error message Number of times an error occurred R/W Head word number (fixed to 1) Up to 999 errors can be displayed. If 1000 errors have occurred, the 1000th error ...

  • マニュアル

    ...+6 00 2F Class ID: 002F Hex 253 Section 6-1 C200H I/O Link Units S+7 Word Contents (Hex) 00 01 Meaning Instance ID: For IR Area 1: 0001 Hex S+8 0A 00 S+9 28 00 Read start address: 10 = 000A Hex Address L: 0A Hex, Address H: 00 Hex No. of bytes of read data: 40 bytes = 28 Hex (The rightmost byte is not used.) D: Destination Information Results are stored as shown in the following table. Word D Contents (Hex) 00 10 (0 010) Meaning Master’s Unit address: 0, No. of words ...

  • マニュアル

    ...m + 27 m + 31 0 to 9 0000 to 0009 hex 0 (0000 hex) 0: K, 1: K (with decimal point), 2: J, 3: J (with decimal point), 4: T, 5: L, 6: L (with decimal point), 7: R, 8: S, 9: B m + 20 m + 24 m + 28 m + 32 0, 1 0000, 0001 hex 0 (0000 hex) Select either high limit or low limit alarm output. 0: High limit alarm; 1: Low limit alarm m + 21 m + 25 m + 29 m + 33 0 to 9999 0000 to 270F hex 0 (0000 hex) m + 22 m + 26 m + 30...

  • マニュアル

    ... number = 3F (Hex) specifies 63 Master’s unit address = FE (Hex) specifies the local Unit • Command Words (Source information) Word S S+1 S+2 S+3 S+4 S+5 S+6 S+7 S+8 S+9 Contents Function (Hex) 82 07 Specifies starting response word = DM 2000 82 (Hex) specifies the DM area D0 00 07D0 (Hex) specifies address 2000 (Refer to the C200HX/HG/HE Operation Manual (W303) for details.) 00 64 Response monitoring time = 64 (Hex) specifies 10.0 seconds 00 0B Number of bytes of command data beginning with word S+4 = 0B (...

  • マニュアル

    ... connections for each Slave (although COS and cyclic cannot be specified simultaneously). Communications cycle time Uses values by default are calculated by the following equations. Example: 16 Input Slaves (16 points each), 16 Output Slaves (16 points each), and a baud rate of 500 Kbit/...

  • マニュアル

    ... step 8. If replacing the LED Board, unscrew the two #2-56 flat head screws that secure the diffuser. Note: Do not touch the electronics or lens, as this may cause damage. MicroHAWK V320-F / V330-F / V420-F / V430-F Barcode Reader User Manual ...

  • カタログ

    ...ュータと通信する場合の通信速度を設定します。 通信速度はそれぞれ次のとおりです。 1.2(1200bit/s)、2.4(2400bit/s)、4.8(4800bit/s)、9.6(9600bit/ s) 、19.2(19200bit/s) なお、設定値は設定後の電源再投入により有効となりますのでご注意ください。 サーマックR サーマ...

  • カタログ

    ... be set using the DIP switch. OFF Time Range (oftr) NPN/PNP Input Mode (imod) Set the time range for the OFF time in the range 0.000 s to 9,999 h. Only settings of type --.-- s (99.99 s), ---.- s (999.9 s), ---- ...

  • マニュアル

    ...), 'lhe"PID§etse亘ectionhyst¢resis"parametersetsthehysteresisfo彗)reventingch-at㈱r且ng d㎞gswitc1血g◎fIPIDsets. 鰹冑_..' C◎mment ・"擁Dsetselectlondata"p蹴meter Set也e】PiDsetselectiondagaby也ecodeswithin也erangeOt{》63inEまxeanalogOPerati《}n assignment(argume斑...

  • マニュアル

    ...ons._.._._._.__._3-4 Settingitem__.,.__、._.___..,__......_.._3-7 Settingitems1-8__.____._.____._5-8 Settinglevel1__._._._______.__.._.1-8 Settinglevel2___"_._______,____.1-8 Settingmode.______.____.__._1-9,5-52 Designatingsettingmodes___.__.__3-3 Settingswitch._._..___..____e.__.._24 Shiftkeys._.._._._、.._.._.___、_._._._..1-5 Specificationssettingmode_._..__.一...、._.5-3 SPfallratelim柱,_......._..,.._、._.._..__._5-69 SPmode._.、__.______.._.、_._._...

  • マニュアル

    ...臼aight-1錐▲eapproxi㎜tionlou甲ut2 0024 S画ght-§neappn⊃x㎞a60n2三nl)ut1 0025 Straight−泡10a匡}P⑳ximano"2i11put2 0026 Straigh卜1三neapprox07Lation2◎utput1 0027 Stまaigh1-lineal)proxinlaUon20utput2 0028 ...

  • マニュアル

    ...once. Doing so will prevent normal operation. (Set Modbus communications unit numbers to between 1 and 99.) • Baud Rate Set the baud rate for communications with the host computer. The following baud rates can be set: 4.8 (4,800 bits/...

  • マニュアル

    ...-Protocol. (R(3N+3), 4) The Inverter’s actual data to be sent. This example selects Variable and Read R() and sets the operand. Set Data to 3N + 3 because the RUN command data uses four bytes each from S + 3, S + 6, and ...

  • マニュアル

    ...-Protocol. (R(3N+3), 4) The Inverter’s actual data to be sent. This example selects Variable and Read R() and sets the operand. Set Data to 3N + 3 because the RUN command data uses four bytes each from S + 3, S + 6, and ...

  • マニュアル

    ... reference to Slave 2 Third Slave address 0003 RUN command to Slave 3 Frequency reference to Slave 3 Protocol macro function S 1 S 2 S 3 S 4 S 5 S 6 S 7 S 8 S 9 S 10 RS-422A /485 Number of data items received in accordance with PMCR instruction 0003 D D D D 999 Data 1 2 3 Slave 1 Inverter status Slave 2 Inverter status Slave 3 Inverter status SYSMAC CS or CJ-series Programmable Controllers 6-101 Communications Board C: Control data (See note.) 15 12 11 C S D Data...

  • マニュアル

    ... CX-Protocol. (R(3N +3), 4) The Inverter’s actual data to be sent. This example selects Variable and Read R() and sets the operand. Set Data to 3N + 3 because the RUN command data uses four bytes each from S + 3, S +6, and ...

  • マニュアル

    ...Response*6 Communications port number: Number of sends: 00 to 0F hex 0 to 7*7 (0 to 15)*8 Response monitor time: 0000 hex → 2 s [in units of 0.1 0001 to FFFF hex → 0.1 to 6553.5 s s] *9 DeviceNet Communications Unit User’s Manual (I581-E1) 5-5 5 5-2-1 How to Issue Explicit Messages by CMND Instruction *1 Set how many bytes the command data storage area occupies from first word address S. *2 Set how many bytes the response data storage area occupies from first word address D. *3 The ...

  • マニュアル

    ... in hours, minutes, and seconds within a range between 0 h, 00 min, 00 s and 9 hrs, 59 min, 59 s. scal Displayed in minutes and seconds (1/100 s) within a range between 00 min, 00 s 0 and 59 min, 59 s, 9...

  • マニュアル

    ...Index Registers --- Indirect addressing using Index Registers ,IR0 or ,IR1 –2048 to +2047 ,IR0 or –2048 to +2047 ,IR1 ,IR0+(++) or ,IR1+(++) , –(– –)IR0 or, –(– –)IR1 Specified values only #0000 STUP(237) writes 10 words of data from S to ...